Hi everyone,
I am using an imx6q board to capture a raw10 bit image. I need to scale it from 10 bit to 16 bit .
I did necessary changes such as disabling the compander . I am able to get 16 bit image as output.
My doubt is that how scaling is done to make 10bit to 16 bit . Whether 0's or 1's are simply added for extra bits to make it 16 bit or any other technique is used?
Where can i find the code portion for scaling ?
Hi igor,
We got a 16-bit output. However, our observation is that the 10-bit data is somehow scaled using some factor to make it 16-bit.
What we expect is 10-bit original data (without any alteration) padded with 0's or 1's (either at LSB or MSB) to make it 16-bit. How can we achieve this? We are using i.MX6q with OV5647 sensor.
Hi Arun
if you did not add special processing, then seems ipu just
writes camera 10 bits data to the MSB of a 16-bit word, this is
described in Table 37-2. Data Formats Supported By The Camera Port
i.MX6DQ Reference Manual
http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf
Best regards
igor
Hi igor,
In mxc_v4l2_capture.c, we are using index 1 (CSI MEM) as input. Hence, we assume there is no special processing involved in storing 10-bit data in 2 bytes. Is this correct?
>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>
static struct v4l2_input mxc_capture_inputs[MXC_V4L2_CAPTURE_NUM_INPUTS] = {
{
.index = 0,
.name = "CSI IC MEM",
.type = V4L2_INPUT_TYPE_CAMERA,
.audioset = 0,
.tuner = 0,
.std = V4L2_STD_UNKNOWN,
.status = 0,
},
{
.index = 1,
.name = "CSI MEM",
.type = V4L2_INPUT_TYPE_CAMERA,
.audioset = 0,
.tuner = 0,
.std = V4L2_STD_UNKNOWN,
.status = V4L2_IN_ST_NO_POWER,
},
};
>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>
Hi Arun
I am not aware of companding examples but
companding formula is given in sect.37.4.3.5 Companding i.MX6DQ RM:
Companding is performed as follows:
input: 10-bit unsigned number.In case that component's size is bigger than 10 bit, 10
MSB bits are taken. In case that component's size is less than 10 bit, color extraction is
performed.
First step: shift:
x-> clip(x + offset, 0, 1023)
where the offset is a 10 bit signed number that is configured in CPD_OFFSET1 and
CPD_OFFSET2 registers.
second step - piecewise-linear map:
y = Min[255, (y1[k]+(((x-x1[k])*slope[k])>>6 + 1))>>1]
where:
- the input range 0..1023 is partitioned to 16 equal segments: x1[k] .. x1[k+1] - 1 where
x1[k] = 0, 64, 128, 192, 256, .. . 960.
- The linear map, in each segment, is characterized by y1[k] (9-bit unsigned number) and
slope[k] (8-bit unsigned number).
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------