Imx6q how to add CAN2 (flexcan1)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Imx6q how to add CAN2 (flexcan1)

761件の閲覧回数
李鹏斌
Contributor II

Imx6q how to add the second CAN (flexcan1), the STBY of the second CAN pin which is it?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

661件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi

please use imx6q-sabreauto-flexcan1.dts

linux-imx.git - i.MX Linux Kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

661件の閲覧回数
李鹏斌
Contributor II

Thank you for your reply, I use the version is "linux3.0.35", I would like to use the "kernel imx6q_add_flexcan1" to add the second CAN, but I do not know how to define "mx6q_sabresd_flexcan1_pdata",

"Mx6q_sabresd_flexcan1_pdata" is defined as follows:

can.png

0 件の賞賛
返信