Imx6q Ethernet throughput workaround

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Imx6q Ethernet throughput workaround

970 Views
prathamrahate
Contributor III

Hi,

I am using imx6q based custom board. When i run iperf server on imx6q i see around 90% packet drops at 1000Mbps UDP traffic. I came across post pointing to The i.MX6DQ Errata document states in Errata ERR004512 that the maximum performance “is limited to 470 Mbps (total for Tx and Rx)”. So are there any patches available to enable pause frame mode and increase the throughput. I am using linux kernel 3.14.52.

Thanks,

Prathamesh 

Labels (3)
0 Kudos
Reply
1 Reply

786 Views
Yuri
NXP Employee
NXP Employee

Hello,

  The following - hope - helps.

https://community.nxp.com/thread/390519 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply