Imx6dl Android P9.0.0_2.2.0 ethernet(usb ethernet) link is up but ping fail

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Imx6dl Android P9.0.0_2.2.0 ethernet(usb ethernet) link is up but ping fail

1,651 Views
chpub70
Contributor II

Hi NXP,

I am using a custom imx6dl board with android_p9.0.0_2.2.0-ga. From the command line, I did ifconfig eth0 up 192.168.30.240 and I did ip link and I can see the link is up.

130|sabresd_6dq:/ # ip link
1: lo: <LOOPBACK,UP,LOWER_UP> mtu 65536 qdisc noqueue state UNKNOWN mode DEFAULT group default qlen 1000
link/loopback 00:00:00:00:00:00 brd 00:00:00:00:00:00
2: ip_vti0@NONE: <NOARP> mtu 1480 qdisc noop state DOWN mode DEFAULT group default qlen 1000
link/ipip 0.0.0.0 brd 0.0.0.0
3: ip6_vti0@NONE: <NOARP> mtu 1500 qdisc noop state DOWN mode DEFAULT group default qlen 1000
link/tunnel6 :: brd ::
4: sit0@NONE: <NOARP> mtu 1480 qdisc noop state DOWN mode DEFAULT group default qlen 1000
link/sit 0.0.0.0 brd 0.0.0.0
5: ip6tnl0@NONE: <NOARP> mtu 1452 qdisc noop state DOWN mode DEFAULT group default qlen 1000
link/tunnel6 :: brd ::
6: eth0: <BROADCAST,MULTICAST,UP,LOWER_UP> mtu 1500 qdisc pfifo_fast state UP mode DEFAULT group default qlen 1000
link/ether 00:de:fa:87:6e:d7 brd ff:ff:ff:ff:ff:ff

However when I did ifconfig eth0, I see all received packet is dropped.

sabresd_6dq:/ # ifconfig eth0
eth0 Link encap:Ethernet HWaddr 00:de:fa:87:6e:d7 Driver smsc95xx
inet addr:192.168.30.240 Bcast:192.168.30.255 Mask:255.255.255.0
inet6 addr: fe80::2de:faff:fe87:6ed7/64 Scope: Link
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:13270 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 TX bytes:0

Please advise. 

Thank You in advance.

Regards,

Pun

0 Kudos
Reply
5 Replies

1,604 Views
joanxie
NXP TechSupport
NXP TechSupport

when the board boot up, could you ping successfully?

0 Kudos
Reply

1,604 Views
chpub70
Contributor II

Hi Joan,

No, I cannot ping successfully.

0 Kudos
Reply

1,603 Views
joanxie
NXP TechSupport
NXP TechSupport

pls share your log file with me

0 Kudos
Reply

1,604 Views
chpub70
Contributor II

Hi Joan,

Attach is the log for dmesg and logcat.

0 Kudos
Reply

1,487 Views
joanxie
NXP TechSupport
NXP TechSupport

what PHY do you use? the same as nxp board? or porting your own PHY? and could you reproduce this on nxp board?

0 Kudos
Reply