Imx6DL/Solo Ethernet stabilize issues

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Imx6DL/Solo Ethernet stabilize issues

491 Views
ganesh1051
Contributor I

HI , 

In my project I have used IMX6Solo/Dual Lite Processor , We are gonna use live video streaming from processor to PC or laptop or cloud with resolution of 1080p@30fps . We are streaming the video via ethernet interface (1Gbps) . I refereed the errata sheets its clearly mentioned like , We can't able to achieve more than 400Mbps .

In our custom board , at 200Mbps itself not stable and facing error of 0.028% and I have tested with wandboard also . Same issue exist . I want to know how to overcome this issue , I need stabilize speed range for ethernet . 

Kernel : Linux kernel 3.14.28 

Processor : IMX6Solo/Duallite.

Note : Please find the iperf test of wandboard .

Labels (3)
0 Kudos
1 Reply

408 Views
igorpadykov
NXP Employee
NXP Employee

Hi ganesh

please check suggestions on

i.MX6 Gigabit Ethernet - Boundary Devices 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos