Imx6 linux + Hypervisor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Imx6 linux + Hypervisor

2,098 次查看
ailtonlopes
Contributor III

Hi, 
I'm working on an trustzone assisted hipervisor (LTZVisor) and i want to run a baremetal OS on the secure World and Linux on the NS Guest.

My question how can i run the linux OS after executing the Startup code and the Hypervisor, now im running the linux using the u-boot as the boot loader and im not sure how to combine both things, the hypervisor and the uboot and linux.

Basically my question is how i can start linux after starting the hypervisor .

Kind regards,

Ailton Lopes

标签 (2)
0 项奖励
回复
1 回复

1,456 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ailton

nxp i.MX6DQ official bsps do not support such use case, one can look on

Boot The i.mx6 dual With Linux+uC/OS-II AMP 

http://www.dave.eu/sites/default/files/an-xelk-001-amp-linux-freertos.pdf 

https://community.nxp.com/thread/324831#408721 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复