Imx6 Sabrilite not receiving Packets

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Imx6 Sabrilite not receiving Packets

639 Views
sarahblessie
Contributor I

Hi,

I have a imx6 sabrelite board and I am trying to ping the boards IP from the PC and It works fine, similarly I could ping PC from the imx6 board.

I have a Vayu EVM board and I trying to ping this board from the imx6 and it could not and the same when tried other way.

this is my result when tried ping

Ping form imx6

ping 172.16.7.117

PING 172.16.7.117 (172.16.7.117): 56 data bytes

^C

--- 172.16.7.117 ping statistics ---

3484 packets transmitted, 0 packets received, 100% packet loss

ping from j6

ping 172.16.7.123

PING 172.16.7.123 (172.16.7.123): 56 data bytes

^C

--- 172.16.7.123 ping statistics ---

2941 packets transmitted, 0 packets received, 100% packet loss

No reply packets are received,

I also tried sending ethernet and IP packets from imx6 on multicast and could successfully receive in the Vayu board. But when the Vayu board sends the packet the imx socket could not receive. But the same packets from PC could be received by imx6.

Please suggest me of solution! Thanks in advance

Regards,

Sarah Blessie

Labels (2)
0 Kudos
1 Reply

465 Views
sarahblessie
Contributor I

Hi,

This is resolved. This issue is due to J6 Packing VLAN Tag with its ethernet Packets

Thanks and regards,

Sarah

0 Kudos