Hi Edward
I am afraid i.MX28 mfg tools is not supported in yocto, however
one can try existing mfg tools and just rename files produces by yocto, then
put them to /files folder, attached ucl.xml shows linux commands.
In general mfg tools firmware is small linux image which can execute
all commands as usual linux. Regarding question:
"get u-boot to find/run/link to the kernel image and also the rootfs.tar.b2z":
for NAND official FSL BSP uses only linux_ivt.sb and rootfs.tar.bz2, for NAND supported only ubifs.
Available kernel boot options one can find in attached Linux Guide
sect.5.1.1 Setting Up Kernel Command Line
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------