Imx rt1050 compilation issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Imx rt1050 compilation issue

Jump to solution
1,192 Views
rizwan_s
Contributor II

Hi,

I am trying to build default code from the below path for imx rt1050.

Version of IAR used :8.20.2

C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar\csi_rgb565.eww

I get the following errors.

Building configuration: csi_rgb565 - sdram_debug
Updating build tree...

0 file(s) deleted.
Updating build tree...
startup_MIMXRT1052.s
Could not open file: 'C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\devices\MIMXRT1052\iar\startup_MIMXRT1052.s'
Error while running Assembler
clock_config.c
Fatal Error[Pe1696]: cannot open source file "fsl_common.h" C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\clock_config.c 30
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar/../../../../../../CMSIS/Include\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar/../../../../../../devices\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar/..\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar/../../../..\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar/../../../../../../devices/MIMXRT1052/drivers\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar/../../../../../../devices/MIMXRT1052\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\
iar/../../../../../../devices/MIMXRT1052/utilities/io\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\
iar/../../../../../../devices/MIMXRT1052/utilities/str\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\
iar/../../../../../../devices/MIMXRT1052/utilities/log\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar/../../../../../../devices/MIMXRT1052/utilities\"
searched: "C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.0\arm\inc\"
searched: "C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.0\arm\inc\c\"
current directory: "C:\NXP\2.3.0_EVK-MIMXRT1050"
Error while running C/C++ Compiler
board.c
Fatal Error[Pe1696]: cannot open source file "fsl_common.h" C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\board.c 30
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar/../../../../../../CMSIS/Include\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar/../../../../../../devices\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar/..\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar/../../../..\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar/../../../../../../devices/MIMXRT1052/drivers\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar/../../../../../../devices/MIMXRT1052\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\
iar/../../../../../../devices/MIMXRT1052/utilities/io\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\
iar/../../../../../../devices/MIMXRT1052/utilities/str\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\
iar/../../../../../../devices/MIMXRT1052/utilities/log\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar/../../../../../../devices/MIMXRT1052/utilities\"
searched: "C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.0\arm\inc\"
searched: "C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.0\arm\inc\c\"
current directory: "C:\NXP\2.3.0_EVK-MIMXRT1050"
Error while running C/C++ Compiler
fsl_assert.c
Fatal Error[Pe1696]: cannot open source file "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\devices\MIMXRT1052\utilities\fsl_assert.c"
Error while running C/C++ Compiler
csi_rgb565.c
Fatal Error[Pe1696]: cannot open source file "fsl_elcdif.h" C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\csi_rgb565.c 31
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar/../../../../../../CMSIS/Include\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar/../../../../../../devices\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar/..\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar/../../../..\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar/../../../../../../devices/MIMXRT1052/drivers\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar/../../../../../../devices/MIMXRT1052\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\
iar/../../../../../../devices/MIMXRT1052/utilities/io\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\
iar/../../../../../../devices/MIMXRT1052/utilities/str\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\
iar/../../../../../../devices/MIMXRT1052/utilities/log\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar/../../../../../../devices/MIMXRT1052/utilities\"
searched: "C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.0\arm\inc\"
searched: "C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.0\arm\inc\c\"
current directory: "C:\NXP\2.3.0_EVK-MIMXRT1050"
Error while running C/C++ Compiler
fsl_clock.c
Fatal Error[Pe1696]: cannot open source file "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\devices\MIMXRT1052\drivers\fsl_clock.c"
Error while running C/C++ Compiler
fsl_common.c
Fatal Error[Pe1696]: cannot open source file "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\devices\MIMXRT1052\drivers\fsl_common.c"
Error while running C/C++ Compiler
fsl_csi.c
Fatal Error[Pe1696]: cannot open source file "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\devices\MIMXRT1052\drivers\fsl_csi.c"
Error while running C/C++ Compiler
fsl_csi_camera_adapter.c
Fatal Error[Pe1696]: cannot open source file "fsl_common.h" C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\fsl_video_common.h 34
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar/../../../../../../CMSIS/Include\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar/../../../../../../devices\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar/..\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar/../../../..\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar/../../../../../../devices/MIMXRT1052/drivers\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar/../../../../../../devices/MIMXRT1052\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\
iar/../../../../../../devices/MIMXRT1052/utilities/io\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\
iar/../../../../../../devices/MIMXRT1052/utilities/str\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\
iar/../../../../../../devices/MIMXRT1052/utilities/log\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar/../../../../../../devices/MIMXRT1052/utilities\"
searched: "C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.0\arm\inc\"
searched: "C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.0\arm\inc\c\"
current directory: "C:\NXP\2.3.0_EVK-MIMXRT1050"
Error while running C/C++ Compiler
fsl_debug_console.c
Fatal Error[Pe1696]: cannot open source file "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\devices\MIMXRT1052\utilities\fsl_debug_console.c"
Error while running C/C++ Compiler
fsl_elcdif.c
Fatal Error[Pe1696]: cannot open source file "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\devices\MIMXRT1052\drivers\fsl_elcdif.c"
Error while running C/C++ Compiler
fsl_gpio.c
Fatal Error[Pe1696]: cannot open source file "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\devices\MIMXRT1052\drivers\fsl_gpio.c"
Error while running C/C++ Compiler
fsl_io.c
Fatal Error[Pe1696]: cannot open source file "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\devices\MIMXRT1052\utilities\io\fsl_io.c"
Error while running C/C++ Compiler
fsl_log.c
Fatal Error[Pe1696]: cannot open source file "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\devices\MIMXRT1052\utilities\log\fsl_log.c"
Error while running C/C++ Compiler
fsl_lpi2c.c
Fatal Error[Pe1696]: cannot open source file "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\devices\MIMXRT1052\drivers\fsl_lpi2c.c"
Error while running C/C++ Compiler
fsl_lpuart.c
Fatal Error[Pe1696]: cannot open source file "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\devices\MIMXRT1052\drivers\fsl_lpuart.c"
Error while running C/C++ Compiler
fsl_ov7725.c
Fatal Error[Pe1696]: cannot open source file "fsl_common.h" C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\fsl_video_common.h 34
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar/../../../../../../CMSIS/Include\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar/../../../../../../devices\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar/..\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar/../../../..\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar/../../../../../../devices/MIMXRT1052/drivers\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar/../../../../../../devices/MIMXRT1052\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\
iar/../../../../../../devices/MIMXRT1052/utilities/io\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\
iar/../../../../../../devices/MIMXRT1052/utilities/str\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\
iar/../../../../../../devices/MIMXRT1052/utilities/log\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar/../../../../../../devices/MIMXRT1052/utilities\"
searched: "C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.0\arm\inc\"
searched: "C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.0\arm\inc\c\"
current directory: "C:\NXP\2.3.0_EVK-MIMXRT1050"
Error while running C/C++ Compiler
fsl_sccb.c
Fatal Error[Pe1696]: cannot open source file "fsl_common.h" C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\fsl_sccb.c 31
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar/../../../../../../CMSIS/Include\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar/../../../../../../devices\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar/..\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar/../../../..\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar/../../../../../../devices/MIMXRT1052/drivers\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar/../../../../../../devices/MIMXRT1052\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\
iar/../../../../../../devices/MIMXRT1052/utilities/io\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\
iar/../../../../../../devices/MIMXRT1052/utilities/str\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\
iar/../../../../../../devices/MIMXRT1052/utilities/log\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar/../../../../../../devices/MIMXRT1052/utilities\"
searched: "C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.0\arm\inc\"
searched: "C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.0\arm\inc\c\"
current directory: "C:\NXP\2.3.0_EVK-MIMXRT1050"
Error while running C/C++ Compiler
fsl_str.c
Fatal Error[Pe1696]: cannot open source file "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\devices\MIMXRT1052\utilities\str\fsl_str.c"
Error while running C/C++ Compiler
pin_mux.c
Fatal Error[Pe1696]: cannot open source file "fsl_common.h" C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\pin_mux.c 43
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar/../../../../../../CMSIS/Include\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar/../../../../../../devices\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar/..\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar/../../../..\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar/../../../../../../devices/MIMXRT1052/drivers\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar/../../../../../../devices/MIMXRT1052\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\
iar/../../../../../../devices/MIMXRT1052/utilities/io\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\
iar/../../../../../../devices/MIMXRT1052/utilities/str\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\
iar/../../../../../../devices/MIMXRT1052/utilities/log\"
searched: "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565\iar/../../../../../../devices/MIMXRT1052/utilities\"
searched: "C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.0\arm\inc\"
searched: "C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.0\arm\inc\c\"
current directory: "C:\NXP\2.3.0_EVK-MIMXRT1050"
Error while running C/C++ Compiler
system_MIMXRT1052.c
Fatal Error[Pe1696]: cannot open source file "C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\devices\MIMXRT1052\system_MIMXRT1052.c"
Error while running C/C++ Compiler

Total number of errors: 21
Total number of warnings: 0

Please provide a solution for this.

Thanks and Regards

Rizwan Syed

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
858 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi rizwaz,

where did you get the examples? Dis you get them from here? Welcome | MCUXpresso SDK Builder 

is it just one project which is not working?

I looks like the project is located in a different path than it should be. Please download the SDK and place it in any folder

E.g. inside C:/NXP/imxrt-sdk and do not change its structure.


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
859 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi rizwaz,

where did you get the examples? Dis you get them from here? Welcome | MCUXpresso SDK Builder 

is it just one project which is not working?

I looks like the project is located in a different path than it should be. Please download the SDK and place it in any folder

E.g. inside C:/NXP/imxrt-sdk and do not change its structure.


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply