Immediately stop of eLCDIF data transfer.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Immediately stop of eLCDIF data transfer.

1,355 次查看
ko-hey
Senior Contributor II

Hi all

I'm reading  IMX7DRM Rev. 0.1, 08/2016 and have question about eLCDIF in MPU interface.

Q1.

I want to transfer data and commands between the SoC via the eLCDIF in MPU interface as fast as possible.
I think the only way is to use higher DISPLAY_CLK.
Does someone have any idea ?

Q2

I want to immediately stop the transfer data.
I speculated that it'll stop when user set SFTRST field of LCDIFx_RLn register.
Am I correct ?
Also do you have any concern for that use case ?

Q2-1

If user can stop the data transfer with setting "1" to SFTRST, what happens to the output ports such as LCD command and data ?
Does the port keep Pull-up, Pull-down or Hi-Z ?

Q2-2

If Q2 is no, do you have any idea to stop the transfer data immediately ?

Ko-hey

标签 (3)
0 项奖励
回复
4 回复数

1,282 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

according to sect.13.2.4.6 MPU Interface i.MX7D RM

http://cache.nxp.com/files/32bit/doc/ref_manual/IMX7DRM.pdf 

"The current transfer can be cancelled/aborted if the RUN bit is manually made 0."

Seems this could be done also with SFTRST, output ports become idle as in Figure 13-13,

pad settings (Pull-up, Pull-down or Hi-Z) stay unchanged.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,282 次查看
ko-hey
Senior Contributor II

Igor

Thank you for reply.

I understand that user should set RUN field to "0” manually if user want to cancel/abort the transfer and the output ports are no change after the transfer cancelled.

How about Q1 ?

Do you have any idea for it ?

Ko-hey

0 项奖励
回复

1,282 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

for Q1 I think your idea is right.

Best regards
igor

0 项奖励
回复

1,282 次查看
ko-hey
Senior Contributor II

Hi Igor

Thank you.

Ko-hey

0 项奖励
回复