Image up scaling on I.MX6 SOLO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Image up scaling on I.MX6 SOLO

Jump to solution
1,050 Views
JHY
Contributor IV

Is it possble to resize 1024x768 video to 1920x1080 on I.MX6 SOLO using IPU?

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
957 Views
igorpadykov
NXP Employee
NXP Employee

Hi JHY

for upsizing the IPU IC resizing output size is resricted to 1024x1024 pixels.

If a larger frame is required,  the resizing should be done in several blocks,

so that the size of each block does not exceed the above limitations.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
958 Views
igorpadykov
NXP Employee
NXP Employee

Hi JHY

for upsizing the IPU IC resizing output size is resricted to 1024x1024 pixels.

If a larger frame is required,  the resizing should be done in several blocks,

so that the size of each block does not exceed the above limitations.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply