Image up scaling on I.MX6 SOLO

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Image up scaling on I.MX6 SOLO

ソリューションへジャンプ
1,485件の閲覧回数
JHY
Contributor IV

Is it possble to resize 1024x768 video to 1920x1080 on I.MX6 SOLO using IPU?

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
1,392件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi JHY

for upsizing the IPU IC resizing output size is resricted to 1024x1024 pixels.

If a larger frame is required,  the resizing should be done in several blocks,

so that the size of each block does not exceed the above limitations.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,393件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi JHY

for upsizing the IPU IC resizing output size is resricted to 1024x1024 pixels.

If a larger frame is required,  the resizing should be done in several blocks,

so that the size of each block does not exceed the above limitations.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信