Image sensor for iMX6Ull

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Image sensor for iMX6Ull

1,470件の閲覧回数
paultran
Contributor I

hi

please help to provide what image sensor that iMX6ULL support in case SW (driver, kernel....)

with HW connection will follow CSI IP on eval board. 

our application is camera detect QR code, bard code (like 1D, 2D scanner), so image sensor resolution can be around 1MP. 

Please any experiment about that help to advise 

thanks 

ラベル(3)
タグ(3)
0 件の賞賛
返信
2 返答(返信)

1,285件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Paul

please look on

How to use OV5640 with i.MX 6UltraLite EVK - i.MXDev Blog 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,285件の閲覧回数
almaz1c
Contributor III

Hi!

Does OV5640 camera module included in i.MX6UltraLite Evaluation Kit | NXP  ?

If no can someone point me how can I order it please?

0 件の賞賛
返信