Image copying on SABRE-SD

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Image copying on SABRE-SD

975 次查看
kapilkumar
Contributor III

Hello Friends,

I am trying to bring up SABRE-SD platform board. while using dd utility, in the android user guide, it has been asked to copy u-boot.imx. suppose, i want to use MFGTools v2 , then, which image file i will keep in the profiles folder of MFGTool : u-boot.imx or u-boot.bin ???

Best Regards & Thank You

Kapil Kumar.

标签 (1)
0 项奖励
回复
2 回复数

932 次查看
art
NXP Employee
NXP Employee

For MFGtool, you have to use the u-boot.bin image.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

932 次查看
kapilkumar
Contributor III

HI Artur

Okay. Then, in what ways u-boot.bin is different from u-boot.imx???

Have a great Day...

Kapil Kumar

0 项奖励
回复