Image Rotation and Alpha Blending examples for i.MX233 PXP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Image Rotation and Alpha Blending examples for i.MX233 PXP

ソリューションへジャンプ
1,837件の閲覧回数
RobMauro
Contributor II

We want to use i.MX233 PXP for image rotation and alpha-blending.

Does anyone have examples of such PXP usage in C code?

ラベル(2)
0 件の賞賛
返信
1 解決策
1,412件の閲覧回数
Yuri
NXP Employee
NXP Employee

  As for rotation - please look at Re: i.MX23 CPU - Display Rotate function not working

Also, please refer to the Linux PXP driver ; the PxP driver source code is located in
drivers/media/video/mxs_pxp.c and drivers/media/video/mxs_pxp.h.

   The PXP driver may be used via V4L2.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,413件の閲覧回数
Yuri
NXP Employee
NXP Employee

  As for rotation - please look at Re: i.MX23 CPU - Display Rotate function not working

Also, please refer to the Linux PXP driver ; the PxP driver source code is located in
drivers/media/video/mxs_pxp.c and drivers/media/video/mxs_pxp.h.

   The PXP driver may be used via V4L2.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信