Hi,
I used kernel 4.6 running on iMx6 dual core platform and found some etnavi drivers error messages like “etnaviv-gpu 2204000.gpu: hw init failed: -6”, “etnaviv-gpu 2204000.gpu: Ignoring GPU with VG and FE2.0”.
Please see the related commit info below.
http://kernel.suse.com/cgit/kernel/commit/?h=v4.5-rc2&id=b98c66887ee1aec661dcb88fe17399d5d112ed98
Is there's anyone can comment on this ?
[ 1.948713] [drm] Initialized drm 1.1.0 20060810
[ 1.967629] etnaviv gpu-subsystem: bound 134000.gpu (ops gpu_ops)
[ 1.973886] etnaviv gpu-subsystem: bound 130000.gpu (ops gpu_ops)
[ 1.980077] etnaviv gpu-subsystem: bound 2204000.gpu (ops gpu_ops)
[ 1.986307] etnaviv-gpu 134000.gpu: model: GC320, revision: 5007
[ 2.025242] etnaviv-gpu 130000.gpu: model: GC2000, revision: 5108
[ 2.067795] etnaviv-gpu 2204000.gpu: model: GC355, revision: 1215
[ 2.073942] etnaviv-gpu 2204000.gpu: Ignoring GPU with VG and FE2.0
[ 2.080230] etnaviv-gpu 2204000.gpu: hw init failed: -6
drivers/gpu/drm/etnaviv/etnaviv_gpu.c
int etnaviv_gpu_init(struct etnaviv_gpu *gpu)
{
int ret, i;
struct iommu_domain *iommu;
enum etnaviv_iommu_version version;
bool mmuv2;
ret = pm_runtime_get_sync(gpu->dev);
if (ret < 0)
return ret;
etnaviv_hw_identify(gpu);
if (gpu->identity.model == 0) {
dev_err(gpu->dev, "Unknown GPU model\n");
ret = -ENXIO;
goto fail;
}
/* Exclude VG cores with FE2.0 */
if (gpu->identity.features & chipFeatures_PIPE_VG &&
gpu->identity.features & chipFeatures_FE20) {
dev_info(gpu->dev, "Ignoring GPU with VG and FE2.0\n");
ret = -ENXIO;
goto fail;
}
…
}
drivers/gpu/drm/etnaviv/etnaviv_drv.c
static void load_gpu(struct drm_device *dev)
{
struct etnaviv_drm_private *priv = dev->dev_private;
unsigned int i;
for (i = 0; i < ETNA_MAX_PIPES; i++) {
struct etnaviv_gpu *g = priv->gpu[i];
if (g) {
int ret;
ret = etnaviv_gpu_init(g);
if (ret) {
dev_err(g->dev, "hw init failed: %d\n", ret);
priv->gpu[i] = NULL;
}
}
}
}