If the LVDS-PCIE-SATA-DSI-USB HOST not to use,how to design the pin of power or REXT?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

If the LVDS-PCIE-SATA-DSI-USB HOST not to use,how to design the pin of power or REXT?

453 Views
翔李
Contributor IV

hi,

I am going to reduce the PCB-size and bom of the design,so I will delete all the parts if they are not useful.

1:If I don't use USB HOST,do the USB_H1_VBUS need to power by 5V?

2:If I don't use LVDS0 and LVDS1,do the NVCC_LVDS2P5 pin need to power?

3:If I don't use SATA-PCIE-DSI-LVDS,do the their REXT pins need to connect  Resistor?

4:how to use the pin of test_mode,tamper,onoff? Can I float these pins if I do not use them?

By the way,can u give me the file of how to deal for unuse pins? 

thanks.

pastedImage_1.png

pastedImage_5.pngpastedImage_2.pngpastedImage_3.pngpastedImage_4.png

0 Kudos
1 Reply

353 Views
igorpadykov
NXP Employee
NXP Employee

Hi 翔李 

please look at sect.2.8 Unused analog interfaces i.MX6 System Development User’s Guide

https://www.nxp.com/docs/en/user-guide/IMX6DQ6SDLHDG.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos