If mx6sx is a spi slave, is it possible to use SS pin as wake up source when it's suspend to ram state?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

If mx6sx is a spi slave, is it possible to use SS pin as wake up source when it's suspend to ram state?

1,305 Views
alex_park
Contributor II

Hello, I'm currently using imx6sx as a slave spi. (kernel 3.10.53 + patch spi slave (see attachment) )

while imx6sx is in suspend to ram state, I want to wake it up by QSPI1B_SSO_B from some external spi master device.

Is anybody who knows how to do it ?

pastedImage_2.png

Labels (3)
5 Replies

1,068 Views
igorpadykov
NXP Employee
NXP Employee

Hi MINKYU

ecspi module has not wake capabilities as for example uart, so

one can configure ss pin as gpio for wake, after resuming return it as ss function.

One can look at example "wakeup-gpios" in imx6sx-sabreauto.dts

linux-2.6-imx.git - Freescale i.MX Linux Tree 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,068 Views
alex_park
Contributor II

Hello igorpadykov

is pin below available for wakeup source?

My engineer tried to do with that pin and it seems it doesn't work.

Please help me.

<MX6SX_PAD_QSPI1B_SS0_B__GPIO4_IO_30>

.

.

.

&ecspi3 {
fsl,spi-num-chipselects = <1>;
cs-gpios = <&gpio4 30 0>;
pinctrl-names = "default";
wakeup-gpios = <&gpio4 30 0>;

.

.

.

0 Kudos

1,068 Views
igorpadykov
NXP Employee
NXP Employee

Hi MINKYU

I do not think that spi driver supports SS pin as wake up.

Please try to use it as separate (not as part of spi) gpio wake source.

Best regards
igor

0 Kudos

1,068 Views
alex_park
Contributor II

Hello igorpadykov‌ Thanx for quick response.

My attempt was to switch the ss pin to gpio when imx6 is in suspend to ram (echo mem> / sys / power / state), and switch to ss pin when resume.
Is not it the same context to use as a separate gpio you said?

0 Kudos

1,068 Views
igorpadykov
NXP Employee
NXP Employee

Hi MINKYU

I think you are right, but these codes are not implemented in existing driver,

you can try to debug it. In general, nxp has special service for helping with porting drivers

NXP Professional Services|NXP 

Best regards
igor

0 Kudos