If i.MX7 is used with 16bits memory bus width

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

If i.MX7 is used with 16bits memory bus width

跳至解决方案
1,671 次查看
george
Senior Contributor II

Dear all,

We use one DDR3L.
DCD for them was generated using Aid Script.
In the test using MCIMX7SABRE, it work fine.

From now on, we will design original PCB.
Is termination required though following pins are not used?

  • DRAM_CS1_B
  • DRAM_SDCKE1
  • DRAM_DATA[16:31]
  • DRAM_SDQS2_P
  • DRAM_SDQS2_N
  • DRAM_SDQS3_P
  • DRAM_SDQS3_N
  • DRAM_DQM2
  • DRAM_DQM3

I think that outputs are NC.
Is Pull-up/down required for inputs, such as DQS?

Best Regards,

George

标签 (2)
1 解答
1,469 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  yes, the mentioned unused DRAM signals may be left floating.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

4 回复数
1,470 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  yes, the mentioned unused DRAM signals may be left floating.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,469 次查看
george
Senior Contributor II

Dear Yuri,

Are these all the pins (DQS is also included) that I showed?

Thanks,

George

0 项奖励
回复
1,469 次查看
Yuri
NXP Employee
NXP Employee

Yes, all the mentioned signals :

  • DRAM_CS1_B
  • DRAM_SDCKE1
  • DRAM_DATA[16:31]
  • DRAM_SDQS2_P
  • DRAM_SDQS2_N
  • DRAM_SDQS3_P
  • DRAM_SDQS3_N
  • DRAM_DQM2
  • DRAM_DQM3

~Yuri.

1,469 次查看
george
Senior Contributor II

Thanks.

0 项奖励
回复