Idle state of RTS in RS-485 mode on IMX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Idle state of RTS in RS-485 mode on IMX6

1,967 Views
jeff_hunsinger
Contributor I

I activated RS-485 mode on the IMX6UL using UART7 and the RTS pin transitions as expected when I have the port open. However, when I close the port, the pin goes high even though I have it configured to be low when not transmitting. There is an external pull-up on this pin because it is used to configure the IMX6UL at reset.

Is there a way to have the pin drive low by default when the UART is not open?

I am using the LCD_DATA06_DTE_RTS pin with the UART in DCE mode.

I use the following to enable RS-485 mode in the Linux driver:

rs485conf.flags |= SER_RS485_ENABLED;
rs485conf.flags |= (SER_RS485_RTS_ON_SEND);
rs485conf.flags &= ~(SER_RS485_RTS_AFTER_SEND);

ioctl(fd, TIOCSRS485, &rs485conf);

Thank you,

Jeff

Tags (1)
0 Kudos
Reply
1 Reply

1,591 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jeff

one can try to change behavior adding codes in driver configuring

that pad as gpio, with low state by default when the UART is not open.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply