Hi,
I signed Linux kernel with HAB by following mx8m_secure_boot.txt and trying to authenticate the signing by,
hab_auth_img <Load Address> <Image Size> <IVT Offset>
This returns "Invalid IVT Structure" Error.
u-boot=> hab_auth_img
hab_auth_img - authenticate image via HAB
Usage:
hab_auth_img addr length ivt_offset
addr - image hex address
length - image hex length
ivt_offset - hex offset of IVT in the image
u-boot=> hab_auth_img 0x40480000 0x1C21020 0x1C21000
hab fuse not enabled
Authenticate image from DDR location 0x40480000...
bad magic magic=0xd5 length=0x4828 version=0x45
bad length magic=0xd5 length=0x4828 version=0x45
Error: Invalid IVT structure
Allowed IVT structure:
IVT HDR = 0x4X2000D1
IVT ENTRY = 0xXXXXXXXX
IVT RSV1 = 0x0
IVT DCD = 0x0
IVT BOOT_DATA = 0xXXXXXXXX
IVT SELF = 0xXXXXXXXX
IVT CSF = 0xXXXXXXXX
IVT RSV2 = 0x0
I want to know,
Thanks in advance.
解決済! 解決策の投稿を見る。
To answer my own questions:
The correct way to use hab_auth_img is as follows,
u-boot=> hab_auth_img <loadaddr> <img_size + ivt_size> <img_size>
1. loadaddr
(in uboot console)
u-boot=> printenv loadaddr
2. img_size
(in host pc's terminal)
~ hexdump -e '/4 "%X"' -s 12 -n <path_to_kernel_Image>
3. ivt_size - 0x20 (fixed)
To answer my own questions:
The correct way to use hab_auth_img is as follows,
u-boot=> hab_auth_img <loadaddr> <img_size + ivt_size> <img_size>
1. loadaddr
(in uboot console)
u-boot=> printenv loadaddr
2. img_size
(in host pc's terminal)
~ hexdump -e '/4 "%X"' -s 12 -n <path_to_kernel_Image>
3. ivt_size - 0x20 (fixed)
question about solution...
hexdump: invalid number '/media/my-kernel-image'
So I do :
hexdump -e '/4 "%X"' -s 12 -n my-kernel-image
but hexdump says:
hexdump: invalid number 'my-kernel-image'.
Posted solution has some issues.
THanks
nevermind... The posted solution should read:
hexdump -e '/4 "%X"' -s 12 -n 8 <kernel-image>
Or you can do :
echo 0x$(echo `od -t x4 -j0x10 -N4 <kernel-image> ` | cut -d' ' -f2)
Hi kanimozhi_t
one can look at below links which may help
https://community.nxp.com/t5/i-MX-Processors/hab-auth-img-problem/m-p/1032545
https://boundarydevices.com/high-assurance-boot-hab-i-mx8m-edition/
Best regards
igor