Hi all
I want to confirm a connection of i.MX6SL with LCD.
My customer want to use eLCDIF in ITU-R BT.656 Digital Video Interface.
So we read section 21.4.11 and 21.4.12 in reference manual but can not understand it.
We understand that they need to connect only data and clock.
However, we can't figure out that which pin can we use as a clock signal.
Which pin can we use ?
i.MX 6SoloLite Applications Processor Reference Manual
http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SLRM.pdf
Ko-hey
已解决! 转到解答。
Hi Ko-hey
it is LSD_RS (CCIR_CLK) as depicted in Table 21-4.
Pin use in DOTCLK Mode and DVI Mode
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Ko-hey
it is LSD_RS (CCIR_CLK) as depicted in Table 21-4.
Pin use in DOTCLK Mode and DVI Mode
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------