Hi all
I want to confirm a connection of i.MX6SL with LCD.
My customer want to use eLCDIF in ITU-R BT.656 Digital Video Interface.
So we read section 21.4.11 and 21.4.12 in reference manual but can not understand it.
We understand that they need to connect only data and clock.
However, we can't figure out that which pin can we use as a clock signal.
Which pin can we use ?
i.MX 6SoloLite Applications Processor Reference Manual
http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SLRM.pdf
Ko-hey
解決済! 解決策の投稿を見る。
Hi Ko-hey
it is LSD_RS (CCIR_CLK) as depicted in Table 21-4.
Pin use in DOTCLK Mode and DVI Mode
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Ko-hey
it is LSD_RS (CCIR_CLK) as depicted in Table 21-4.
Pin use in DOTCLK Mode and DVI Mode
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor
Thank you for reply.
In other words, we should use LCD_DOTCLK pin to provide a clock.
Is it correct ?
Ko-hey
Hi Ko-hey
one needs to use signal LCD_RS, pad LCD_VSYNC(ALT2)
check Table 4-1. Pin Assignments i.MX6SL RM
Best regards
igor
Hi Igor
Thank you for your support.
Ko-hey