IT6263 LVDS to HDMI board initialize fail

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IT6263 LVDS to HDMI board initialize fail

2,200件の閲覧回数
xiaoqiang81
Contributor I

I am using NXP's LVDS conversion HDMI board to drive the computer screen on evaluation board MCIMX8QM-CPU. The CPU is i.MX 8 QuadMax. I think that driver is android_build\vendor\nxp-opensource\kernel_imx\drivers\gpu\drm\bridge\it6263.c . The code failed on regmap_write of it6263_probe.
1.Could you please tell me which configuration is required.
2.I need to insert miniSAS cable into which slot on the MCIMX8QM-CPU board.
3.If I only want to send control commands to IT6263, whether need to plug the HDMI of computer's screen to the it6263.
4.Could you tell me the connection relation of LVDS and IT6263 which used miniSAS cable to connect? Because I don't have a PCB

0 件の賞賛
返信
1 返信

2,190件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

You need to change the dtb file to match the screen you are using.

0 件の賞賛
返信