I am using NXP's LVDS conversion HDMI board to drive the computer screen on evaluation board MCIMX8QM-CPU. The CPU is i.MX 8 QuadMax. I think that driver is android_build\vendor\nxp-opensource\kernel_imx\drivers\gpu\drm\bridge\it6263.c . The code failed on regmap_write of it6263_probe.
1.Could you please tell me which configuration is required.
2.I need to insert miniSAS cable into which slot on the MCIMX8QM-CPU board.
3.If I only want to send control commands to IT6263, whether need to plug the HDMI of computer's screen to the it6263.
4.Could you tell me the connection relation of LVDS and IT6263 which used miniSAS cable to connect? Because I don't have a PCB