ISO/IEC 5230:2020 certification confirmation for i.MX software.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ISO/IEC 5230:2020 certification confirmation for i.MX software.

ソリューションへジャンプ
2,691件の閲覧回数
Yoshidaj
Contributor I

Customer request NXP to confirm for the certification ISO/IEC 5230:2020 ( OSS Compliance ).

We cannot confirm that the NXP i.MX Linux/ Android BSP was certified for OSS compliance, would you kindly let us know the NXP software certification status for OSS ?

*The attached file is OSS leaflet.

If NXP doesn't have its certification, also let us know the plan to acquire its certification.

ラベル(1)
0 件の賞賛
返信
1 解決策
2,655件の閲覧回数
nxf63675
NXP TechSupport
NXP TechSupport

Hi @Yoshidaj,

 

Please open a case as the info can't be shared on the community, mention this community thread and I will answer there.

 

Regards,

Israel.

元の投稿で解決策を見る

2 返答(返信)
2,656件の閲覧回数
nxf63675
NXP TechSupport
NXP TechSupport

Hi @Yoshidaj,

 

Please open a case as the info can't be shared on the community, mention this community thread and I will answer there.

 

Regards,

Israel.

2,642件の閲覧回数
Yoshidaj
Contributor I

Dear Israel.

Thanks for your reply. We also put question on TIC and check it.

Yoshida

0 件の賞賛
返信