IRQ Driver irq-imx-gpcv2.c

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IRQ Driver irq-imx-gpcv2.c

1,622 Views
viniciusmaciel
Contributor II

Hi,

I was wondering why irq-imx-gpcv2.c driver is not used in current imx kernel: kernel/4.1-2.0.x-imx/drivers/irqchip/Makefile. Which driver is used to manage interruptions in kernel?

Thanks,

Vini

Labels (3)
Tags (3)
0 Kudos
Reply
1 Reply

1,462 Views
igorpadykov
NXP Employee
NXP Employee

Hi Vini

please check Chapter 3 Machine-Specific Layer (MSL)

attached Linux Manual and below thread

difference between Yocto Community BSP and Freescale BSP Release 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply