IR receiver on i.MX8M mini EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IR receiver on i.MX8M mini EVK

Jump to solution
2,019 Views
Kazuma_Sasaki
Senior Contributor I

The IR receiver (P/N IRM-V538M3/TR1) implemented on i.MX8M mini EVK.

This module connect to GPIO1_IO13 of i.MX8MM. However, I could not find any description to use this module into iMX8MMEVKUG and latest Linux BSP documents (L4.14.98_2.0.0_ga)

How do I use this module with linux BSP?

I suppose NXP will support lIRC later. is it right?

Copy from iMX8MMEVKHUG.pdf.

pastedImage_2.png

Best Regards,

Kazuma Sasaki.

Labels (1)
0 Kudos
Reply
1 Solution
1,714 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

The IR Receiver on the i.MX8M Mini EVK board is intended for IR Remote Receiving. GPIO1_IO13 will be assigned as IO input, and will work with INT mechanism and internal Timer to decode different IR Remote protocol, such as RC-5, RC-6, ans so on. Normally, this code shall be built by customers themselves.

Have a nice day

Rita

View solution in original post

0 Kudos
Reply
4 Replies
1,715 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

The IR Receiver on the i.MX8M Mini EVK board is intended for IR Remote Receiving. GPIO1_IO13 will be assigned as IO input, and will work with INT mechanism and internal Timer to decode different IR Remote protocol, such as RC-5, RC-6, ans so on. Normally, this code shall be built by customers themselves.

Have a nice day

Rita

0 Kudos
Reply
1,714 Views
eric_kang
Contributor II

Hi Rita,

Some peoples are made questions for the valid IR Control and the IR Software.

Could you give the informations for the valid IR Control and the IR Software?

Best Regards,

Eric.

0 Kudos
Reply
1,714 Views
sam_wu
Contributor I

Hi Rita,

Where can I find this IR software source code in the linux BSP ? Thank you.

Best Regards,
Sam

0 Kudos
Reply
1,714 Views
Kazuma_Sasaki
Senior Contributor I

Hi Rita,

I appreciate your support. I see.

NXP has already validated IR receiver? because, current schematics is here.

I think we need rework D709 to receive signals from U701.

pastedImage_1.png

Best Regards,

Kazuma Sasaki.

0 Kudos
Reply