IPU2 CS1 1080p60 YUY2 16-bit capture over i.MX6QDL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IPU2 CS1 1080p60 YUY2 16-bit capture over i.MX6QDL

1,561 次查看
jeromebolduc
Contributor III

Hi,

We already designed a product using iMX6 Dual / Quad and this one is able to capture 1080p30 HDMI video using an ADV7612. Parallel bus from ADV7612 is sent to IPU1_CSI0 of iMX6. ADV7612 is working DDR (PIXCLK at 2 x 74.25MHz) with 8-bit pixel bus @ 1080p30.
We are using a Variscite VAR-SOM-MX6 and we would like to be able to do 1080p60 using same module.

We have found that Variscite VAR-SOM-MX6 exposes 20-bit CSI port of IPU2_CSI1 compared to IPU1_CS0 which exposes only 12-bits. We cannot do 1080p60 with that interface. We would like to be able to put the ADV7612 parallel port 16-bit (8-bit luma and 8-bit chroma) with PIXCLK at 148.5MHz for 1080p60.

Is it achievable with iMX6 Quad / Dual? Seems like in the datasheet CSI parallel can work up to 240MHz.

We base our driver for ADV7612 on the ov564x driver.

I am trying to modify the imx6q-var-som-vsc.dts file by adding this:

&i2c1 {
	clock-frequency = <100000>;
	pinctrl-names = "default";
	pinctrl-0 = <&pinctrl_i2c1_2>;
	status = "okay";

	ov564x: ov564x@3c {
		compatible = "ovti,ov564x";
		reg = <0x3c>;
		pinctrl-names = "default";
		pinctrl-0 = <&pinctrl_ipu1_2>;
		clocks = <&clks IMX6QDL_CLK_CKO>;
		clock-names = "csi_mclk";
		//DOVDD-supply = <&vgen4_reg>; /* 1.8v */
		//AVDD-supply = <&vgen3_reg>;  /* 2.8v, on rev C board is VGEN3,
		//				on rev B board is VGEN5 */
		//DVDD-supply = <&vgen2_reg>;  /* 1.5v*/
		//pwn-gpios = <&gpio1 16 1>;   /* active low: SD1_DAT0 */
		//rst-gpios = <&gpio1 17 0>;   /* active high: SD1_DAT1 */
		csi_id = <1>;
		mclk = <24000000>;
		mclk_source = <0>;
	};
};


We also add this pin-ctrl to iomuxc

pinctrl_ipu1_2: ipu1grp-2 { /* parallel camera */
	fsl,pins = <
		MX6QDL_PAD_EIM_DA9__IPU2_CSI1_DATA00 0x10000
		MX6QDL_PAD_EIM_DA8__IPU2_CSI1_DATA01 0x10000
		MX6QDL_PAD_EIM_DA7__IPU2_CSI1_DATA02 0xb0b1
		MX6QDL_PAD_EIM_DA6__IPU2_CSI1_DATA03 0xb0b1
		MX6QDL_PAD_EIM_DA5__IPU2_CSI1_DATA04 0xb0b1
		MX6QDL_PAD_EIM_DA4__IPU2_CSI1_DATA05 0xb0b1
		MX6QDL_PAD_EIM_DA3__IPU2_CSI1_DATA06 0xb0b1
		MX6QDL_PAD_EIM_DA2__IPU2_CSI1_DATA07 0xb0b1
		MX6QDL_PAD_EIM_DA1__IPU2_CSI1_DATA08 0xb0b1
		MX6QDL_PAD_EIM_DA0__IPU2_CSI1_DATA09 0xb0b1
		MX6QDL_PAD_EIM_EB1__IPU2_CSI1_DATA10 0x10000
		MX6QDL_PAD_EIM_EB0__IPU2_CSI1_DATA11 0x10000
		MX6QDL_PAD_EIM_A17__IPU2_CSI1_DATA12 0xb0b1
		MX6QDL_PAD_EIM_A18__IPU2_CSI1_DATA13 0xb0b1
		MX6QDL_PAD_EIM_A19__IPU2_CSI1_DATA14 0xb0b1
		MX6QDL_PAD_EIM_A20__IPU2_CSI1_DATA15 0xb0b1
		MX6QDL_PAD_EIM_A21__IPU2_CSI1_DATA16 0xb0b1
		MX6QDL_PAD_EIM_A22__IPU2_CSI1_DATA17 0xb0b1
		MX6QDL_PAD_EIM_A23__IPU2_CSI1_DATA18 0xb0b1
		MX6QDL_PAD_EIM_A24__IPU2_CSI1_DATA19 0xb0b1
		MX6QDL_PAD_EIM_DA10__IPU2_CSI1_DATA_EN 0xb0b1
		MX6QDL_PAD_EIM_DA11__IPU2_CSI1_HSYNC 0x10000
		MX6QDL_PAD_EIM_DA12__IPU2_CSI1_VSYNC 0x10000
		MX6QDL_PAD_EIM_A16__IPU2_CSI1_PIXCLK 0xb0b1
	>;
};


In the imx6qdl-var-som.dtsi file, we changed this node:

v4l2_cap_0 {
	compatible = "fsl,imx6q-v4l2-capture";
	ipu_id = <1>;
	csi_id = <1>;
	mclk_source = <0>;
	status = "okay";
};


When booting our Linux, here is what we get when doing dmesg | grep ov:

[    0.119680] cpuidle: using governor ladder
[    0.149678] cpuidle: using governor menu
[    3.240495] sit: IPv6 over IPv4 tunneling driver
[    3.834873] EXT4-fs (mmcblk1p2): recovery complete
[    4.938636] ov564x 0-003c: Error applying setting, reverse things back
[    4.944876]    ov5640_probe
[    5.052599] ov564x 0-003c: Error applying setting, reverse things back
[    5.072072] ov564x 0-003c: set io voltage ok
[    5.085775] ov564x 0-003c: set core voltage ok
[    5.090943] ov564x 0-003c: set analog voltage ok
[    5.203270] camera ov5640 is found
[    5.953170] ov5640: unsupported bit mode 0
[    5.969493] EXT4-fs (mmcblk0p1): recovery complete


How do we successfully change IPU_ID and CSI_ID in kernel in order to use the IPU2_CSI1 interface?

Thanks,

Jérôme

0 项奖励
回复
7 回复数

1,491 次查看
jeromebolduc
Contributor III

I should be able to capture YUV 1920x1080p 60fps image like this one:

good-pattern.png

However, I am capturing something like this:

bad-pattern.png

The video feed goes from top to bottom on constant speed without stablizing.

REG 0x2a38000 = 0x0400cb00

Seems like chroma is seen like luma. 

In ipu_capture.c, I need to set this in order to capture 16-bit.

cfg_param.data_fmt = CSI_SENS_CONF_DATA_FMT_BAYER;

How to tell the IPU that incoming data is YUV?

Thanks!

Jerome

0 项奖励
回复

1,487 次查看
joanxie
NXP TechSupport
NXP TechSupport

did you try the patch or not? still get the error with this patch?

0 项奖励
回复

1,534 次查看
joanxie
NXP TechSupport
NXP TechSupport

you should connect ADV7612  to mipi csi, right? refer to the reference manual,

The maximum bandwidth of the interface is as follows:
• 200Mhz for 4 data lanes configuration (800Mbps/lane, 400MByte/sec)
• 187.5Mhz for 3 data lanes configuration (1000Mbps/lane, 375MByte/sec)
• 125Mhz for 2 data lanes configuration (1000Mbps/lane, 250MByte/sec )
• 62.5Mhz for 1 data lane configuration (1000Mbps/lane, 125Mbyte/sec)

and if you use RGB565 over 16 bit format, I think you need to enable 4 data lans for this, for 16bits capture, you can refer to the enclosed patch for reference

0 项奖励
回复

1,528 次查看
jeromebolduc
Contributor III

Hi,

ADV7612 output is parallel, not MIPI-CSI.

How to enable 16-bit YUY2 parallel capture on kernel?

Jérôme

0 项奖励
回复

1,506 次查看
joanxie
NXP TechSupport
NXP TechSupport

 refer to the data sheet, YCbCr, 16 bits—Supported as a “generic-data” input, I send the patch to you for 16bits generic data capture, you can refe to it,

0 项奖励
回复

1,502 次查看
jeromebolduc
Contributor III

This patch is already applied to our BSP.

I configured kernel to capture IPU_PIX_FMT_GENERIC_16.

How to tell iMX6 this generic capture is YUYV? Pixel mapping is not correct right now.

Regards,

Jérôme

0 项奖励
回复

1,548 次查看
jeromebolduc
Contributor III

Any updates on this?

0 项奖励
回复