IPU examples on yocto dora_3.10.17-1.0.0_GA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IPU examples on yocto dora_3.10.17-1.0.0_GA

Jump to solution
3,008 Views
haizhouli
Contributor III

Hi all,

I am new to IMX6, I am working on the IPU now.

I got examples from https://github.com/rogeriorps/ipu-examples

My system build is from yocto dora_3.10.17-1.0.0_GA fsl-image-fb.

I tried to cross compile the resizing example based on this build.  I saw this message:


-----------------------------------------

res_ex1.c: In function 'fmt_to_bpp':

res_ex1.c:49:22: error: 'IPU_PIX_FMT_YUV444P' undeclared (first use in this function)

                 case IPU_PIX_FMT_YUV444P:

                      ^

res_ex1.c:49:22: note: each undeclared identifier is reported only once for each function it appears in

res_ex1.c: In function 'main':

res_ex1.c:76:18: error: storage size of 'task' isn't known

  struct ipu_task task;

                  ^

res_ex1.c:129:22: error: 'IPU_ALLOC' undeclared (first use in this function)

  ret = ioctl(fd_ipu, IPU_ALLOC, &task.input.paddr);

                      ^

res_ex1.c:181:22: error: 'IPU_QUEUE_TASK' undeclared (first use in this function)

  ret = ioctl(fd_ipu, IPU_QUEUE_TASK, &task);

                      ^

res_ex1.c:212:17: error: 'IPU_FREE' undeclared (first use in this function)

   ioctl(fd_ipu, IPU_FREE, &task.output.paddr);

--------------------------------------------

Are those examples compatible with the latest yocto build?

If not, are there some examples for latest build?

Thanks!

Labels (2)
1 Solution
1,205 Views
rogerio_silva
NXP Employee
NXP Employee

Hi haizhouli

I just updated the repository with 2 patches to fix the Makefile and configure files and also to update the Readme file. It's now building with kernel 3.10.17 + Yocto.

If you have problems to build or in some example code, please let me know.

Best Regards,

Rogerio

View solution in original post

0 Kudos
7 Replies
1,205 Views
rogerio_silva
NXP Employee
NXP Employee

Hi haizhouli,

These examples was made with kernel 3.0.35.

I'll test (and fix if needed) with kernel 3.10.17 and let you know.

Rgds

Rogerio

0 Kudos
1,205 Views
haizhouli
Contributor III

Thank you so much for the reply!

Based on the location of toolchain in the the README.md file, it seems you build the example based on LTIB, is that right?

Since these examples were tested on 3.0.35, I do have one yocto build is based on 3.0.35-4.1.0.  I just did another test, here are my steps:

This yocto build is based on   fsl-image-gui

I went to my virtual machine which has LTIB build, based on Ubuntu 10.4.  I copied the linaro toolchain from LTIB to the exact location required in your README.md

I downloaded automake 1.11 and installed it into the /usr/share/

~$ ./configure --host=arm-none-linux-gnueabi --target=mx6 --prefix=/home/hli/fsl-community-bsp/build/tmp/work/imx6qsabresd-poky-linux-gnueabi/fsl-tp-image/1.0-r0/rootfs

./configure: line 2197: S: command not found

checking for a BSD-compatible install... /usr/bin/install -c

checking whether build environment is sane... yes

checking for arm-none-linux-gnueabi-strip... arm-none-linux-gnueabi-strip

checking for a thread-safe mkdir -p... /bin/mkdir -p

checking for gawk... gawk

checking whether make sets $(MAKE)... yes

checking for arm-none-linux-gnueabi-gcc... arm-none-linux-gnueabi-gcc

checking whether the C compiler works... yes

checking for C compiler default output file name... a.out

checking for suffix of executables...

checking whether we are cross compiling... yes

checking for suffix of object files... o

checking whether we are using the GNU C compiler... yes

checking whether arm-none-linux-gnueabi-gcc accepts -g... yes

checking for arm-none-linux-gnueabi-gcc option to accept ISO C89... none needed

checking for style of include used by make... GNU

checking dependency style of arm-none-linux-gnueabi-gcc... gcc3

checking how to run the C preprocessor... arm-none-linux-gnueabi-gcc -E

checking for grep that handles long lines and -e... /bin/grep

checking for egrep... /bin/grep -E

checking for ANSI C header files... yes

checking for sys/types.h... yes

checking for sys/stat.h... yes

checking for stdlib.h... yes

checking for string.h... yes

checking for memory.h... yes

checking for strings.h... yes

checking for inttypes.h... yes

checking for stdint.h... yes

checking for unistd.h... yes

checking fcntl.h usability... yes

checking fcntl.h presence... yes

checking for fcntl.h... yes

checking for stdint.h... (cached) yes

checking for stdlib.h... (cached) yes

checking for string.h... (cached) yes

checking sys/ioctl.h usability... yes

checking sys/ioctl.h presence... yes

checking for sys/ioctl.h... yes

checking for unistd.h... (cached) yes

checking for size_t... yes

checking for stdlib.h... (cached) yes

checking for unistd.h... (cached) yes

checking for sys/param.h... yes

checking for getpagesize... yes

checking for working mmap... no

checking for gettimeofday... yes

checking for memset... yes

checking for munmap... yes

configure: ==> Used target i.MX6!

configure: creating ./config.status

config.status: creating Makefile

config.status: creating mx5/basic/example1/Makefile

config.status: creating mx5/rotation/example1/Makefile

config.status: creating mx6/alphablending/example1/Makefile

config.status: creating mx6/alphablending/example2/Makefile

config.status: creating mx6/cropping/example1/Makefile

config.status: creating mx6/csc/example1/Makefile

config.status: creating mx6/deinterlacing/example1/Makefile

config.status: creating mx6/resizing/example1/Makefile

config.status: creating mx6/rotation/example1/Makefile

config.status: creating mx6/basic/example1/Makefile

config.status: executing depfiles commands

---------------------------------

~$ make

Making all in mx6/basic/example1

make[1]: Entering directory `/home/hli/codetest/ipu-examples/mx6/basic/example1'

arm-none-linux-gnueabi-gcc -DPACKAGE_NAME=\"ipu-examples\" -DPACKAGE_TARNAME=\"ipu-examples\" -DPACKAGE_VERSION=\"0.1\" -DPACKAGE_STRING=\"ipu-examples\ 0.1\" -DPACKAGE_BUGREPORT=\"rpimentel.silva@gmail.com\" -DPACKAGE_URL=\"\" -DPACKAGE=\"ipu-examples\" -DVERSION=\"0.1\" -DSTDC_HEADERS=1 -DHAVE_SYS_TYPES_H=1 -DHAVE_SYS_STAT_H=1 -DHAVE_STDLIB_H=1 -DHAVE_STRING_H=1 -DHAVE_MEMORY_H=1 -DHAVE_STRINGS_H=1 -DHAVE_INTTYPES_H=1 -DHAVE_STDINT_H=1 -DHAVE_UNISTD_H=1 -DHAVE_FCNTL_H=1 -DHAVE_STDINT_H=1 -DHAVE_STDLIB_H=1 -DHAVE_STRING_H=1 -DHAVE_SYS_IOCTL_H=1 -DHAVE_UNISTD_H=1 -DHAVE_STDLIB_H=1 -DHAVE_UNISTD_H=1 -DHAVE_SYS_PARAM_H=1 -DHAVE_GETPAGESIZE=1 -DHAVE_GETTIMEOFDAY=1 -DHAVE_MEMSET=1 -DHAVE_MUNMAP=1 -I.     -Wall -I /home/hli/fsl-community-bsp/build/tmp/work/imx6qsabresd-poky-linux-gnueabi/fsl-tp-image/1.0-r0/rootfs/usr/include -I /home/hli/fsl-community-bsp/build/tmp/work/imx6qsabresd-poky-linux-gnueabi/fsl-tp-image/1.0-r0/rootfs/usr/src/linux/include -MT basic_ex1.o -MD -MP -MF .deps/basic_ex1.Tpo -c -o basic_ex1.o basic_ex1.c

basic_ex1.c:32:25: fatal error: linux/mxcfb.h: No such file or directory

compilation terminated.

make[1]: *** [basic_ex1.o] Error 1

make[1]: Leaving directory `/home/hli/codetest/ipu-examples/mx6/basic/example1'

make: *** [all-recursive] Error 1

I showed that the compiler cannot find linux/mxcfb.h

I do not know this is due to the yocto or my yocto recipe setup.  Do i need extra steps to make it work in yocto?

the build i tried to make yesterday is based on dora_3.10.17-1.0.0_GA, actually I saw the same problems. it cannot find either linux/ipu.h or linux/mxcfb.h. During this build, I did not use the LTIB toochain and rootfs; I used yocto built-in toolchain and target sysroot to build it.

In order to make the compile find these two library files,

i switched the <linux/ipu.h> to <mxc_ipu_hl_lib.h> which is showed in IPUV3 library user guide.

and copied two mxcfb.h files to sysroot folder.

Of course, it still does not work.


Thanks a lot!


Haizhou

0 Kudos
1,205 Views
rogerio_silva
NXP Employee
NXP Employee

Hi haizhouli,

Yes, it was based on LTIB. It's time to move to Yocto... (I'm doing it right now)

I got the same error. I'm working to fix it and make it compatible to Yocto. It's a Makefile and configure problem.

The missing mxcfb.h error is because these demos require kernel headers that Yocto doesn't add by default on root file system.

mxc_ipu_hl_lib.h is the header from IPUv3 library used only on i.MX53. i.MX6 doesn't use this library.

I hope to have this fixed till the beginning of the next week. I'll keep you informed.

Rgds

Rogerio

0 Kudos
1,205 Views
haizhouli
Contributor III

Thanks for the update!

I have already made your examples working on yocto based on 3.0.35 using yocto built-in toolchain and target sysroot. But still show errors on 3.10.17.

I will begin to work on IPU coding on 3.0.35 currently and waiting for your update.

Thanks!

0 Kudos
1,206 Views
rogerio_silva
NXP Employee
NXP Employee

Hi haizhouli

I just updated the repository with 2 patches to fix the Makefile and configure files and also to update the Readme file. It's now building with kernel 3.10.17 + Yocto.

If you have problems to build or in some example code, please let me know.

Best Regards,

Rogerio

0 Kudos
1,205 Views
miroslavkopecek
Contributor II

Hi,
I am glad to hear that it is fixable, could you send me info, which 2 patches you applied ?
Thank you

Best regards

Miroslav Kopecek

0 Kudos