INIT: Id "mxc" respawning too fast: disabled for 5 minutes

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

INIT: Id "mxc" respawning too fast: disabled for 5 minutes

840 Views
yk704066
Contributor I

update-rc.d: /etc/init.d/run-postinsts exists during rc.d purge (continuing)
Removing any system startup links for run-postinsts ...
/etc/rcS.d/S99run-postinsts
INIT: Entering runlevel: 5/init.d/rc_g
Configuring network interfaces... fec 2188000.ethernet eth0: no PHY, assuming direct connection to switch
libphy: PHY fixed-0:00 not found
fec 2188000.ethernet eth0: could not attach to PHY
RTNETLINK answers: No such device
Starting system message bus: dbus.
Starting Dropbear SSH server: Generating key, this may take a while...
Public key portion is:
ssh-rsa AAAAB3NzaC1yc2EAAAADAQABAAABAQDFa9yOfqd0JEgxJ09aWn1Wv37opMiklmOg5wIBM48e/VdezmqYyvMTpNjRtgxH5b+ENjxRap4HR6c8v0CEHG6NgzhI21QQPUTz2wWrNxC3OndP0lkk98I7sMvolCxHoMVU+NG3IgUFGSeI3q1d9Nj07M3DRG6H1vmMfHBLAo+YMZLGFniq+yRqVSR+50lO793fXiscucMlWIVMSuo1or6yMLakWk6RAcvxtpBJenzUOiMp5fxlUZh9hkGiKOw+OlmQvq35R1B3wG15dPLIgxYMRv6eicUMGxK1wo2RYAICxKZw6YX26MYpvzpWLj0y1BgLr5xrpZ8XcH/0I/zW8VC5 root@imx6qsabresd
Fingerprint: md5 2e:0d:1f:5d:95:59:0e:95:47:1f:bd:b4:b9:2e:af:e5
dropbear.
Starting rpcbind daemon...done.
creating NFS state directory: done
starting statd: done
Starting advanced power management daemon: No APM support in kernel
(failed.)
NFS daemon support not enabled in kernel
Starting syslogd/klogd: done
* Starting Avahi mDNS/DNS-SD Daemon: avahi-daemon
...done.
Starting Telephony daemon
Starting Linux NFC daemon
Starting OProfileUI server
Running local boot scripts (/etc/rc.local).
Stopping Bootlog daemon: bootlogd.
INIT: cannot execute "/etc/init.d/rc_mxc.S"
INIT: cannot execute "/etc/init.d/rc_mxc.S"
INIT: cannot execute "/etc/init.d/rc_mxc.S"
INIT: cannot execute "/etc/init.d/rc_mxc.S"
INIT: cannot execute "/etc/init.d/rc_mxc.S"
INIT: cannot execute "/etc/init.d/rc_mxc.S"
INIT: cannot execute "/etc/init.d/rc_mxc.S"
INIT: cannot execute "/etc/init.d/rc_mxc.S"
INIT: cannot execute "/etc/init.d/rc_mxc.S"
INIT: cannot execute "/etc/init.d/rc_mxc.S"
INIT: Id "mxc" respawning too fast: disabled for 5 minutes

Labels (1)
0 Kudos
1 Reply

580 Views
b36401
NXP Employee
NXP Employee

It seems wrong script is noted in /etc/inittab file.
I mean that /etc/inittab has an option to respawn /etc/init.d/rc_mxc.S script which is wrong.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos