IMx6 Android 4.2 BSP: g_audio enabling for USB host interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMx6 Android 4.2 BSP: g_audio enabling for USB host interface

1,057 Views
manju_g
Contributor I

Hi Support,

.

I need your support in configuring the USB audio for HOST interface ‘0’.

 

I enabled currently USB Audio:

 

1014: [0]  <2020-03-02> <12:15:30.686>  3 [MS             ]: USB-Audio - Jabra UC VOICE 550a MS

1015: [0]  <2020-03-02> <12:15:30.687>                       Jabra Jabra UC VOICE 550a MS at usb-fsl-ehci.1-1, full speed

 

Actually it is enabled for “usb-fsl-ehci.1-1”. I need to enable for “fsl-ehci.0

 

Can you please provide the change points where we can enable the host “fsl-ehci.0”.

 

Below are the 2 USB interfaces which are enabled in our board.

 

 

1216: [0]  <2020-03-02> <12:24:38.492> ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver

1217: [0]  <2020-03-02> <12:24:38.493> fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller

1218: [0]  <2020-03-02> <12:24:38.494> fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 1

1219: [0]  <2020-03-02> <12:24:38.504> fsl-ehci fsl-ehci.0: irq 75, io base 0x02184000

1220: [0]  <2020-03-02> <12:24:38.520> fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00

1221: [0]  <2020-03-02> <12:24:38.552> hub 1-0:1.0: USB hub found

1222: [0]  <2020-03-02> <12:24:38.553> hub 1-0:1.0: 1 port detected

1223: [0]  <2020-03-02> <12:24:38.554> add wake up source irq 72

1224: [0]  <2020-03-02> <12:24:38.554> fsl-ehci fsl-ehci.1: Freescale On-Chip EHCI Host Controller

1225: [0]  <2020-03-02> <12:24:38.555> fsl-ehci fsl-ehci.1: new USB bus registered, assigned bus number 2

1226: [0]  <2020-03-02> <12:24:38.566> fsl-ehci fsl-ehci.1: irq 72, io base 0x02184200

1227: [0]  <2020-03-02> <12:24:38.582> fsl-ehci fsl-ehci.1: USB 2.0 started, EHCI 1.00

1228: [0]  <2020-03-02> <12:24:38.707> hub 2-0:1.0: USB hub found

1229: [0]  <2020-03-02> <12:24:38.707> hub 2-0:1.0: 1 port detected

Labels (3)
Tags (1)
0 Kudos
Reply
1 Reply

999 Views
igorpadykov
NXP Employee
NXP Employee

Hi MANJU

one can look at patches provided on

i.MX6 solo with Linux : Android phone as USB Sound card : no PCM 

Please note that Android 4.2 is outdated release and may be supported

with Commercial Support and Engineering Services | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply