IMXRT1176 evk running from SDRAM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMXRT1176 evk running from SDRAM

跳至解决方案
1,354 次查看
ahmedhrabi
Contributor IV

Hi all, 

I'am trying to run an SDK example (evkmimxrt1170_lvgl_demo_widgets_cm7) on imxrt1176 evk board, from the external ram SDRAM.

here's my config : 

SDRAM conf.png

The example crash with this conf, did someone have an idea about that ? 

Another question, when running the app from SDRAM can i debug through CMSIS-DAP linkserver or with PE Multilink ? 

Regards. 

标记 (2)
0 项奖励
回复
1 解答
1,340 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi @ahmedhrabi ,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Firstly, regarding the MCU settings, just clicking the Link application to RAM is enough, further, follow the post to set up the script to enable the debug in the SDRAM.

jeremyzhou_0-1658891006158.png


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

在原帖中查看解决方案

2 回复数
1,337 次查看
ahmedhrabi
Contributor IV

Hi @jeremyzhou

It works. Thank you for your support.

Regards.

0 项奖励
回复
1,341 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi @ahmedhrabi ,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Firstly, regarding the MCU settings, just clicking the Link application to RAM is enough, further, follow the post to set up the script to enable the debug in the SDRAM.

jeremyzhou_0-1658891006158.png


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------