现在我需要将IMXRT1170-EVK的摄像头的视频数据实时传输到PC显示,SDK里面只有传输到LCD显示的例程。如果有办法的话,可以详细的告知我吗?
你好,请参考RT1170 SDK软件包提供的<usb_device_video_virtual_camera> 例程,具体路径为:..\SDK_2_12_1_MIMXRT1170-EVK\boards\evkmimxrt1170\usb_examples\usb_device_video_virtual_camera
The USB video virtual camera application is a simple demonstration program based on the MCUXpresso SDK. It is enumerated as a camera and users can see the video of the device by using a PC test tool.
祝顺利。
thanks you ,your chinese is good.But why can't I switch my camera after burning the program,My system is Windows11.