IMXRT1050-EVK: Ethernet clock to PHY

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMXRT1050-EVK: Ethernet clock to PHY

2,001 Views
ulipe
Contributor II

Hello,

After setup my development environment with success on imxrt1050 evk, I started to port the tcp/ip (picoTCP) to my project, so write the enet driver was required, and I got the phy<->processor MII (MDIO/MDC) communication working and now I'm able to configure it. But when I read the link status register, even with cable connected it never report the link was up.

Loooking deeper on hardware ( in EVK schematic) I noted the phy XI pin (clock input) receives it from ENET_TX_CLK signal from processor, measuring with the oscilloscope I found no clock in this pin. Given this my question is, what is the correct ENET configuration to provide clock to enet phy in IMXRT1050-EVK?

Thank you in advance.

Felipe

0 Kudos
Reply
2 Replies

1,648 Views
art
NXP Employee
NXP Employee

Also, as the reference, you can use the enet driver code, included in the MCUXpresso SDK package, available for download on the processor's Software&Tools web page:

https://www.nxp.com/products/processors-and-microcontrollers/applications-processors/i.mx-applicatio...


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,648 Views
ulipe
Contributor II

3 days and no response useful response (again).


So I solved the problem, after configuring ENET PLL as stated on reference manual, and set the IOMUX to redirect the generated clock to the phy, now I able the 50MHz clock to use in RMII mode and got the phy fully working, to help others with same question, follow the code snippet below before configure the ethernet:

const clock_enet_pll_config_t config = { .enableClkOutput0 = true, .enableClkOutput1 = false, .enableClkOutput2 = false, .loopDivider0 = 0x01, .loopDivider1 = 0x01 };

/* configure ethernet pin_muxing and clocking*/

CLOCK_InitEnetPll(&config);

IOMUXC_EnableMode(IOMUXC_GPR, kIOMUXC_GPR_ENET1TxClkOutputDir, true);

BOARD_InitENET();

Best.

Felipe

0 Kudos
Reply