IMXRT: option to configure delay in RMII path

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMXRT: option to configure delay in RMII path

1,623件の閲覧回数
geovarghese
Contributor II

We are using IMXRT1051 in one of our design which is interfaced with an Ethernet switch IP175D using RMII. We are facing an issue here. The packets from IMXRT to external PC via the IP175D switch reaches fine. But when we are trying to send packet from external PC to the IMXRT, the data packet received is having CRC error.

We tried the following with Ethernet interface.

  • Configured imxrt ENET_REF_CLK as input to receive reference clock from IP75D switch. Then we connected the RMII1_MAC_CLK_OUT(50MHz RMII clock out) of switch to GPIO_B1_10 pin of IMXRT to receive 50MHz RMII reference clock. With this configuration we are getting CRC error on packets received at the IMXRT.
  • Configured iMXRT ENET_REF_CLK as RMII reference clock out. Then we connected the RMII1_MAC_CLK_IN(RMII CLK IN) of switch to GPIO_B1_10 pin of IMXRT to receive the 50MHz RMII reference clock. With this configuration also we are getting CRC error on packets received at the IMXRT.

We are assuming that there is issue in timing between the TX of the switch and RX side of the IMXRT. Is there any register option to configure delay in RMII RX side of IMXRT?

タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,430件の閲覧回数
dmarples
Contributor IV

You might want to checkout https://community.nxp.com/message/1040701  in case it has any bearing on the symptom you've got.

Regards

DAVE

0 件の賞賛
返信

1,430件の閲覧回数
art
NXP Employee
NXP Employee

Q. Is there any register option to configure delay in RMII RX side of IMXRT?

A. No, there is no way to add a programmable delay in the i.MX RT1050 RMII Rx path.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信