IMXRT CUSTOM ETHERNET PHY NOT WORKING

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMXRT CUSTOM ETHERNET PHY NOT WORKING

跳至解决方案
4,956 次查看
nicolasmuratore
Contributor III

Hi all, hope this email finds you well, I'm trying to develop a custom board using IMXRT1021DAG, this board has an ethernet interface based on the same ethernet interface of the EVK.

In fact I'm using the same PHY KSZ8081RNB, and the circuit is almost the same of the EVK too (I didn't put the pull ups resistors on the analog side because those are implemented inside the PHY):  

nicolasmuratore_0-1652789445364.png

The only difference is the RJ45 connector, I'm using Thru hole (WURSHT 7499010211A) against the SMD of the EVK, just for robustness, but the internal transformers and parameters are the same:

 

nicolasmuratore_1-1652789620136.png

I'm using an example of the SDK that allow me to test the interface sending frames and then reading them back, using a loopback cable connected to the RJ45 that is working perfectly on EVK.

Problem: The test is not working on my board, the PHY doesn't send any frame to the analog side (RJ45 side).

I know that the communication between the MAC (IMXRT1021) and PHY is ok because I can do a digital loopback test (available on KSZ8081RNB to test RMII communication).

I tried to test doing the following connection too:

nicolasmuratore_2-1652791374710.png

My board receive all the frames, sent from EVK, in right way, but in the moment of transmiting from custom board to EVK, the MAC send information over RMII channel but PHY doesn't send any frame to the other side.

I've checked the PCB, the components, the routing of RJ45 is similar to EVK, keeping differential pairs togueter and impedance low 100Ohm. 

I really don't understand what is happening, any idea would be very appreciated.

Many thanks. 

      

标签 (1)
0 项奖励
回复
1 解答
4,897 次查看
nicolasmuratore
Contributor III

I found it!!!

One of the resistors that controls the output power, with a value that should be 6.49K, is wrongly 64K, so the output didn't have enough power to transmit signals, my components supplier made a mistake.

Now is working, besides that I solved some welding problems too.

Many thanks for your guidence on this issue.

在原帖中查看解决方案

0 项奖励
回复
8 回复数
4,948 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

From the problem description, the only difference at Ethernet circuit design is the PHY.

And customer board could receive data frame from EVK board sent.

Besides of PHY circuit and soldering review, please check the Ethernet cable status.

Mike

0 项奖励
回复
4,926 次查看
nicolasmuratore
Contributor III

I did some test and realized that many packets are missing during reception on my custom board from the EVK transmission, so I was wrong on my first post when I said that the reception was ok.

I think that maybe the problem is related to signal levels or signal detection on the RJ45 side.

I've checked the circuit and components from RJ45 side (there are not many really, just two capacitors and the connector) and everything semms to be ok, I have soldered the KSZ8081 again.

So, what could be wrong?

Is a mistery by now. 

Many thanks.

0 项奖励
回复
4,916 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

How many boards have you tested? All with the same issue?

Mike

标记 (1)
0 项奖励
回复
4,908 次查看
nicolasmuratore
Contributor III

Hi Mike, I've tested 6 six  boards with the same issue, I have almost 20 prototipes, so I will continuing cheking all of them to find something related to the PCB construction, welding, etc.. 

I really can't think in another thing that is not related to PCB manufacturing.

Many thanks.

0 项奖励
回复
4,902 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Besides of hardware soldering, please check the PCB layout design also, especially for ENET PHY connection with RJ45 connector. Thanks.

Mike

0 项奖励
回复
4,898 次查看
nicolasmuratore
Contributor III

I found it!!!

One of the resistors that controls the output power, with a value that should be 6.49K, is wrongly 64K, so the output didn't have enough power to transmit signals, my components supplier made a mistake.

Now is working, besides that I solved some welding problems too.

Many thanks for your guidence on this issue.

0 项奖励
回复
4,891 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Great!

You are welcome. Nice to know this issue was fixed. 

Mike

0 项奖励
回复
4,944 次查看
nicolasmuratore
Contributor III

Hi Mike, thanks for your answer, I will check all the connections again, then I will let you know.

Many thanks!!!

0 项奖励
回复