IMXQP SD Boot Issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMXQP SD Boot Issue

1,124 次查看
kishorr
Contributor II

We are observing SD Boot Issue on IMX6QP based custom hardware board. We have the below

SD BOOT Configuration
SRC_SBMR1(0x020d8004) = 0x00001040
SRC_SBMR2(0x020d801c) = 0x12000001

On POR, SD boot is not happening.

But when we boot from eMMC, run "mmc dev 1" the SD card returns the message: "Card did not respond to voltage select"

At this time if we plug out the SD card and plug in and execute "mmc dev 1" the SD cards gets detected.

After the card is detected if we reset the board (not POR) after installing jumpers for SD boot we could see SD boot working.

But if we do POR the SD boot is not working.

Based on this behavior we are suspecting that ROM code is unable to access the SD card for some reason?

Appreciate if anyone have any inputs on this issue.

Thanks

Kishor

0 项奖励
回复
1 回复

966 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Kishor

one can check if clocks are stable (24MHz crystal, 32.768KHz) and try

to extend POR up to 0.8-1 sec. Also may be recommended to check power supplies,

are they are stable when POR released, some hints may found in i.MX6 System Development User’s

Guide Chapter 8 Avoiding Board Bring-up Problems

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复