IMX93QSB - JTAG Flashing/Debugging via USB-C (FTDI FT4232H) on Windows/Linux

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX93QSB - JTAG Flashing/Debugging via USB-C (FTDI FT4232H) on Windows/Linux

ソリューションへジャンプ
2,139件の閲覧回数
sergiomauro
Contributor II

Hello Everyone,

I hope you're doing well. I’m currently seeking assistance on how to perform JTAG flashing and debugging on the IMX93QSB using the USB-C debug port. Specifically, I would like to know if this can be done using an FTDI FT4232H (Port A configured as JTAG) through the USB-C port. Is this functionality supported on both Windows 10/11 and Linux?

I’ve reviewed the Reference Manual but couldn’t find clear guidance on this feature. Could someone confirm whether this is feasible, and if so, provide the necessary steps to make it work?

Thank you in advance for your help!

0 件の賞賛
返信
1 解決策
2,077件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

It is not be possible to flash the board using JTAG, please note that JTAG in the i.MX devices, excluding the RT family, is used for the debug purpose only.

Regarding OpenOCD, please take a look in the next presentation.

Best regards.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,078件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

It is not be possible to flash the board using JTAG, please note that JTAG in the i.MX devices, excluding the RT family, is used for the debug purpose only.

Regarding OpenOCD, please take a look in the next presentation.

Best regards.

0 件の賞賛
返信
2,060件の閲覧回数
sergiomauro
Contributor II

Hello,

thank you for the clarification.

Just to confirm, is debugging possible only with a SEGGER J-Link, or is it also feasible to use the USB-C port with FTDI FT4232H chip (configured with Port A as JTAG)? I’d like to understand if this setup would work for debugging, and if so, whether there are any specific configurations required.

Thanks in advance for your assistance.

BR
Sergio

0 件の賞賛
返信
2,053件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

It is possible to debug using both methods, SEGGER J-Link and OpenOCD.

Best regards.

0 件の賞賛
返信