IMX93 ,lvds have signal,cann't display

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX93 ,lvds have signal,cann't display

921 Views
5454ty
Contributor II

HI,

    I have signale,the clock is 71.4MHZ,and lvds signal also have ,but cann't display

    My log is as follows:

   


U-Boot SPL 2023.04-dirty (Jun 03 2024 - 21:53:22 -0700)
SOC: 0xa1009300
LC: 0x2040010
PMIC: PCA9451A
PMIC: Over Drive Voltage Mode
DDR: 1866MTS
M33 prepare ok
Normal Boot
Trying to boot from BOOTROM
Boot Stage: Primary boot
image offset 0x8000, pagesize 0x200, ivt offset 0x0
Load image from 0x52400 by ROM_API
NOTICE: BL31: v2.8(release):lf-6.1.55-2.2.0-0-g08e9d4eef
NOTICE: BL31: Built : 06:43:30, Nov 21 2023


U-Boot 2023.04-dirty (Jun 03 2024 - 21:53:22 -0700)

CPU: i.MX93(52) rev1.1 1700 MHz (running at 1692 MHz)
CPU: Industrial temperature grade (-40C to 105C) at 38C
Reset cause: POR (0x1)
Model: NXP i.MX93 11X11 EVK board
DRAM: 2 GiB
tcpc_init: Can't find device id=0x52
setup_typec: tcpc portpd init failed, err=-19
setup_pd_switch: Can't find device id=0x73
TCPC: Vendor ID [0x8008], Product ID [0xd488], Addr [I2C2 0x51]
tcpc_init: Can't find device id=0x50
setup_typec: tcpc port1 init failed, err=-19
pca953x gpio@22: Error reading output register
Core: 225 devices, 36 uclasses, devicetree: separate
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... OK
[*]-Video Link 0adv7535_mipi2hdmi hdmi@3d: Can't find cec device id=0x3c
fail to probe panel device hdmi@3d
fail to get display timings
probe video device failed, ret -19

[0] lcd-controller@4ae30000, video
[1] dsi@4ae10000, video_bridge
[2] hdmi@3d, panel
adv7535_mipi2hdmi hdmi@3d: Can't find cec device id=0x3c
fail to probe panel device hdmi@3d
fail to get display timings
probe video device failed, ret -19
In: serial
Out: serial
Err: serial

BuildInfo:
- ELE firmware version 0.1.0-44880904

switch to partitions #0, OK
mmc1 is current device
flash target is MMC:1
Net: pca953x gpio@22: Error reading output register
pca953x gpio@22: Error reading output register
Could not get PHY for FEC0: addr 2
pca953x gpio@22: Error reading output register
pca953x gpio@22: Error reading output register
Could not get PHY for FEC0: addr 2
pca953x gpio@22: Error reading output register
pca953x gpio@22: Error reading output register
eth1: ethernet@428a0000 [PRIME]
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot: 0
Working FDT set to 83000000
switch to partitions #0, OK
mmc0(part 0) is current device
** No partition table - mmc 0 **
Couldn't find partition mmc 0:1
switch to partitions #0, OK
mmc1 is current device
Scanning mmc 1:1...
47695 bytes read in 4 ms (11.4 MiB/s)
Working FDT set to 83000000
Unable to open OP-TEE session (err=-5)
mm_communicate failed!
Error: Cannot initialize UEFI sub-system, r = 3
starting USB...
Bus usb@4c100000: Port not available.
Bus usb@4c200000: Port not available.
USB is stopped. Please issue 'usb start' first.
Running BSP bootcmd ...
switch to partitions #0, OK
mmc1 is current device
Failed to load 'boot.scr'
32856576 bytes read in 355 ms (88.3 MiB/s)
Booting from mmc ...
47695 bytes read in 5 ms (9.1 MiB/s)
## Flattened Device Tree blob at 83000000
Booting using the fdt blob at 0x83000000
Working FDT set to 83000000
Using Device Tree in place at 0000000083000000, end 000000008300ea4e
Working FDT set to 83000000
adv7535_mipi2hdmi hdmi@3d: Can't find cec device id=0x3c
fail to probe panel device hdmi@3d
fail to get display timings
probe video device failed, ret -19

Starting kernel ...

[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x412fd050]
[ 0.000000] Linux version 6.1.55+g770c5fe2c1d1 (tangyuan@ubuntu) (aarch64-poky-linux-gcc (GCC) 12.3.0, GNU ld (GNU Binutils) 2.40.0.20230703) #96 SMP PREEMPT Sat Jul 6 00:16:15 PDT 2024
[ 0.000000] Machine model: NXP i.MX93 11X11 EVK board
[ 0.000000] efi: UEFI not found.
[ 0.000000] Reserved memory: created CMA memory pool at 0x00000000b0000000, size 256 MiB
[ 0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a4020000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vdevbuffer@a4020000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a4120000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node ele-reserved@a4120000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created CMA memory pool at 0x00000000c0000000, size 256 MiB
[ 0.000000] OF: reserved mem: initialized node ethosu_region@C0000000, compatible id shared-dma-pool
[ 0.000000] earlycon: lpuart32 at MMIO32 0x0000000044380000 (options '')
[ 0.000000] printk: bootconsole [lpuart32] enabled
[ 0.000000] NUMA: No NUMA configuration found
[ 0.000000] NUMA: Faking a node at [mem 0x0000000080000000-0x00000000ffffffff]
[ 0.000000] NUMA: NODE_DATA [mem 0xffbd3700-0xffbd5fff]
[ 0.000000] Zone ranges:
[ 0.000000] DMA [mem 0x0000000080000000-0x00000000ffffffff]
[ 0.000000] DMA32 empty
[ 0.000000] Normal empty
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000080000000-0x0000000095ffffff]
[ 0.000000] node 0: [mem 0x0000000098000000-0x00000000a3ffffff]
[ 0.000000] node 0: [mem 0x00000000a4000000-0x00000000a421ffff]
[ 0.000000] node 0: [mem 0x00000000a4220000-0x00000000ffffffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000000ffffffff]
[ 0.000000] On node 0, zone DMA: 8192 pages in unavailable ranges
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: Trusted OS migration not required
[ 0.000000] psci: SMC Calling Convention v1.2
[ 0.000000] percpu: Embedded 20 pages/cpu s44520 r8192 d29208 u81920
[ 0.000000] Detected VIPT I-cache on CPU0
[ 0.000000] CPU features: detected: GIC system register CPU interface
[ 0.000000] CPU features: detected: Virtualization Host Extensions
[ 0.000000] CPU features: detected: Qualcomm erratum 1009, or ARM erratum 1286807, 2441009
[ 0.000000] CPU features: detected: ARM errata 1165522, 1319367, or 1530923
[ 0.000000] alternatives: applying boot alternatives
[ 0.000000] Fallback order for Node 0: 0
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 507904
[ 0.000000] Policy zone: DMA
[ 0.000000] Kernel command line: console=ttyLP0,115200 earlycon root=/dev/mmcblk1p2 rootwait rw
[ 0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)
[ 0.000000] mem auto-init: stack:all(zero), heap alloc:off, heap free:off
[ 0.000000] Memory: 1464832K/2064384K available (19776K kernel code, 1622K rwdata, 7240K rodata, 3328K init, 644K bss, 75264K reserved, 524288K cma-reserved)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU event tracing is enabled.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=2.
[ 0.000000] Trampoline variant of Tasks RCU enabled.
[ 0.000000] Tracing variant of Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000] GICv3: 960 SPIs implemented
[ 0.000000] GICv3: 0 Extended SPIs implemented
[ 0.000000] Root IRQ handler: gic_handle_irq
[ 0.000000] GICv3: GICv3 features: 16 PPIs
[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000048040000
[ 0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention.
[ 0.000000] arch_timer: cp15 timer(s) running at 24.00MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x588fe9dc0, max_idle_ns: 440795202592 ns
[ 0.000000] sched_clock: 56 bits at 24MHz, resolution 41ns, wraps every 4398046511097ns
[ 0.008375] Console: colour dummy device 80x25
[ 0.012633] Calibrating delay loop (skipped), value calculated using timer frequency.. 48.00 BogoMIPS (lpj=96000)
[ 0.022789] pid_max: default: 32768 minimum: 301
[ 0.027421] LSM: Security Framework initializing
[ 0.032069] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[ 0.039346] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[ 0.048035] cacheinfo: Unable to detect cache hierarchy for CPU 0
[ 0.054371] cblist_init_generic: Setting adjustable number of callback queues.
[ 0.061375] cblist_init_generic: Setting shift to 1 and lim to 1.
[ 0.067451] cblist_init_generic: Setting adjustable number of callback queues.
[ 0.074606] cblist_init_generic: Setting shift to 1 and lim to 1.
[ 0.080795] rcu: Hierarchical SRCU implementation.
[ 0.085438] rcu: Max phase no-delay instances is 1000.
[ 0.091556] EFI services will not be available.
[ 0.096080] smp: Bringing up secondary CPUs ...
[ 0.100783] Detected VIPT I-cache on CPU1
[ 0.100878] cacheinfo: Unable to detect cache hierarchy for CPU 1
[ 0.100892] GICv3: CPU1: found redistributor 100 region 0:0x0000000048060000
[ 0.100940] CPU1: Booted secondary processor 0x0000000100 [0x412fd050]
[ 0.101054] smp: Brought up 1 node, 2 CPUs
[ 0.128475] SMP: Total of 2 processors activated.
[ 0.133143] CPU features: detected: 32-bit EL0 Support
[ 0.138266] CPU features: detected: 32-bit EL1 Support
[ 0.143371] CPU features: detected: Data cache clean to the PoU not required for I/D coherence
[ 0.151944] CPU features: detected: Common not Private translations
[ 0.158184] CPU features: detected: CRC32 instructions
[ 0.163300] CPU features: detected: RCpc load-acquire (LDAPR)
[ 0.169017] CPU features: detected: LSE atomic instructions
[ 0.174564] CPU features: detected: Privileged Access Never
[ 0.180110] CPU features: detected: RAS Extension Support
[ 0.185488] CPU features: detected: Speculative Store Bypassing Safe (SSBS)
[ 0.192480] CPU: All CPU(s) started at EL2
[ 0.196493] alternatives: applying system-wide alternatives
[ 0.207779] devtmpfs: initialized
[ 0.216515] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.226034] futex hash table entries: 512 (order: 3, 32768 bytes, linear)
[ 0.243323] pinctrl core: initialized pinctrl subsystem
[ 0.249867] DMI not present or invalid.
[ 0.254002] NET: Registered PF_NETLINK/PF_ROUTE protocol family
[ 0.260708] DMA: preallocated 256 KiB GFP_KERNEL pool for atomic allocations
[ 0.267659] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[ 0.275341] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[ 0.283184] audit: initializing netlink subsys (disabled)
[ 0.288762] audit: type=2000 audit(0.192:1): state=initialized audit_enabled=0 res=1
[ 0.289261] thermal_sys: Registered thermal governor 'step_wise'
[ 0.296242] thermal_sys: Registered thermal governor 'power_allocator'
[ 0.302409] cpuidle: using governor menu
[ 0.312855] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.319429] ASID allocator initialised with 65536 entries
[ 0.325507] Serial: AMBA PL011 UART driver
[ 0.329410] imx mu driver is registered.
[ 0.333255] imx rpmsg driver is registered.
[ 0.343074] imx93-pinctrl 443c0000.pinctrl: initialized IMX pinctrl driver
[ 0.356328] platform 4ae30000.lcd-controller: Fixed dependency cycle(s) with /soc@0/ldb@4ac10020/lvds-channel@0/port@0/endpoint
[ 0.370533] platform lvds_panel: Fixed dependency cycle(s) with /soc@0/ldb@4ac10020/lvds-channel@0/port@1/endpoint
[ 0.380939] KASLR disabled due to lack of seed
[ 0.396942] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages
[ 0.403484] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page
[ 0.409710] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages
[ 0.416468] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page
[ 0.422709] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.429467] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page
[ 0.435708] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages
[ 0.442467] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page
[ 0.450688] ACPI: Interpreter disabled.
[ 0.455174] 5v en is failed================================================
[ 0.461891] lvdsen is failed================================
[ 0.467507] lvdspwr is failed================================
[ 0.473226] lvdspwm is failed================================
[ 0.478946] mipi pwr is failed===========================
[ 0.484542] 5v en is failed================================================
[ 0.491263] lvdsen is failed================================
[ 0.496886] lvdspwr is failed================================
[ 0.502606] lvdspwm is failed================================
[ 0.508326] mipi pwr is failed===========================
[ 0.514382] iommu: Default domain type: Translated
[ 0.519001] iommu: DMA domain TLB invalidation policy: strict mode
[ 0.525518] SCSI subsystem initialized
[ 0.529390] usbcore: registered new interface driver usbfs
[ 0.534652] usbcore: registered new interface driver hub
[ 0.539913] usbcore: registered new device driver usb
[ 0.545877] mc: Linux media interface: v0.10
[ 0.549938] videodev: Linux video capture interface: v2.00
[ 0.555393] pps_core: LinuxPPS API ver. 1 registered
[ 0.560285] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.569390] PTP clock support registered
[ 0.573408] EDAC MC: Ver: 3.0.0
[ 0.577735] FPGA manager framework
[ 0.580952] Advanced Linux Sound Architecture Driver Initialized.
[ 0.587456] Bluetooth: Core ver 2.22
[ 0.590795] NET: Registered PF_BLUETOOTH protocol family
[ 0.596070] Bluetooth: HCI device and connection manager initialized
[ 0.602391] Bluetooth: HCI socket layer initialized
[ 0.607242] Bluetooth: L2CAP socket layer initialized
[ 0.612276] Bluetooth: SCO socket layer initialized
[ 0.617571] vgaarb: loaded
[ 0.620697] clocksource: Switched to clocksource arch_sys_counter
[ 0.626795] VFS: Disk quotas dquot_6.6.0
[ 0.630507] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 0.637455] pnp: PnP ACPI: disabled
[ 0.645987] NET: Registered PF_INET protocol family
[ 0.650846] IP idents hash table entries: 32768 (order: 6, 262144 bytes, linear)
[ 0.659214] tcp_listen_portaddr_hash hash table entries: 1024 (order: 2, 16384 bytes, linear)
[ 0.667565] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear)
[ 0.675211] TCP established hash table entries: 16384 (order: 5, 131072 bytes, linear)
[ 0.683157] TCP bind hash table entries: 16384 (order: 7, 524288 bytes, linear)
[ 0.690956] TCP: Hash tables configured (established 16384 bind 16384)
[ 0.697409] UDP hash table entries: 1024 (order: 3, 32768 bytes, linear)
[ 0.703943] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes, linear)
[ 0.711188] NET: Registered PF_UNIX/PF_LOCAL protocol family
[ 0.717154] RPC: Registered named UNIX socket transport module.
[ 0.722830] RPC: Registered udp transport module.
[ 0.727490] RPC: Registered tcp transport module.
[ 0.732169] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.739226] PCI: CLS 0 bytes, default 64
[ 0.743466] hw perfevents: enabled with armv8_cortex_a55 PMU driver, 7 counters available
[ 0.752037] kvm [1]: IPA Size Limit: 40 bits
[ 0.756085] kvm [1]: GICv3: no GICV resource entry
[ 0.760815] kvm [1]: disabling GICv2 emulation
[ 0.765255] kvm [1]: GIC system register CPU interface enabled
[ 0.771098] kvm [1]: vgic interrupt IRQ9
[ 0.774996] kvm [1]: VHE mode initialized successfully
[ 0.781219] Initialise system trusted keyrings
[ 0.785653] workingset: timestamp_bits=42 max_order=19 bucket_order=0
[ 0.796235] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.802451] NFS: Registering the id_resolver key type
[ 0.807319] Key type id_resolver registered
[ 0.811413] Key type id_legacy registered
[ 0.815451] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 0.822072] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[ 0.829453] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
[ 0.835850] 9p: Installing v9fs 9p2000 file system support
[ 0.866290] Key type asymmetric registered
[ 0.870121] Asymmetric key parser 'x509' registered
[ 0.875022] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 243)
[ 0.882342] io scheduler mq-deadline registered
[ 0.886845] io scheduler kyber registered
[ 0.894079] led init
[ 0.896208] success
[ 0.900549] EINJ: ACPI disabled.
[ 0.909253] Bus freq driver module loaded
[ 0.918834] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 0.936632] printk: console [ttyLP0] enabled0x44380010 (irq = 18, base_baud = 1500000) is a FSL_LPUART
[ 0.936632] printk: console [ttyLP0] enabled
[ 0.945032] printk: bootconsole [lpuart32] disabled
[ 0.945032] printk: bootconsole [lpuart32] disabled
[ 0.955529] 42590000.serial: ttyLP4 at MMIO 0x42590010 (irq = 19, base_baud = 1500000) is a FSL_LPUART
[ 0.964952] serial serial0: tty port ttyLP4 registered
[ 0.971366] add by tangyuan imx drm probe=============================
[ 0.979040] add by tangyuan imx93_ldb probe=================================
[ 0.988476] add by tangyuan============================panel================
[ 0.995569] LVDS PANEL==============================================
[ 1.001931] panel-simple lvds_panel: supply power not found, using dummy regulator
[ 1.009646] 5v en is failed================================================
[ 1.016617] lvdsen is failed================================
[ 1.022269] lvdspwr is failed================================
[ 1.028059] lvdspwm is failed================================
[ 1.033795] mipi pwr is failed===========================
[ 1.041361] imx drm bind=================================
[ 1.047560] imx-drm display-subsystem: bound imx-lcdifv3-crtc.0 (ops lcdifv3_crtc_ops)
[ 1.055529] imx93 ldb bind======================================================
[ 1.064502] cacheinfo: Unable to detect cache hierarchy for CPU 0
[ 1.074918] loop: module loaded
[ 1.079401] of_reserved_mem_lookup() returned NULL
[ 1.084380] megasas: 07.719.03.00-rc1
[ 1.094090] tun: Universal TUN/TAP device driver, 1.6
[ 1.100112] thunder_xcv, ver 1.0
[ 1.103416] thunder_bgx, ver 1.0
[ 1.106662] nicpf, ver 1.0
[ 1.110357] pps pps0: new PPS source ptp0
[ 1.116137] mdio_bus 42890000.ethernet-1: MDIO device at address 2 is missing.
[ 1.123861] fec 42890000.ethernet eth0: registered PHC device 0
[ 1.131857] hns3: Hisilicon Ethernet Network Driver for Hip08 Family - version
[ 1.139105] hns3: Copyright (c) 2017 Huawei Corporation.
[ 1.144510] hclge is initializing
[ 1.147850] e1000: Intel(R) PRO/1000 Network Driver
[ 1.152726] e1000: Copyright (c) 1999-2006 Intel Corporation.
[ 1.158500] e1000e: Intel(R) PRO/1000 Network Driver
[ 1.163458] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[ 1.169393] igb: Intel(R) Gigabit Ethernet Network Driver
[ 1.174787] igb: Copyright (c) 2007-2014 Intel Corporation.
[ 1.180387] igbvf: Intel(R) Gigabit Virtual Function Network Driver
[ 1.186641] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[ 1.192837] sky2: driver version 1.30
[ 1.197124] usbcore: registered new interface driver r8152
[ 1.202988] VFIO - User Level meta-driver version: 0.3
[ 1.211633] usbcore: registered new interface driver uas
[ 1.217010] usbcore: registered new interface driver usb-storage
[ 1.223095] usbcore: registered new interface driver usbserial_generic
[ 1.229628] usbserial: USB Serial support registered for generic
[ 1.235644] usbcore: registered new interface driver ftdi_sio
[ 1.241390] usbserial: USB Serial support registered for FTDI USB Serial Device
[ 1.248709] usbcore: registered new interface driver usb_serial_simple
[ 1.255285] usbserial: USB Serial support registered for carelink
[ 1.261375] usbserial: USB Serial support registered for flashloader
[ 1.267726] usbserial: USB Serial support registered for funsoft
[ 1.273742] usbserial: USB Serial support registered for google
[ 1.279670] usbserial: USB Serial support registered for hp4x
[ 1.285415] usbserial: USB Serial support registered for kaufmann
[ 1.291507] usbserial: USB Serial support registered for libtransistor
[ 1.298033] usbserial: USB Serial support registered for moto_modem
[ 1.304299] usbserial: USB Serial support registered for motorola_tetra
[ 1.310912] usbserial: USB Serial support registered for nokia
[ 1.316745] usbserial: USB Serial support registered for novatel_gps
[ 1.323097] usbserial: USB Serial support registered for siemens_mpi
[ 1.329449] usbserial: USB Serial support registered for suunto
[ 1.335369] usbserial: USB Serial support registered for vivopay
[ 1.341383] usbserial: USB Serial support registered for zio
[ 1.347059] usbcore: registered new interface driver usb_ehset_test
[ 1.356127] bbnsm_pwrkey 44440000.bbnsm:pwrkey: KEY_POWER without setting in dts
[ 1.364420] input: 44440000.bbnsm:pwrkey as /devices/platform/soc@0/44000000.bus/44440000.bbnsm/44440000.bbnsm:pwrkey/input/input0
[ 1.379468] bbnsm_rtc 44440000.bbnsm:rtc: registered as rtc0
[ 1.385548] bbnsm_rtc 44440000.bbnsm:rtc: setting system clock to 1970-01-01T00:00:00 UTC (0)
[ 1.395011] i2c_dev: i2c /dev entries driver
[ 1.402995] imx7ulp-wdt 42490000.wdog: imx93 wdt probe
[ 1.432930] Bluetooth: HCI UART driver ver 2.3
[ 1.437397] Bluetooth: HCI UART protocol H4 registered
[ 1.442524] Bluetooth: HCI UART protocol BCSP registered
[ 1.447863] Bluetooth: HCI UART protocol LL registered
[ 1.452994] Bluetooth: HCI UART protocol ATH3K registered
[ 1.458399] Bluetooth: HCI UART protocol Three-wire (H5) registered
[ 1.464856] Bluetooth: HCI UART protocol Broadcom registered
[ 1.470526] Bluetooth: HCI UART protocol QCA registered
[ 1.477701] sdhci: Secure Digital Host Controller Interface driver
[ 1.483913] sdhci: Copyright(c) Pierre Ossman
[ 1.488914] Synopsys Designware Multimedia Card Interface Driver
[ 1.495432] sdhci-pltfm: SDHCI platform and OF driver helper
[ 1.503216] sdhci-esdhc-imx 428b0000.mmc: allocated mmc-pwrseq
[ 1.509157] ledtrig-cpu: registered to indicate activity on CPUs
[ 1.516961] fsl-ele-mu soc@0:ele-mu: ele_mu_probe: Not able to read cmd_tag
[ 1.523953] fsl-ele-mu soc@0:ele-mu: ele_mu_probe: Not able to read rsp_tag
[ 1.531564] fsl-ele-mu soc@0:ele-mu: assigned reserved memory node ele-reserved@a4120000
[ 1.539760] fsl-ele-mu soc@0:ele-mu: registering ele-trng
[ 1.540276] mmc2: SDHCI controller on 428b0000.mmc [428b0000.mmc] using ADMA
[ 1.545334] mmc0: SDHCI controller on 42850000.mmc [42850000.mmc] using ADMA
[ 1.559375] random: crng init done
[ 1.559650] fsl-ele-mu soc@0:ele-mu: Successfully registered ele-trng
[ 1.569547] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[ 1.576540] usbcore: registered new interface driver usbhid
[ 1.582208] usbhid: USB HID core driver
[ 1.589109] ethosu ethosu: assigned reserved memory node ethosu_region@C0000000
[ 1.638566] cs_system_cfg: CoreSight Configuration manager initialised
[ 1.647547] optee: probing for conduit method.
[ 1.652057] optee: revision 4.0 (a303fc80)
[ 1.652654] optee: dynamic shared memory is enabled
[ 1.661988] optee: initialized driver
[ 1.667988] mmc0: new HS400 Enhanced strobe MMC card at address 0001
[ 1.675349] mmcblk0: mmc0:0001 DA6016 14.7 GiB
[ 1.678083] NET: Registered PF_LLC protocol family
[ 1.681843] mmcblk0boot0: mmc0:0001 DA6016 4.00 MiB
[ 1.685489] NET: Registered PF_INET6 protocol family
[ 1.690930] mmcblk0boot1: mmc0:0001 DA6016 4.00 MiB
[ 1.695703] Segment Routing with IPv6
[ 1.700679] mmcblk0rpmb: mmc0:0001 DA6016 4.00 MiB, chardev (511:0)
[ 1.703431] In-situ OAM (IOAM) with IPv6
[ 1.713566] NET: Registered PF_PACKET protocol family
[ 1.718683] bridge: filtering via arp/ip/ip6tables is no longer available by default. Update your scripts to load br_netfilter if you need this.
[ 1.731799] Bluetooth: RFCOMM TTY layer initialized
[ 1.736709] Bluetooth: RFCOMM socket layer initialized
[ 1.741887] Bluetooth: RFCOMM ver 1.11
[ 1.745648] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[ 1.750962] Bluetooth: BNEP filters: protocol multicast
[ 1.756192] Bluetooth: BNEP socket layer initialized
[ 1.761223] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[ 1.767153] Bluetooth: HIDP socket layer initialized
[ 1.772441] 8021q: 802.1Q VLAN Support v1.8
[ 1.776710] lib80211: common routines for IEEE802.11 drivers
[ 1.782489] 9pnet: Installing 9P2000 support
[ 1.786881] Key type dns_resolver registered
[ 1.791700] registered taskstats version 1
[ 1.795836] Loading compiled-in X.509 certificates
[ 1.823605] usb_phy_generic soc@0:usbphynop1: supply vcc not found, using dummy regulator
[ 1.832130] usb_phy_generic soc@0:usbphynop1: dummy supplies not allowed for exclusive requests
[ 1.841083] usb_phy_generic soc@0:usbphynop2: supply vcc not found, using dummy regulator
[ 1.849408] usb_phy_generic soc@0:usbphynop2: dummy supplies not allowed for exclusive requests
[ 1.868434] imx8mp_lvds_phy_probe============================================================
[ 1.877225] imx93-ldb soc@0:ldb@4ac10020: Failed to create device link (0x180) with soc@0:phy@4ac10024
[ 1.888039] sdhci-esdhc-imx 428b0000.mmc: Failed to create device link (0x180) with 43820080.gpio
[ 1.898247] add by tangyuan pwm=========================================
[ 1.905080] pwm-backlight lvds_backlight: supply power not found, using dummy regulator
[ 1.913205] of_pwm_get(): can't parse "pwms" property
[ 1.918249] pwm-backlight lvds_backlight: unable to request PWM
[ 1.924157] pwm-backlight: probe of lvds_backlight failed with error -2
[ 1.933460] imx drm bind=================================
[ 1.939523] imx-drm display-subsystem: bound imx-lcdifv3-crtc.0 (ops lcdifv3_crtc_ops)
[ 1.947491] imx93 ldb bind======================================================
[ 1.955171] imx8mp_lvds_phy_init================================================
[ 1.962598] imx93 ldb bind===============ending===================================
[ 1.970168] imx-drm display-subsystem: bound soc@0:ldb@4ac10020 (ops imx93_ldb_ops)
[ 1.978157] [drm] Initialized imx-drm 1.0.0 20120507 for display-subsystem on minor 0
[ 1.985986] drm fbdev setup====================================================
[ 1.993293] add by tangyuan =========drm fbdev plug===============================
[ 2.000849] fb helper initial config=====================================
[ 2.007673] imx93 ldb mode valid================================================
[ 2.015125] addby tangyuan fb=====================================
[ 2.023573] imx93 ldb mode valid================================================
[ 2.023617] imx93 ldb encoder atomic check=====================================================
[ 2.023652] imx93 ldb encoder atomic mode set===========================================
[ 2.036714] imx93 ldb encoder enable======================================================
[ 2.036736] imx8mp_lvds_phy_power_on==============================================
[ 2.036739] phy_read============================================================
[ 2.036775] phy_read============================================================
[ 2.036801] add by tangyuan panel bridge enable===================================
[ 2.036804] add by tangyuan for drm_panel_enable=================================
[ 2.368767] 11111111111111111111111111111111111111111111111111111111111
[ 2.368771] tangyuan test for enable=================================================
[ 2.376140] imx93 ldb encoder atomic check=====================================================
[ 2.396839] Console: switching to colour frame buffer device 160x50
[ 2.396884] imx93 ldb encoder atomic check=====================================================
[ 2.521168] imx-drm display-subsystem: [drm] fb0: imx-drmdrmfb frame buffer device
[ 2.528778] add by tangyuan =========drm fbdev plug===============================
[ 2.537491] imx-dwmac 428a0000.ethernet: IRQ eth_lpi not found
[ 2.543376] fb helper hotplug=================================
[ 2.543847] imx-dwmac 428a0000.ethernet: User ID: 0x10, Synopsys ID: 0x52
[ 2.549249] imx93 ldb mode valid================================================
[ 2.556002] imx-dwmac 428a0000.ethernet: DWMAC4/5
[ 2.563486] imx93 ldb encoder atomic check=====================================================
[ 2.568143] imx-dwmac 428a0000.ethernet: DMA HW capability register supported
[ 2.568147] imx-dwmac 428a0000.ethernet: RX Checksum Offload Engine supported
[ 2.591064] imx-dwmac 428a0000.ethernet: TX Checksum insertion supported
[ 2.597796] imx-dwmac 428a0000.ethernet: Wake-Up On Lan supported
[ 2.603971] imx-dwmac 428a0000.ethernet: Enable RX Mitigation via HW Watchdog Timer
[ 2.611617] imx-dwmac 428a0000.ethernet: Enabled L3L4 Flow TC (entries=8)
[ 2.618393] imx-dwmac 428a0000.ethernet: Enabled RFS Flow TC (entries=10)
[ 2.625186] imx-dwmac 428a0000.ethernet: Enabling HW TC (entries=256, max_off=256)
[ 2.632748] imx-dwmac 428a0000.ethernet: Using 32/32 bits DMA host/device width
[ 2.648848] isi-capture 4ae40000.isi:cap_device: deferring 4ae40000.isi:cap_device device registration
[ 2.658374] mxc-isi 4ae40000.isi: mxc_isi.0 registered successfully
[ 2.667182] remoteproc remoteproc0: imx-rproc is available
[ 2.680921] st_lsm6dsx_i2c 0-006a: supply vdd not found, using dummy regulator
[ 2.688292] st_lsm6dsx_i2c 0-006a: supply vddio not found, using dummy regulator
[ 2.752783] st_lsm6dsx_i2c 0-006a: failed to read whoami register
[ 2.759157] st_lsm6dsx_i2c: probe of 0-006a failed with error -5
[ 2.765574] i2c i2c-0: LPI2C adapter registered
[ 2.771365] pca9450 probe========================================================
[ 2.778896] nxp-pca9450 1-0025: No IRQ configured?
[ 2.783710] nxp-pca9450: probe of 1-0025 failed with error -22
[ 2.789685] i2c i2c-1: LPI2C adapter registered
[ 2.795318] i2c 2-0050: Fixed dependency cycle(s) with /soc@0/usb@4c100000/port/endpoint
[ 2.803804] tcpci: probe of 2-0050 failed with error -5
[ 2.809193] i2c 2-0051: Fixed dependency cycle(s) with /soc@0/usb@4c200000/port/endpoint
[ 2.818209] i2c 2-003c: Fixed dependency cycle(s) with /soc@0/bus@42800000/camera/csi@4ae00000/port@0/endpoint
[ 2.828540] i2c i2c-2: LPI2C adapter registered
[ 2.846207] sdhci-esdhc-imx 42860000.mmc: Got CD GPIO
[ 2.846775] dwc-mipi-csi2-host 4ae00000.csi: lanes: 2, name: mxc-mipi-csi2.0
[ 2.865874] OF: graph: no port node found in /soc@0/bus@42000000/i2c@42530000/tcpc@51/connector
[ 2.874618] OF: graph: no port node found in /soc@0/bus@42000000/i2c@42530000/tcpc@51/connector
[ 2.883348] OF: graph: no port node found in /soc@0/bus@42000000/i2c@42530000/tcpc@51/connector
[ 2.887376] mmc1: SDHCI controller on 42860000.mmc [42860000.mmc] using ADMA
[ 2.914030] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[ 2.923530] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[ 2.930215] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2
[ 2.933399] ALSA device list:
[ 2.938868] platform regulatory.0: Falling back to sysfs fallback for: regulatory.db
[ 2.941838] No soundcards found.
[ 2.953389] Waiting for root device /dev/mmcblk1p2...
[ 3.037333] mmc1: host does not support reading read-only switch, assuming write-enable
[ 3.071349] mmc1: new ultra high speed SDR104 SDHC card at address 0001
[ 3.078693] mmcblk1: mmc1:0001 SD16G 14.8 GiB
[ 3.085201] mmcblk1: p1 p2
[ 3.465177] EXT4-fs (mmcblk1p2): recovery complete
[ 3.471173] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Quota mode: none.
[ 3.479783] VFS: Mounted root (ext4 filesystem) on device 179:98.
[ 3.493529] devtmpfs: mounted
[ 3.498190] Freeing unused kernel memory: 3328K
[ 3.502858] Run /sbin/init as init process
[ 3.921726] systemd[1]: System time before build time, advancing clock.
[ 4.006563] systemd[1]: systemd 253.1^ running in system mode (+PAM -AUDIT -SELINUX -APPARMOR +IMA -SMACK +SECCOMP -GCRYPT -GNUTLS -OPENSSL +ACL +BLKID -CURL -ELFUTILS -FIDO2 -IDN2 -IDN -IPTC +KMOD -LIBCRYPTSETUP +LIBFDISK -PCRE2 -PWQUALITY -P11KIT -QRENCODE -TPM2 -BZIP2 -LZ4 -XZ -ZLIB +ZSTD -BPF_FRAMEWORK +XKBCOMMON +UTMP +SYSVINIT default-hierarchy=hybrid)
[ 4.038366] systemd[1]: Detected architecture arm64.

Welcome to NXP i.MX Release Distro 6.1-mickledore (mickledore)!

[ 4.104753] systemd[1]: Hostname set to <imx93evk>.
[ 4.270295] systemd-sysv-generator[173]: SysV service '/etc/init.d/sshd' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 4.298197] systemd-sysv-generator[173]: SysV service '/etc/init.d/psplash.sh' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 4.324944] systemd-sysv-generator[173]: SysV service '/etc/init.d/umountnfs.sh' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 4.350313] systemd-sysv-generator[173]: SysV service '/etc/init.d/halt' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 4.377794] systemd-sysv-generator[173]: SysV service '/etc/init.d/single' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 4.401646] systemd-sysv-generator[173]: SysV service '/etc/init.d/trousers' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 4.425579] systemd-sysv-generator[173]: SysV service '/etc/init.d/reboot' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 4.450525] systemd-sysv-generator[173]: SysV service '/etc/init.d/save-rtc.sh' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 4.475723] systemd-sysv-generator[173]: SysV service '/etc/init.d/umountfs' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 4.500630] systemd-sysv-generator[173]: SysV service '/etc/init.d/sendsigs' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 4.525458] systemd-sysv-generator[173]: SysV service '/etc/init.d/fuse' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 4.552000] systemd-sysv-generator[173]: SysV service '/etc/init.d/rc.local' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 4.907530] systemd[1]: Queued start job for default target Graphical Interface.
[ 4.962706] systemd[1]: Created slice Slice /system/getty.
[ OK ] Created slice Slice /system/getty.
[ 4.987109] systemd[1]: Created slice Slice /system/modprobe.
[ OK ] Created slice Slice /system/modprobe.
[ 5.011073] systemd[1]: Created slice Slice /system/serial-getty.
[ OK ] Created slice Slice /system/serial-getty.
[ 5.034569] systemd[1]: Created slice User and Session Slice.
[ OK ] Created slice User and Session Slice.
[ 5.057395] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[ OK ] Started Dispatch Password …ts to Console Directory Watch.
[ 5.081205] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ OK ] Started Forward Password R…uests to Wall Directory Watch.
[ 5.105158] systemd[1]: Reached target Host and Network Name Lookups.
[ OK ] Reached target Host and Network Name Lookups.
[ 5.128904] systemd[1]: Reached target Path Units.
[ OK ] Reached target Path Units.
[ 5.148926] systemd[1]: Reached target Remote File Systems.
[ OK ] Reached target Remote File Systems.
[ 5.168911] systemd[1]: Reached target Slice Units.
[ OK ] Reached target Slice Units.
[ 5.188939] systemd[1]: Reached target Swaps.
[ OK ] Reached target Swaps.
[ 5.259959] systemd[1]: Listening on RPCbind Server Activation Socket.
[ OK ] Listening on RPCbind Server Activation Socket.
[ 5.285009] systemd[1]: Reached target RPC Port Mapper.
[ OK ] Reached target RPC Port Mapper.
[ 5.305717] systemd[1]: Listening on Syslog Socket.
[ OK ] Listening on Syslog Socket.
[ 5.325362] systemd[1]: Listening on initctl Compatibility Named Pipe.
[ OK ] Listening on initctl Compatibility Named Pipe.
[ 5.349796] systemd[1]: Listening on Journal Audit Socket.
[ OK ] Listening on Journal Audit Socket.
[ 5.373508] systemd[1]: Listening on Journal Socket (/dev/log).
[ OK ] Listening on Journal Socket (/dev/log).
[ 5.397660] systemd[1]: Listening on Journal Socket.
[ OK ] Listening on Journal Socket.
[ 5.417821] systemd[1]: Listening on Network Service Netlink Socket.
[ OK ] Listening on Network Service Netlink Socket.
[ 5.441798] systemd[1]: Listening on udev Control Socket.
[ OK ] Listening on udev Control Socket.
[ 5.465543] systemd[1]: Listening on udev Kernel Socket.
[ OK ] Listening on udev Kernel Socket.
[ 5.485542] systemd[1]: Listening on User Database Manager Socket.
[ OK ] Listening on User Database Manager Socket.
[ 5.533280] systemd[1]: Mounting Huge Pages File System...
Mounting Huge Pages File System...
[ 5.557378] systemd[1]: Mounting POSIX Message Queue File System...
Mounting POSIX Message Queue File System...
[ 5.605360] systemd[1]: Mounting Kernel Debug File System...
Mounting Kernel Debug File System...
[ 5.625304] systemd[1]: Kernel Trace File System was skipped because of an unmet condition check (ConditionPathExists=/sys/kernel/tracing).
[ 5.643536] systemd[1]: Mounting Temporary Directory /tmp...
Mounting Temporary Directory /tmp...
[ 5.689572] systemd[1]: Starting Create List of Static Device Nodes...
Starting Create List of Static Device Nodes...
[ 5.718016] systemd[1]: Starting Load Kernel Module configfs...
Starting Load Kernel Module configfs...
[ 5.757800] systemd[1]: Starting Load Kernel Module drm...
Starting Load Kernel Module drm...
[ 5.809616] systemd[1]: Starting Load Kernel Module fuse...
Starting Load Kernel Module fuse...
[ 5.830740] fuse: init (API version 7.37)
[ 5.837427] systemd[1]: Starting RPC Bind...
Starting RPC Bind...
[ 5.857224] systemd[1]: File System Check on Root Device was skipped because of an unmet condition check (ConditionPathIsReadWrite=!/).
[ 5.889765] systemd[1]: Starting Journal Service...
Starting Journal Service...
[ 5.921169] systemd[1]: Starting Load Kernel Modules...
Starting Load Kernel Modules...
[ 5.950295] systemd[1]: Starting Generate network units from Kernel command line...
Starting Generate network …ts from Kernel command line...
[ 5.969340] systemd-journald[188]: Collecting audit messages is enabled.
[ 6.001875] systemd[1]: Starting Remount Root and Kernel File Systems...
Starting Remount Root and Kernel File Systems...
[ 6.051331] EXT4-fs (mmcblk1p2): re-mounted. Quota mode: none.
[ 6.058558] systemd[1]: Starting Coldplug All udev Devices...
Starting Coldplug All udev Devices...
[ 6.086673] systemd[1]: Starting Setup Virtual Console...
Starting Setup Virtual Console...
[ 6.123456] systemd[1]: Started RPC Bind.
[ OK ] Started RPC Bind.
[ 6.141929] systemd[1]: Started Journal Service.
[ OK ] Started Journal Service.
[ OK ] Mounted Huge Pages File System.
[ OK ] Mounted POSIX Message Queue File System.
[ OK ] Mounted Kernel Debug File System.
[ OK ] Mounted Temporary Directory /tmp.
[ OK ] Finished Create List of Static Device Nodes.
[ OK ] Finished Load Kernel Module configfs.
[ OK ] Finished Load Kernel Module drm.
[ OK ] Finished Load Kernel Module fuse.
[ OK ] Finished Load Kernel Modules.
[ OK ] Finished Generate network units from Kernel command line.
[ OK ] Finished Remount Root and Kernel File Systems.
[ OK ] Finished Setup Virtual Console.
Mounting FUSE Control File System...
Mounting Kernel Configuration File System...
Starting Flush Journal to Persistent Storage...
Starting Apply Kernel Variables...
[ 6.503937] systemd-journald[188]: Received client request to flush runtime journal.
Starting Create Static Device Nodes in /dev...
[ OK ] Mounted FUSE Control File System.
[ OK ] Mounted Kernel Configuration File System.
[ OK ] Finished Flush Journal to Persistent Storage.
[ OK ] Finished Apply Kernel Variables.
[ OK ] Finished Create Static Device Nodes in /dev.
[ OK ] Reached target Preparation for Local File Systems.
Mounting /var/volatile...
[ 6.676214] audit: type=1334 audit(1677836960.748:2): prog-id=5 op=LOAD
[ 6.686448] audit: type=1334 audit(1677836960.760:3): prog-id=6 op=LOAD
Starting Rule-based Manage…for Device Events and Files...
[ OK ] Mounted /var/volatile.
Starting Load/Save OS Random Seed...
[ OK ] Reached target Local File Systems.
Starting Create Volatile Files and Directories...
[ OK ] Finished Load/Save OS Random Seed.
[ OK ] Finished Coldplug All udev Devices.
[ OK ] Finished Create Volatile Files and Directories.
Starting Network Time Synchronization...
Starting Record System Boot/Shutdown in UTMP...
[ OK ] Started Rule-based Manager for Device Events and Files.
Starting Start Psplash Boot Screen...
[ OK ] Finished Record System Boot/Shutdown in UTMP.
[ OK ] Started Start Psplash Boot Screen.
[ OK ] Started Start psplash-syst…progress communication helper.
[ 7.182697] imx93 ldb encoder atomic check=====================================================
[ OK ] Started Network Time Synchronization.
[ OK ] Reached target System Initialization.
[ OK ] Started Daily Cleanup of Temporary Directories.
[ OK ] Reached target System Time Set.
[ OK ] Started Daily rotation of log files.
[ OK ] Reached target Timer Units.
[ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[ OK ] Listening on D-Bus System Message Bus Socket.
Starting sshd.socket...
Starting Weston socket...
Starting Console System Startup Logging...
[ OK ] Listening on sshd.socket.
[ OK ] Listening on Weston socket.
[ OK ] Finished Console System Startup Logging.
[ OK ] Reached target Socket Units.
[ OK ] Reached target Basic System.
[ OK ] Started Job spooling tools.
[ OK ] Started Periodic Command Scheduler.
Starting D-Bus System Message Bus...
[ OK ] Started Linux Firmware Loader Daemon.
Starting IPv6 Packet Filtering Framework...
Starting IPv4 Packet Filtering Framework...
Starting Telephony service...
[ OK ] Started Parsec Service.
[ OK ] Started Updates psplash to basic.
Starting LSB: Run /etc/rc.local if it exist...
[ OK ] Started System Logging Service.
Starting User Login Management...
[ OK ] Started TEE Supplicant.
Starting OpenSSH Key Generation...
[ OK ] Started D-Bus System Message Bus.
[ OK ] Finished IPv6 Packet Filtering Framework.
[ OK ] Finished IPv4 Packet Filtering Framework.
[ OK ] Started LSB: Run /etc/rc.local if it exist.
[ OK ] Finished OpenSSH Key Generation.
[ OK ] Started Telephony service.
[ OK ] Reached target Preparation for Network.
Starting Connection service...
Starting Network Configuration...
[ OK ] Started User Login Management.
[ OK ] Started Connection service.
Starting Avahi mDNS/DNS-SD Stack...
[ OK ] Started Network Configuration.
[ OK ] Reached target Network.
[ 9.258289] fec 42890000.ethernet eth0: Unable to connect to phy
[ 9.285488] imx-dwmac 428a0000.ethernet eth1: Register MEM_TYPE_PAGE_POOL RxQ-0
[ OK ] Started NFS status monitor for NFSv2/3 locking..
Starting Network Time Service...
[ 9.384840] imx-dwmac 428a0000.ethernet eth1: PHY [stmmac-1:01] driver [RTL8211F Gigabit Ethernet] (irq=POLL)
[ 9.408794] imx-dwmac 428a0000.ethernet eth1: No Safety Features support found
[ 9.419293] imx-dwmac 428a0000.ethernet eth1: IEEE 1588-2008 Advanced Timestamp supported
[ OK ] Started Update psplash to network.
[ 9.445117] imx-dwmac 428a0000.ethernet eth1: registered PTP clock
Starting Terminate Psplash Boot Screen...
[ 9.479868] imx-dwmac 428a0000.ethernet eth1: FPE workqueue start
[ 9.492397] imx-dwmac 428a0000.ethernet eth1: configuring for phy/rgmii-id link mode
Starting /etc/rc.local Compatibility...
[ 9.529304] 8021q: adding VLAN 0 to HW filter on device eth1
Starting Wait for Network to be Configured...
Starting Permit User Sessions...
[ OK ] Finished Terminate Psplash Boot Screen.
[ OK ] Started /etc/rc.local Compatibility.
[ OK ] Started Network Time Service.
[ OK ] Finished Permit User Sessions.
[ OK ] Started Avahi mDNS/DNS-SD Stack.
[ OK ] Started Getty on tty1.
[ OK ] Started Serial Getty on ttyLP0.
[ OK ] Reached target Login Prompts.
Starting Weston, a Wayland…ositor, as a system service...
[ 9.891608] fec 42890000.ethernet eth0: Unable to connect to phy
Starting WPA supplicant...
[ 9.987799] audit: type=1334 audit(1678284983.272:6): prog-id=9 op=LOAD
[ 10.015043] audit: type=1334 audit(1678284983.300:7): prog-id=10 op=LOAD
Starting Hostname Service...
[ 10.098831] audit: type=1334 audit(1678284983.384:8): prog-id=11 op=LOAD
[ 10.113745] audit: type=1334 audit(1678284983.396:9): prog-id=12 op=LOAD
Starting User Database Manager...
[ OK ] Started WPA supplicant.
[ OK ] Created slice Slice /system/systemd-fsck.
[ OK ] Found device /dev/mmcblk1p1.
[ OK ] Started User Database Manager.
Starting File System Check on /dev/mmcblk1p1...
[ OK ] Started Hostname Service.
[ OK ] Created slice User Slice of UID 0.
Starting User Runtime Directory /run/user/0...
[ 10.840251] imx8_media_dev: module is from the staging directory, the quality is unknown, you have been warned.
[ 10.913045] CAN device driver interface
[ OK ] Finished User Runtime Directory /run/user/0.
[ 10.989148] mx8-img-md: Registered mxc_isi.0.capture as /dev/video0
Starting User Manager for UID 0...
[ 11.021099] unregister ISI channel: mxc_isi.0
[ 11.048404] audit: type=1006 audit(1678284984.332:10): pid=466 uid=0 old-auid=4294967295 auid=0 tty=(none) old-ses=4294967295 ses=1 res=1
[ 11.066437] audit: type=1300 audit(1678284984.332:10): arch=c00000b7 syscall=64 success=yes exit=1 a0=8 a1=ffffd32ea440 a2=1 a3=1 items=0 ppid=1 pid=466 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=1 comm="(systemd)" exe="/lib/systemd/systemd" key=(null)
[ OK ] Finished File System Check on /dev/mmcblk1p1.
[ 11.151106] rtc-pcf2131-i2c 2-0053: pcf2131_probe: watchdog config (wd_ctl) failed
Mounting /run/media/mmcblk1p1...
[ 11.185609] rtc-pcf2131-i2c: probe of 2-0053 failed with error -5
[ OK ] Mounted /run/media/mmcblk1p1.
[ 11.300277] input: EETI EXC80H60 Touch Screen as /devices/platform/soc@0/44000000.bus/44340000.i2c/i2c-0/0-002a/input/input1
[ 11.322889] exc3000 0-002a: Retry 1 get EETI EXC3000 model: -151
[ 11.408160] exc3000 0-002a: Retry 2 get EETI EXC3000 model: -151
[ 11.457377] fsl_mc_err_probe: No ECC DIMMs discovered
[ OK ] Reached target Hardware activated USB gadget.
[ 11.517100] exc3000 0-002a: Retry 3 get EETI EXC3000 model: -151
[ 11.556993] exc3000: probe of 0-002a failed with error -151
[ OK ] Started User Manager for UID 0.
[ OK ] Started Session c1 of User root.
[ 12.072462] kauditd_printk_skb: 9 callbacks suppressed
[ 12.072479] audit: type=1006 audit(1678284985.356:15): pid=431 uid=0 old-auid=4294967295 auid=0 tty=tty7 old-ses=4294967295 ses=2 res=1
[ 12.096828] audit: type=1300 audit(1678284985.356:15): arch=c00000b7 syscall=64 success=yes exit=1 a0=8 a1=ffffd32ea440 a2=1 a3=1 items=0 ppid=1 pid=431 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=tty7 ses=2 comm="(weston)" exe="/lib/systemd/systemd" key=(null)
[ 12.135039] audit: type=1327 audit(1678284985.356:15): proctitle="(weston)"
Starting Save/Restore Sound Card State...
[ 12.873843] imx93 ldb mode valid================================================
[ OK ] Finished Save/Restore Sound Card State.
[ OK ] Reached target Sound Card.
[ OK ] Started Weston, a Wayland …mpositor, as a system service.
[ 13.184390] imx93 ldb encoder atomic check=====================================================
[ 13.531009] imx93 ldb encoder atomic check=====================================================
[ 13.546857] imx93 ldb encoder atomic check=====================================================
[ 13.566198] imx93 ldb encoder atomic check=====================================================
[ 13.575106] imx93 ldb encoder atomic check=====================================================
[ 13.599746] imx93 ldb encoder atomic check=====================================================
[ 13.615174] imx93 ldb encoder atomic check=====================================================
[ 13.633323] imx93 ldb encoder atomic check=====================================================
[ 13.648652] imx93 ldb encoder atomic check=====================================================
[ 13.666797] imx93 ldb encoder atomic check=====================================================
[ 13.682123] imx93 ldb encoder atomic check=====================================================
[ 13.700412] imx93 ldb encoder atomic check=====================================================
[ 13.715722] imx93 ldb encoder atomic check=====================================================
[ 13.733929] imx93 ldb encoder atomic check=====================================================
[ 13.749355] imx93 ldb encoder atomic check=====================================================
[ 13.767476] imx93 ldb encoder atomic check=====================================================
[ 13.782775] imx93 ldb encoder atomic check=====================================================
[ 13.801029] imx93 ldb encoder atomic check=====================================================
[ 13.816317] imx93 ldb encoder atomic check=====================================================
[ 13.834561] imx93 ldb encoder atomic check=====================================================
[ 13.849862] imx93 ldb encoder atomic check=====================================================
[ 13.868098] imx93 ldb encoder atomic check=====================================================
[ 13.883360] imx93 ldb encoder atomic check=====================================================
[ 13.901648] imx93 ldb encoder atomic check=====================================================
[ 13.916924] imx93 ldb encoder atomic check=====================================================
[ 13.935195] imx93 ldb encoder atomic check=====================================================
[ 13.950506] imx93 ldb encoder atomic check=====================================================
[ 13.968775] imx93 ldb encoder atomic check=====================================================
[ 13.984046] imx93 ldb encoder atomic check=====================================================
[ 14.002301] imx93 ldb encoder atomic check=====================================================
[ 14.017608] imx93 ldb encoder atomic check=====================================================
[ 14.035832] imx93 ldb encoder atomic check=====================================================
[ 14.051126] imx93 ldb encoder atomic check=====================================================
[ 14.069408] imx93 ldb encoder atomic check=====================================================
[ 14.084734] imx93 ldb encoder atomic check=====================================================
[ 14.102952] imx93 ldb encoder atomic check=====================================================
[ 14.118247] imx93 ldb encoder atomic check=====================================================
[ 14.136494] imx93 ldb encoder atomic check=====================================================
[ 14.151776] imx93 ldb encoder atomic check=====================================================
[ 14.170054] imx93 ldb encoder atomic check=====================================================
[ 14.185324] imx93 ldb encoder atomic check=====================================================
[ 14.203591] imx93 ldb encoder atomic check=====================================================
[ 14.218847] imx93 ldb encoder atomic check=====================================================
[ 14.237151] imx93 ldb encoder atomic check=====================================================
[ 14.252461] imx93 ldb encoder atomic check=====================================================
[ 14.270703] imx93 ldb encoder atomic check=====================================================
[ 14.285984] imx93 ldb encoder atomic check=====================================================
[ 14.304248] imx93 ldb encoder atomic check=====================================================
[ 14.319507] imx93 ldb encoder atomic check=====================================================
[ 14.337819] imx93 ldb encoder atomic check=====================================================
[ 14.353180] imx93 ldb encoder atomic check=====================================================
[ 14.371330] imx93 ldb encoder atomic check=====================================================
[ 14.386668] imx93 ldb encoder atomic check=====================================================
[ 14.404926] imx93 ldb encoder atomic check=====================================================
[ 14.420186] imx93 ldb encoder atomic check=====================================================
[ 14.438447] imx93 ldb encoder atomic check=====================================================
[ 14.453714] imx93 ldb encoder atomic check=====================================================
[ 14.471987] imx93 ldb encoder atomic check=====================================================
[ 14.487283] imx93 ldb encoder atomic check=====================================================
[ 14.505497] imx93 ldb encoder atomic check=====================================================
[ 14.520795] imx93 ldb encoder atomic check=====================================================

NXP i.MX Release Distro 6.1-mickledore imx93evk ttyLP0

imx93evk login: rroot
Password: [ 21.673606] platform regulator-can2-stby: deferred probe pending
[ 21.679688] platform regulator-audio-pwr: deferred probe pending
[ 21.687561] platform regulator-dvdd_sel: deferred probe pending
[ 21.693539] platform regulator-dvdd: deferred probe pending
[ 21.699119] platform regulator-vdd: deferred probe pending
[ 21.704610] platform 425b0000.can: deferred probe pending
[ 21.710008] i2c 0-001a: deferred probe pending
[ 21.714453] platform regulator-vddo: deferred probe pending
[ 21.720024] platform regulator-vaa_sel: deferred probe pending
[ 21.725867] platform regulator-avdd: deferred probe pending
[ 21.731442] i2c 2-003c: deferred probe pending
[ 21.735884] platform sound-bt-sco: deferred probe pending
[ 21.741285] platform sound-wm8962: deferred probe pending
[ OK ] Stopped Serial Getty on ttyLP0.
[ OK ] Started Serial Getty on ttyLP0.

NXP i.MX Release Distro 6.1-mickledore imx93evk ttyLP0

imx93evk login: root
root@imx93evk:~# ls
gstshark_2023-03-07_01:05:35 helloworld
root@imx93evk:~# [ 40.864861] audit: type=1334 audit(1678285014.152:16): prog-id=10 op=UNLOAD
[ 40.872294] audit: type=1334 audit(1678285014.152:17): prog-id=9 op=UNLOAD

The critical log is as follows:

 imx93-ldb soc@0:ldb@4ac10020: Failed to create device link (0x180) with soc@0:phy@4ac10024

我不知道这个日志是不是问题所在

我的DTS在附件中

 

0 Kudos
Reply
0 Replies