IMX93 Yocto build fails Ubuntu 25.04 with glibc_2.39.bb:do_package exit code 134

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX93 Yocto build fails Ubuntu 25.04 with glibc_2.39.bb:do_package exit code 134

963件の閲覧回数
Bugger
Contributor III

Following the FRDM getting started bumped into some problems to complete those tasks for Yocto build. Needed to edit some files in in tmp/work files to fix other issues (see other posts today). Now getting the following errors. Not sure if that is related ? Should code modification been made in other files, not in tmp ?) ,or is this a different issue ? Would this be related to (Ubuntu )distro version or not ?

ERROR: Task (/media/user/H8D2P2/develop/NXP/IMX93/Yocto/sources/poky/meta/recipes-core/glibc/glibc_2.39.bb:do_package) failed with exit code '134'
Pseudo log:
path mismatch [2 links]: ino 12190095 db '/media/user/H8D2P2/develop/NXP/IMX93/Yocto/frdm-imx93/tmp/work/armv8a-poky-linux/glibc/2.39+git/packages-split/ldd/usr/bin/ldd' req '/media/user/H8D2P2/develop/NXP/IMX93/Yocto/frdm-imx93/tmp/work/armv8a-poky-linux/glibc/2.39+git/package/usr/bin/ldd'.
Setup complete, sending SIGUSR1 to pid 1736497.

ERROR: Task (/media/user/H8D2P2/develop/NXP/IMX93/Yocto/sources/poky/meta/recipes-core/base-files/base-files_3.0.14.bb:do_package) failed with exit code '134'
Pseudo log:
path mismatch [2 links]: ino 12198909 db '/media/user/H8D2P2/develop/NXP/IMX93/Yocto/frdm-imx93/tmp/work/imx93frdm-poky-linux/base-files/3.0.14/packages-split/base-files/etc/nsswitch.conf' req '/media/user/H8D2P2/develop/NXP/IMX93/Yocto/frdm-imx93/tmp/work/imx93frdm-poky-linux/base-files/3.0.14/sstate-build-package/package/etc/nsswitch.conf'.
Setup complete, sending SIGUSR1 to pid 1750913.

ラベル(2)
0 件の賞賛
返信
0 返答(返信)