I'm trying to connect the I2S signal to HDMI output through LT9611UXC DSI to HDMI chip, the setup of my kernel device tree is:
/ {
hdmi-out {
compatible = "hdmi-connector";
type = "a";
port {
hdmi_con: endpoint {
remote-endpoint = <<9611_out>;
};
};
};
};
&iomuxc {
pinctrl_sai3: sai3grp {
fsl,pins = <
MX93_PAD_GPIO_IO26__SAI3_TX_SYNC 0x31e
MX93_PAD_GPIO_IO16__SAI3_TX_BCLK 0x31e
MX93_PAD_GPIO_IO17__SAI3_MCLK 0x31e
MX93_PAD_GPIO_IO19__SAI3_TX_DATA00 0x31e
MX93_PAD_GPIO_IO20__SAI3_RX_DATA00 0x31e
>;
};
};
&lpi2c3 {
#address-cells = <1>;
#size-cells = <0>;
clock-frequency = <400000>;
pinctrl-names = "default", "sleep";
pinctrl-0 = <&pinctrl_lpi2c3>;
pinctrl-1 = <&pinctrl_lpi2c3>;
status = "okay";
lt9611uxc_codec: hdmi-bridge@2b {
compatible = "lontium,lt9611uxc";
reg = <0x2b>;
#sound-dai-cells = <1>;
adi,dsi-lanes = <4>;
interrupts-extended = <&gpio1 12 IRQ_TYPE_EDGE_FALLING>;
reset-gpios = <&gpio3 26 GPIO_ACTIVE_HIGH>;
status = "okay";
ports {
#address-cells = <1>;
#size-cells = <0>;
port@0 {
reg = <0>;
lt9611_to_dsi: endpoint {
remote-endpoint = <&dsi_to_lt9611>;
};
};
port@2 {
reg = <2>;
lt9611_out: endpoint {
remote-endpoint = <&hdmi_con>;
};
};
};
};
};
&dsi {
status = "okay";
#address-cells = <1>;
#size-cells = <0>;
dsi-lanes = <4>;
ports {
port@1 {
reg = <1>;
dsi_to_lt9611: endpoint {
remote-endpoint = <<9611_to_dsi>;
};
};
};
};
But I can't find any sound card with command aplay -l
I'm using the imx-6.6.3 kernel version with Yocto
Can anybody help me figure this issue out ? Thanks in advanced.