[IMX93] How to config device tree for SPDIF bind with HDMI Audio

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[IMX93] How to config device tree for SPDIF bind with HDMI Audio

3,275件の閲覧回数
charleshuang
Senior Contributor II

Hi NXP Team,

As title, we connect SPDIF output "MX93_PAD_GPIO_IO23__SPDIF_OUT" to ADV7535 audio on our board. So, for this purpose, how should we configure the device tree?

 

 

0 件の賞賛
返信
9 返答(返信)

3,214件の閲覧回数
charleshuang
Senior Contributor II

Hi @jimmychan ,

Yes, the imx93 does not directly support HDMI video/audio.

Our board is MIPI to HDMI, and the SPDIF_OUT is connected to the bridge IC.

In theory, it should work. Please refer to the attached document for the device tree modifications.

And please help us confirm where the issue might be? Thank you!

 

0 件の賞賛
返信

3,162件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

What is the issue you met? No sound come out?

When you test, do you unblank the HDMI?

FYI. https://community.nxp.com/t5/i-MX-Processors/IMX8MP-HDMI-audio-no-sound/td-p/1939886

0 件の賞賛
返信

3,104件の閲覧回数
weikeng-jimmy
Contributor III

Hi Sir,

My customer would to know how to achieve this function as figure (hdmi audio).

We refer Beacon development board setting and use "i2s" audio card format can work normally. (imx8mm-beacon-kit.dts)

sound-hdmi {
compatible = "simple-audio-card";
simple-audio-card,name = "sound-hdmi";
simple-audio-card,format = "i2s";

simple-audio-card,cpu {
sound-dai = <&sai5>;
system-clock-direction-out;
};

simple-audio-card,codec {
sound-dai = <&adv_bridge>;
};
};


Can you give we some suggestion for "spdif" setting. Thanks !

sound-hdmi {
compatible = "simple-audio-card";
simple-audio-card,name = "sound-hdmi";

#address-cells = <1>;
#size-cells = <0>;

simple-audio-card,cpu {
sound-dai = <&xcvr>; // sound-dai = <&sai5>;
};

simple-audio-card,codec {
sound-dai = <&adv7535>;
};
};

error log message as below.

[ 3.134115] asoc-simple-card sound-hdmi: control 3:0:0:IEC958 Playback Default:0 is already present
[ 3.143195] hdmi-audio-codec hdmi-audio-codec.1.auto: ASoC: error at snd_soc_pcm_dai_new on spdif-hifi: -16

螢幕截圖 2024-09-02 13.44.17.png

 

0 件の賞賛
返信

3,143件の閲覧回数
charleshuang
Senior Contributor II

Hi @jimmychan 

Thank your reply, I tried 'unblank the HDMI' but it look like no use.

Yes, there is no audio output.
I tested by using `gplay` to play a AV file.
The SPDIF_OUT has a signal, but there is no sound heard from the HDMI panel.

And my sound card information as below :

root@imx93afee320a1:~# aplay -l
**** List of PLAYBACK Hardware Devices ****
card 0: imxaudioxcvr [imx-audio-xcvr], device 0: XCVR PCM snd-soc-dummy-dai-0 [XCVR PCM snd-soc-dummy-dai-0]
Subdevices: 1/1
Subdevice #0: subdevice #0
card 1: sgtl5000 [sgtl5000], device 0: HiFi sgtl5000-0 [HiFi sgtl5000-0]
Subdevices: 1/1
Subdevice #0: subdevice #0

 

The document of `xcvr` say it support HDMI Audio, is there anything that we need to pay attention to?
https://github.com/nxp-imx/linux-imx/blob/lf-6.1.36-2.1.0/Documentation/devicetree/bindings/sound/fs...

0 件の賞賛
返信

2,840件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

For your reference, the attachment is an example of spdif in dts.

0 件の賞賛
返信

2,777件の閲覧回数
weikeng-jimmy
Contributor III

Hi Jimmy,                                                                                                                                                               Thanks for your support. The imx93-11x11-frdm-aud-hat.dts have xcvr setting same as original imx93 dts file. Can you help to provide spdif access bridge definition in dts as below example.

https://kernel.googlesource.com/pub/scm/linux/kernel/git/next/linux-next/+/refs/heads/akpm-base/Docu...

sound {
compatible = "simple-audio-card";
simple-audio-card,name = "Cubox Audio";

#address-cells = <1>;
#size-cells = <0>;

simple-audio-card,dai-link@0 { /* I2S - HDMI */
reg = <0>;
format = "i2s";
cpu {
sound-dai = <&audio0>;
};
codec {
sound-dai = <&tda998x0>;
};
};

simple-audio-card,dai-link@1 { /* S/PDIF - HDMI */
reg = <1>;
cpu {
sound-dai = <&audio1>;
};
codec {
sound-dai = <&tda998x1>;
};
};

simple-audio-card,dai-link@2 { /* S/PDIF - S/PDIF */
reg = <2>;
cpu {
sound-dai = <&audio2>;
};
codec {
sound-dai = <&spdif_codec>;
};
};
};

 

0 件の賞賛
返信

2,695件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Hello,

 

I got the AE reply. The define of SPDIF in the example "imx93-11x11-frdm-aud-hat.dts " is almost the same with the one on i.mx93-11x11-evk.dts. The attachment is the imx93-11x11-frdm.dts that the AE used. 

 

Best regards,

Jimmy

0 件の賞賛
返信

3,098件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

"The SPDIF_OUT has a signal, but there is no sound heard from the HDMI panel."

Have you try the "alsamixer" to tune the volume?

0 件の賞賛
返信

3,224件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

According to the release notes, i.MX93 is not support the HDMI audio.

https://www.nxp.com/docs/en/release-note/IMX_LINUX_RELEASE_NOTES.pdf

0 件の賞賛
返信