IMX93 DSI: failed to attach bridge /soc@0/dsi@4ae10000 to encoder DSI-34: -517

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX93 DSI: failed to attach bridge /soc@0/dsi@4ae10000 to encoder DSI-34: -517

2,743件の閲覧回数
Satan
Contributor I

I'm working on IMX93 board with mipi screen named "startek,kd050fwfia019" driven by "ili9806e" for a while, and still stucked.

There is no display output while encountering the following message from booting up.

 

[    2.089408] imx-drm display-subsystem: bound imx-lcdifv3-crtc.0 (ops lcdifv3_crtc_ops)
[    2.097386] [drm:drm_bridge_attach] *ERROR* failed to attach bridge /soc@0/dsi@4ae10000 to encoder DSI-34: -517
[    2.107483] dw-mipi-dsi-imx 4ae10000.dsi: [drm:dw_mipi_dsi_imx_bind] *ERROR* failed to attach bridge: -517
[    2.117351] dw-mipi-dsi-imx 4ae10000.dsi: [drm:dw_mipi_dsi_imx_probe] *ERROR* failed to register component: -517

 

 

I have tried two cases of kernel divice tree, both end up with the same error mentioned above.

test case 1 :

 

&dsi {
	status = "okay";

	panel@0 {
		compatible = "startek,kd050fwfia019";
		pinctrl-names = "default";
		pinctrl-0 = <&pinctrl_panel0_gpios>;
	  	vdd-supply = <&reg_vdd_3v3>;
	 	vccio-supply = <&reg_vddio_1v8>;
        reset-gpios = <&gpio2 16 GPIO_ACTIVE_LOW>;
		backlight = <&dsi_backlight>;
		rotation = <90>;
		status = "okay";

		port {
			panel_in: endpoint {
				remote-endpoint = <&dsi_out>;
			};
		};
	};

	ports{
 		#address-cells = <1>;
 		#size-cells = <0>;

		port@1 {
			reg = <1>;

			dsi_out: endpoint {
				remote-endpoint = <&panel_in>;
			};
		};
	};
};

 

test case 2:

 

/ {
        dsi_panel {
		compatible = "startek,kd050fwfia019";
		pinctrl-names = "default";
		pinctrl-0 = <&pinctrl_panel0_gpios>;
	  	vdd-supply = <&reg_vdd_3v3>;
	 	vccio-supply = <&reg_vddio_1v8>;
        reset-gpios = <&gpio2 16 GPIO_ACTIVE_LOW>;
		backlight = <&dsi_backlight>;
		rotation = <90>;
		status = "okay";

		port {
			panel_in: endpoint {
				remote-endpoint = <&dsi_out>;
			};
		};
	};
};

&dsi {
	status = "okay";

	ports{
 		#address-cells = <1>;
 		#size-cells = <0>;

		port@1 {
			reg = <1>;

			dsi_out: endpoint {
				remote-endpoint = <&panel_in>;
			};
		};
	};
};

 

 

panel-ilitek-ili9806e.c :

 

// SPDX-License-Identifier: GPL-2.0

#include <linux/delay.h>
#include <linux/device.h>
#include <linux/err.h>
#include <linux/errno.h>
#include <linux/gpio/consumer.h>
#include <linux/kernel.h>
#include <linux/mod_devicetable.h>
#include <linux/module.h>
#include <linux/property.h>
#include <linux/regulator/consumer.h>

#include <drm/drm_mipi_dsi.h>
#include <drm/drm_modes.h>
#include <drm/drm_panel.h>
#include <drm/drm_probe_helper.h>

#include <video/mipi_display.h>

struct ili9806e_panel;

struct panel_desc {
	const struct drm_display_mode *display_mode;
	unsigned long mode_flags;
	enum mipi_dsi_pixel_format format;
	unsigned int lanes;
	int (*init_sequence)(struct ili9806e_panel *ctx);
};

struct ili9806e_panel {
	struct drm_panel panel;
	struct mipi_dsi_device *dsi;
	struct gpio_desc *reset_gpio;
	struct regulator_bulk_data supplies[2];
	const struct panel_desc *desc;
	enum drm_panel_orientation orientation;
};

static const char * const regulator_names[] = {
	"vdd",
	"vccio",
};

static inline struct ili9806e_panel *to_ili9806e_panel(struct drm_panel *panel)
{
	return container_of(panel, struct ili9806e_panel, panel);
}

static int ili9806e_power_on(struct ili9806e_panel *ctx)
{
	struct mipi_dsi_device *dsi = ctx->dsi;
	int ret;

	gpiod_set_value(ctx->reset_gpio, 1);

	ret = regulator_bulk_enable(ARRAY_SIZE(ctx->supplies), ctx->supplies);
	if (ret < 0) {
		dev_err(&dsi->dev, "regulator bulk enable failed: %d\n", ret);
		return ret;
	}

	usleep_range(10000, 20000);
	gpiod_set_value(ctx->reset_gpio, 0);
	usleep_range(10000, 20000);

	return 0;
}

static int ili9806e_power_off(struct ili9806e_panel *ctx)
{
	struct mipi_dsi_device *dsi = ctx->dsi;
	int ret;

	gpiod_set_value(ctx->reset_gpio, 1);

	ret = regulator_bulk_disable(ARRAY_SIZE(ctx->supplies), ctx->supplies);
	if (ret)
		dev_err(&dsi->dev, "regulator bulk disable failed: %d\n", ret);

	return ret;
}

static int ili9806e_on(struct ili9806e_panel *ctx)
{
    int ret = 0;
	if (ctx->desc->init_sequence) {
		ret = ctx->desc->init_sequence(ctx);
    }

    if (ret != 0) {
        return ret;
    }

	return mipi_dsi_dcs_exit_sleep_mode(ctx->dsi);
}

static int ili9806e_enable(struct drm_panel *panel)
{
	struct ili9806e_panel *ctx = to_ili9806e_panel(panel);

	usleep_range(100000, 120000);

	return mipi_dsi_dcs_set_display_on(ctx->dsi);
}

static int ili9806e_off(struct ili9806e_panel *ctx)
{
	return mipi_dsi_dcs_enter_sleep_mode(ctx->dsi);
}

static int ili9806e_disable(struct drm_panel *panel)
{
	struct ili9806e_panel *ctx = to_ili9806e_panel(panel);

	return mipi_dsi_dcs_set_display_off(ctx->dsi);
}

static int ili9806e_prepare(struct drm_panel *panel)
{
	struct ili9806e_panel *ctx = to_ili9806e_panel(panel);
	int ret;

	ret = ili9806e_power_on(ctx);
	if (ret < 0)
		return ret;

	ret = ili9806e_on(ctx);
	if (ret < 0) {
		ili9806e_power_off(ctx);
		return ret;
	}

	return 0;
}

static int ili9806e_unprepare(struct drm_panel *panel)
{
	struct ili9806e_panel *ctx = to_ili9806e_panel(panel);
	struct mipi_dsi_device *dsi = ctx->dsi;
	int ret;

	ili9806e_off(ctx);

	ret = ili9806e_power_off(ctx);
	if (ret < 0)
		dev_err(&dsi->dev, "power off failed: %d\n", ret);

	return ret;
}

static int ili9806e_get_modes(struct drm_panel *panel,
			      struct drm_connector *connector)
{
	struct ili9806e_panel *ctx = to_ili9806e_panel(panel);
	const struct drm_display_mode *mode = ctx->desc->display_mode;

	return drm_connector_helper_get_modes_fixed(connector, mode);
}

static enum drm_panel_orientation ili9806e_get_orientation(struct drm_panel *panel)
{
	struct ili9806e_panel *ctx = to_ili9806e_panel(panel);

	return ctx->orientation;
}

static const struct drm_panel_funcs ili9806e_funcs = {
	.prepare = ili9806e_prepare,
	.unprepare = ili9806e_unprepare,
    .enable = ili9806e_enable,
    .disable = ili9806e_disable,
	.get_modes = ili9806e_get_modes,
	.get_orientation = ili9806e_get_orientation,
};

static int ili9806e_dsi_probe(struct mipi_dsi_device *dsi)
{
	struct device *dev = &dsi->dev;
	struct ili9806e_panel *ctx;
	int i, ret;

	ctx = devm_kzalloc(dev, sizeof(*ctx), GFP_KERNEL);
	if (!ctx)
		return -ENOMEM;

	ctx->desc = device_get_match_data(dev);

	for (i = 0; i < ARRAY_SIZE(ctx->supplies); i++)
		ctx->supplies[i].supply = regulator_names[i];

	ret = devm_regulator_bulk_get(dev, ARRAY_SIZE(ctx->supplies),
				      ctx->supplies);
	if (ret < 0)
		return ret;

	ctx->reset_gpio = devm_gpiod_get(dev, "reset", GPIOD_OUT_LOW);
	if (IS_ERR(ctx->reset_gpio))
		return dev_err_probe(dev, PTR_ERR(ctx->reset_gpio),
				     "Failed to get reset-gpios\n");

	mipi_dsi_set_drvdata(dsi, ctx);
	ctx->dsi = dsi;

	dsi->mode_flags = ctx->desc->mode_flags;
	dsi->format = ctx->desc->format;
	dsi->lanes = ctx->desc->lanes;

	drm_panel_init(&ctx->panel, dev, &ili9806e_funcs,
		       DRM_MODE_CONNECTOR_DSI);

	ret = of_drm_get_panel_orientation(dev->of_node, &ctx->orientation);
	if (ret)
		return dev_err_probe(dev, ret, "Failed to get orientation\n");

	ret = drm_panel_of_backlight(&ctx->panel);
	if (ret)
		return dev_err_probe(dev, ret, "Failed to get backlight\n");

	drm_panel_add(&ctx->panel);

	ret = mipi_dsi_attach(dsi);
	if (ret < 0) {
		dev_err_probe(dev, ret, "Failed to attach to DSI host\n");
		drm_panel_remove(&ctx->panel);
		return ret;
	}

	return 0;
}

static void ili9806e_dsi_remove(struct mipi_dsi_device *dsi)
{
	struct ili9806e_panel *ctx = mipi_dsi_get_drvdata(dsi);

	mipi_dsi_detach(dsi);
	drm_panel_remove(&ctx->panel);
}

static int ili9806e_switch_page(struct ili9806e_panel *ctx, u8 page)
{
	u8 buf[7] = { 0xff, 0xff, 0x98, 0x81, 0x06, 0x04, page };
	int ret;

	ret = mipi_dsi_dcs_write_buffer(ctx->dsi, buf, sizeof(buf));
	if (ret < 0)
		return ret;

	return 0;
}

static int ili9806e_send_cmd_data(struct ili9806e_panel *ctx, u8 cmd, u8 data)
{
	u8 buf[2] = { cmd, data };
	int ret;

	ret = mipi_dsi_dcs_write_buffer(ctx->dsi, buf, sizeof(buf));
	if (ret < 0)
		return ret;

	return 0;
}

static int ili9806e_send_cmd(struct ili9806e_panel *ctx, u8 cmd)
{
	u8 buf[1] = { cmd };
	int ret;

	ret = mipi_dsi_dcs_write_buffer(ctx->dsi, buf, sizeof(buf));
	if (ret < 0)
		return ret;

	return 0;
}

static int kd050fwfia019_init(struct ili9806e_panel *ctx)
{
    // Change to Page 1
    ili9806e_switch_page(ctx, 0x01);
    //Output    SDA
    ili9806e_send_cmd_data(ctx, 0x08, 0x10);
    //set DE/VSYNC mode
    ili9806e_send_cmd_data(ctx, 0x20, 0x00);
    //DE = 1 Active
    ili9806e_send_cmd_data(ctx, 0x21, 0x01);
    //Resolution setting 480 X 854
    ili9806e_send_cmd_data(ctx, 0x30, 0x01);
    //Inversion setting 2-dot
    ili9806e_send_cmd_data(ctx, 0x31, 0x00);
    //BT  AVDD,AVDD
    ili9806e_send_cmd_data(ctx, 0x40, 0x16);
    //22
    ili9806e_send_cmd_data(ctx, 0x41, 0x33);
    //VGL=DDVDH+VCIP -DDVDL,VGH=2DDVDL-VCIP
    ili9806e_send_cmd_data(ctx, 0x42, 0x03);
    //SET VGH clamp level
    ili9806e_send_cmd_data(ctx, 0x43, 0x09);
    //SET VGL clamp level
    ili9806e_send_cmd_data(ctx, 0x44, 0x06);
    //VREG1
    ili9806e_send_cmd_data(ctx, 0x50, 0x88);
    //VREG2
    ili9806e_send_cmd_data(ctx, 0x51, 0x88);
    //Flicker MSB
    ili9806e_send_cmd_data(ctx, 0x52, 0x00);
    //Flicker LSB
    ili9806e_send_cmd_data(ctx, 0x53, 0x49);
    //Flicker
    ili9806e_send_cmd_data(ctx, 0x55, 0x49);

    ili9806e_send_cmd_data(ctx, 0x60, 0x07);
    ili9806e_send_cmd_data(ctx, 0x61, 0x00);
    ili9806e_send_cmd_data(ctx, 0x62, 0x07);
    ili9806e_send_cmd_data(ctx, 0x63, 0x00);

    //++++++++++++++++++ Gamma Setting ++++++++++++++++++//
    //Positive Gamma
    ili9806e_send_cmd_data(ctx, 0xA0, 0x00);
    ili9806e_send_cmd_data(ctx, 0xA1, 0x09);
    ili9806e_send_cmd_data(ctx, 0xA2, 0x11);
    ili9806e_send_cmd_data(ctx, 0xA3, 0x0B);
    ili9806e_send_cmd_data(ctx, 0xA4, 0x05);
    ili9806e_send_cmd_data(ctx, 0xA5, 0x08);
    ili9806e_send_cmd_data(ctx, 0xA6, 0x06);
    ili9806e_send_cmd_data(ctx, 0xA7, 0x04);
    ili9806e_send_cmd_data(ctx, 0xA8, 0x09);
    ili9806e_send_cmd_data(ctx, 0xA9, 0x0C);
    ili9806e_send_cmd_data(ctx, 0xAA, 0x15);
    ili9806e_send_cmd_data(ctx, 0xAB, 0x08);
    ili9806e_send_cmd_data(ctx, 0xAC, 0x0F);
    ili9806e_send_cmd_data(ctx, 0xAD, 0x12);
    ili9806e_send_cmd_data(ctx, 0xAE, 0x09);
    ili9806e_send_cmd_data(ctx, 0xAF, 0x00);
    //Negative Gamma
    ili9806e_send_cmd_data(ctx, 0xC0, 0x00);
    ili9806e_send_cmd_data(ctx, 0xC1, 0x09);
    ili9806e_send_cmd_data(ctx, 0xC2, 0x10);
    ili9806e_send_cmd_data(ctx, 0xC3, 0x0C);
    ili9806e_send_cmd_data(ctx, 0xC4, 0x05);
    ili9806e_send_cmd_data(ctx, 0xC5, 0x08);
    ili9806e_send_cmd_data(ctx, 0xC6, 0x06);
    ili9806e_send_cmd_data(ctx, 0xC7, 0x04);
    ili9806e_send_cmd_data(ctx, 0xC8, 0x08);
    ili9806e_send_cmd_data(ctx, 0xC9, 0x0C);
    ili9806e_send_cmd_data(ctx, 0xCA, 0x14);
    ili9806e_send_cmd_data(ctx, 0xCB, 0x08);
    ili9806e_send_cmd_data(ctx, 0xCC, 0x0F);
    ili9806e_send_cmd_data(ctx, 0xCD, 0x11);
    ili9806e_send_cmd_data(ctx, 0xCE, 0x09);
    ili9806e_send_cmd_data(ctx, 0xCF, 0x00);

    // Change to Page 6 CMD for GIP timing
    ili9806e_switch_page(ctx, 0x06);
    ili9806e_send_cmd_data(ctx, 0x00, 0x20);
    ili9806e_send_cmd_data(ctx, 0x01, 0x0A);
    ili9806e_send_cmd_data(ctx, 0x02, 0x00);
    ili9806e_send_cmd_data(ctx, 0x03, 0x00);
    ili9806e_send_cmd_data(ctx, 0x04, 0x01);
    ili9806e_send_cmd_data(ctx, 0x05, 0x01);
    ili9806e_send_cmd_data(ctx, 0x06, 0x98);
    ili9806e_send_cmd_data(ctx, 0x07, 0x06);
    ili9806e_send_cmd_data(ctx, 0x08, 0x01);
    ili9806e_send_cmd_data(ctx, 0x09, 0x80);
    ili9806e_send_cmd_data(ctx, 0x0A, 0x00);
    ili9806e_send_cmd_data(ctx, 0x0B, 0x00);
    ili9806e_send_cmd_data(ctx, 0x0C, 0x01);
    ili9806e_send_cmd_data(ctx, 0x0D, 0x01);
    ili9806e_send_cmd_data(ctx, 0x0E, 0x05);
    ili9806e_send_cmd_data(ctx, 0x0F, 0x00);
    ili9806e_send_cmd_data(ctx, 0x10, 0xF0);
    ili9806e_send_cmd_data(ctx, 0x11, 0xF4);
    ili9806e_send_cmd_data(ctx, 0x12, 0x01);
    ili9806e_send_cmd_data(ctx, 0x13, 0x00);
    ili9806e_send_cmd_data(ctx, 0x14, 0x00);
    ili9806e_send_cmd_data(ctx, 0x15, 0xC0);
    ili9806e_send_cmd_data(ctx, 0x16, 0x08);
    ili9806e_send_cmd_data(ctx, 0x17, 0x00);
    ili9806e_send_cmd_data(ctx, 0x18, 0x00);
    ili9806e_send_cmd_data(ctx, 0x19, 0x00);
    ili9806e_send_cmd_data(ctx, 0x1A, 0x00);
    ili9806e_send_cmd_data(ctx, 0x1B, 0x00);
    ili9806e_send_cmd_data(ctx, 0x1C, 0x00);
    ili9806e_send_cmd_data(ctx, 0x1D, 0x00);
    ili9806e_send_cmd_data(ctx, 0x20, 0x01);
    ili9806e_send_cmd_data(ctx, 0x21, 0x23);
    ili9806e_send_cmd_data(ctx, 0x22, 0x45);
    ili9806e_send_cmd_data(ctx, 0x23, 0x67);
    ili9806e_send_cmd_data(ctx, 0x24, 0x01);
    ili9806e_send_cmd_data(ctx, 0x25, 0x23);
    ili9806e_send_cmd_data(ctx, 0x26, 0x45);
    ili9806e_send_cmd_data(ctx, 0x27, 0x67);
    ili9806e_send_cmd_data(ctx, 0x30, 0x11);
    ili9806e_send_cmd_data(ctx, 0x31, 0x11);
    ili9806e_send_cmd_data(ctx, 0x32, 0x00);
    ili9806e_send_cmd_data(ctx, 0x33, 0xEE);
    ili9806e_send_cmd_data(ctx, 0x34, 0xFF);
    ili9806e_send_cmd_data(ctx, 0x35, 0xBB);
    ili9806e_send_cmd_data(ctx, 0x36, 0xAA);
    ili9806e_send_cmd_data(ctx, 0x37, 0xDD);
    ili9806e_send_cmd_data(ctx, 0x38, 0xCC);
    ili9806e_send_cmd_data(ctx, 0x39, 0x66);
    ili9806e_send_cmd_data(ctx, 0x3A, 0x77);
    ili9806e_send_cmd_data(ctx, 0x3B, 0x22);
    ili9806e_send_cmd_data(ctx, 0x3C, 0x22);
    ili9806e_send_cmd_data(ctx, 0x3D, 0x22);
    ili9806e_send_cmd_data(ctx, 0x3E, 0x22);
    ili9806e_send_cmd_data(ctx, 0x3F, 0x22);
    ili9806e_send_cmd_data(ctx, 0x40, 0x22);

    // Change to Page 7 CMD for GIP timing
    ili9806e_switch_page(ctx, 0x07);
    ili9806e_send_cmd_data(ctx, 0x17, 0x22);
    ili9806e_send_cmd_data(ctx, 0x02, 0x77);
    ili9806e_send_cmd_data(ctx, 0x26, 0xB2);

    // Change to Page 0 CMD for Normal command
    ili9806e_switch_page(ctx, 0x00);
    //TE ON
    ili9806e_send_cmd(ctx, 0x35);
    //24BIT
    ili9806e_send_cmd_data(ctx, 0x3A, 0x70);

    // exit sleep
    ili9806e_send_cmd(ctx, 0x11);
    usleep_range(120, 140);
    ili9806e_send_cmd(ctx, 0x29);
    usleep_range(25, 30);

    // enter sleep
    // ili9806e_send_cmd(ctx, 0x28);
    // usleep_range(10, 20);
    // ili9806e_send_cmd(ctx, 0x10);
    // usleep_range(25, 30);

    return 0;
}

static const struct drm_display_mode kd050fwfia019_default_mode = {
	.clock		= 29000,    /* 29000kHz, fps: 60hZ */

	.hdisplay	= 480,
	.hsync_start	= 480 + 30,     /* h + hbp */
	.hsync_end	= 480 + 30 + 4,     /* h + hbp + hspw */
	.htotal		= 480 + 30 + 4 + 18,     /* h + hbp + hspw + hfp = 532 */

	.vdisplay	= 854,
	.vsync_start	= 854 + 30,     /* h + hbp */
	.vsync_end	= 854 + 30 + 4,     /* h + hbp + vspw */
	.vtotal		= 854 + 30 + 4 + 20,     /* h + hbp + vspw + vfp = 908 */

	.width_mm	= 62,
	.height_mm	= 110,

	.flags		= DRM_MODE_FLAG_NHSYNC | DRM_MODE_FLAG_NVSYNC,
	.type		= DRM_MODE_TYPE_DRIVER | DRM_MODE_TYPE_PREFERRED,
};

static const struct panel_desc kd050fwfia019_desc = {
	.init_sequence = kd050fwfia019_init,
	.display_mode = &kd050fwfia019_default_mode,
	.mode_flags = MIPI_DSI_MODE_VIDEO | MIPI_DSI_MODE_VIDEO_BURST |
		      MIPI_DSI_MODE_LPM,
	.format = MIPI_DSI_FMT_RGB888,
	.lanes = 2,
};

static const struct of_device_id ili9806e_of_match[] = {
	{ .compatible = "startek,kd050fwfia019", .data = &kd050fwfia019_desc },
	{ }
};
MODULE_DEVICE_TABLE(of, ili9806e_of_match);

static struct mipi_dsi_driver ili9806e_dsi_driver = {
	.driver = {
		.name = "ili9806e-dsi",
		.of_match_table = ili9806e_of_match,
	},
	.probe = ili9806e_dsi_probe,
	.remove = ili9806e_dsi_remove,
};
module_mipi_dsi_driver(ili9806e_dsi_driver);

MODULE_AUTHOR("Author <author@example.com>");
MODULE_DESCRIPTION("Ilitek ILI9806E Controller Driver");
MODULE_LICENSE("GPL");

 

 

Hope someone can help me figure it out. Thanks

ラベル(2)
タグ(5)
0 件の賞賛
返信
2 返答(返信)

2,677件の閲覧回数
harold07douglas
Contributor I

Hello,

You're encountering (failed to attach bridge: -517) typically indicates that a required component or dependency is not ready during the device initialization process. This is often related to probe order issues in the Linux kernel device tree or missing configurations.

-517 corresponds to -EPROBE_DEFER, which indicates that the kernel driver is deferring its initialization because a dependency (e.g., another device or resource) is not ready.
The common reasons for this error include:
Missing or incorrect configuration in the device tree.
Drivers for dependent components are not loaded or initialized in the correct order.

Ensure that the panel and dsi nodes are correctly defined and match the bindings expected by the driver. Based on your device tree examples:
Confirm that the compatible strings ("startek,kd050fwfia019" and "ili9806e") match those in the kernel drivers.
Validate that the reset-gpios, vdd-supply, and vccio-supply properties are correctly defined and available.

Confirm that the dw-mipi-dsi and ili9806e drivers are being initialized in the correct order. Use dmesg to check for related logs: dmesg | grep -i dsi If the panel driver (panel-ilitek-ili9806e.c) is being probed before the DSI controller is ready, you may need to ensure the controller initializes earlier. Move the panel node to be a sub-node of the dsi controller node. This ensures that the panel is registered as part of the DSI controller's initialization. The panel-ilitek-ili9806e.c file should contain a valid initialization sequence for the ili9806e panel. Double-check the init_sequence function in your driver for any missing steps. 

Enable debug logs for DRM and DSI:

Add the following kernel parameters: 

drm.debug=0x1f

This provides detailed information about DRM and DSI initialization.
Use these logs to identify whether the panel or DSI controller is failing to probe.

Ensure that the regulators (vdd and vccio) and GPIOs are defined and active.
Verify that the backlight node is properly defined and linked in the device tree.

 

If you are still encountering issues, consider checking the driver documentation or consultar ingreso solidario similar device examples in the kernel source. You can also try using CONFIG_DRM_PANEL_SIMPLE as a temporary panel driver for basic testing.
loglevel=8

0 件の賞賛
返信

2,686件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

refer to your driver, do you attach 480x854 display, the clock is 29Mhz, right? then I checked the clock driver, current driver doesn't support this, so you should add the new clock in the fracn_tbl

linux-imx/drivers/clk/imx/clk-fracn-gppll.c at lf-6.6.y · nxp-imx/linux-imx · GitHub

0 件の賞賛
返信