IMX93 A1 can't running bcu

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX93 A1 can't running bcu

2,157件の閲覧回数
Chihyu_Lin
Contributor III

Hello,

I had IMX93 A1 chip PIMX9352CVVXMAB, and trying to run bcu with our board and got error

"Can't auto recognize the board on location_id=1-1.4.2.1..."

I had tried to run with EVK which is A0  it seems working fine, but our boadrd wasn't. It looks like bcu was not support A1 chip right?eeprom.png

regards,

Julie

タグ(1)
0 件の賞賛
返信
5 返答(返信)

2,116件の閲覧回数
Chihyu_Lin
Contributor III

Hi @Manuel_Salas 

Thanks for your reply, but I noticed your SOC Info still shown "i.MX93 Rev A0" is that correct? Our board Uboot shonw Rev1.1.

rev.png

Regards,

Julie

 

0 件の賞賛
返信

2,109件の閲覧回数
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @Chihyu_Lin 

 

I am not pretty sure if BCU is not prepared yet to display A1 SOC revision, but I wanted show to you that A1 and A0 works well in BCU from 1.1.71 version and higher.

 

Best regards!

 

Salas.

 

0 件の賞賛
返信

2,082件の閲覧回数
Chihyu_Lin
Contributor III

Hi @Manuel_Salas 

Thanks for your clarification.

regards,

Julie

2,139件の閲覧回数
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @Chihyu_Lin ,

 

The BCU is supported in both revision, A0 and A1.

I am trying to replicate your issue but unsuccessfully.

Here the logs from my A1 board:

Alejandro_Salas_0-1705008210421.png

 

And from A0:

Alejandro_Salas_1-1705008304459.png

 

Note at first I am doing a Write eeprom (-w) command and the BCU version I am using is 1.1.71.

Is there any thing that I can do for replicate this issue?

 

Best regards.

0 件の賞賛
返信

1,155件の閲覧回数
Saravanans1
Contributor III
Hi,

I am also facing simillar issue, is this issue resolved can anyone provide the steps to resolve the issue?

Regards,
Saravanan S
0 件の賞賛
返信