We have the iMX8QuadXPlus MEK CPU Board.
We followed the below steps to enable Secure Storage TA on this board.
Step 1: Built the Android image for the same using the android_p9.0.0_2.3.4 package.
Step 2: Flashed the trusty image using the following command:
./uuu_imx_android_flash.sh -f imx8qxp -a -e -u trusty-c0
Step 3: The board boots successfully.
Step 4: Entered the fastboot mode using reboot bootloader command on the target
Step 5: Tried to enable the Secure Storage using the following commands
root@XXXX:/android_build/out/target/product/mek_8q# fastboot stage rpmb_key_test.bin
target reported max download size of 419430400 bytes
sending 'rpmb_key_test.bin' (0 KB)...
OKAY [  0.028s]
finished. total time: 0.028s
root@XXXX://android_build/out/target/product/mek_8q# fastboot oem set-rpmb-key
...
OKAY [  0.152s]
finished. total time: 0.152s
root@test-Precision-3630-Tower:/home/nanduser/nishad_2_3_4/android_build/out/target/product/mek_8q#
Step 6: Got the following output :
Starting download of 36bytes
downloading of 36 bytes finished
RPMB key programmed successfully!
RPMB key blob generated!
Step 7: Rebooted the board.
Step 8: After reboot the board executes the uboot and reboots.
Step 9: This happens in a continuous loop.
How do I recover from this ?
Thanks and Regards,
Nishad
Solved! Go to Solution.
Hello,
The solution to the question here:
is the solution to this question as well.
Thanks and Regards,
Nishad
Hi nishadkamdar
seems Step 5 may be incomplete, should be
$ fastboot stage rpmb_key.bin 
$ fastboot oem set-rpmb-key 
as described for example on thread :
https://community.nxp.com/t5/i-MX-Processors/Trusty-RPMB-Key-question/m-p/877366
Best regards
igor
Hi Igor,
Sorry, but both the commands you mentioned are present in the Step 5 log.
Can you pls recheck?
The default rpmb key in the package is rpmb_key_test.bin
Thanks,
nishad
Hello,
The solution to the question here:
is the solution to this question as well.
Thanks and Regards,
Nishad