IMX8qx MEK CPU board goes in a continuous reboot loop after enabling Secure Storage in Trusty

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8qx MEK CPU board goes in a continuous reboot loop after enabling Secure Storage in Trusty

Jump to solution
1,848 Views
nishadkamdar
Contributor III

We have the iMX8QuadXPlus MEK CPU Board.

We followed the below steps to enable Secure Storage TA on this board.

Step 1: Built the Android image for the same using the android_p9.0.0_2.3.4 package.

Step 2: Flashed the trusty image using the following command:

 

 

./uuu_imx_android_flash.sh -f imx8qxp -a -e -u trusty-c0

 

Step 3: The board boots successfully.

Step 4: Entered the fastboot mode using reboot bootloader command on the target

Step 5: Tried to enable the Secure Storage using the following commands

 

 

root@XXXX:/android_build/out/target/product/mek_8q# fastboot stage rpmb_key_test.bin
target reported max download size of 419430400 bytes
sending 'rpmb_key_test.bin' (0 KB)...
OKAY [  0.028s]
finished. total time: 0.028s
root@XXXX://android_build/out/target/product/mek_8q# fastboot oem set-rpmb-key
...
OKAY [  0.152s]
finished. total time: 0.152s
root@test-Precision-3630-Tower:/home/nanduser/nishad_2_3_4/android_build/out/target/product/mek_8q#

 

Step 6: Got the following output :

 

 

Starting download of 36bytes

downloading of 36 bytes finished
RPMB key programmed successfully!
RPMB key blob generated!

 

Step 7: Rebooted the board.

Step 8: After reboot the board executes the uboot and reboots.

Step 9: This happens in a continuous loop.

How do I recover from this ?

Thanks and Regards,

Nishad

0 Kudos
Reply
1 Solution
1,816 Views
nishadkamdar
Contributor III

Hello,

The solution to the question here:

https://community.nxp.com/t5/i-MX-Processors/iMX8QP-MEK-Boot-fails-with-Read-public-key-error-after-...

is the solution to this question as well.

Thanks and Regards,

Nishad

View solution in original post

0 Kudos
Reply
3 Replies
1,836 Views
igorpadykov
NXP Employee
NXP Employee

Hi nishadkamdar

 

seems Step 5 may be incomplete, should be

$ fastboot stage rpmb_key.bin
$ fastboot oem set-rpmb-key

as described for example on thread :

https://community.nxp.com/t5/i-MX-Processors/Trusty-RPMB-Key-question/m-p/877366

 

Best regards
igor

0 Kudos
Reply
1,833 Views
nishadkamdar
Contributor III

Hi Igor,

Sorry, but both the commands you mentioned are present in the Step 5 log.

Can you pls recheck?

The default rpmb key in the package is rpmb_key_test.bin

 

Thanks,

nishad

 

0 Kudos
Reply
1,817 Views
nishadkamdar
Contributor III

Hello,

The solution to the question here:

https://community.nxp.com/t5/i-MX-Processors/iMX8QP-MEK-Boot-fails-with-Read-public-key-error-after-...

is the solution to this question as well.

Thanks and Regards,

Nishad

0 Kudos
Reply