Which version of Linux BSP are you using? Do you mean rotate the screen 90 degree?
hi Rita :
我使用的是 imx-yocto-L4.14.98_2.0.0_ga
root@imx8mmevk:~# cat /proc/version 
Linux version 4.14.98 (root@sunday) (gcc version 7.3.0 (GCC)) #60 SMP PREEMPT Thu Jun 11 14:15:30 CST 2020
I want to rotate screen by soft set
here some infometion:
https://community.nxp.com/thread/521316
title is :How To Rotate 90 Degree Video For Display In I.MX8X
Hi Bright
   rotation patch was sent via mail.
   Best regards
igor
can you give me the patch ???
Sorry that I do not have that patch, you can ask in that thread or creat NXP Support Tickets to him for it.