IMX8mini linux设置横屏

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8mini linux设置横屏

1,464 Views
tanyid
Contributor I

请教:

imx8mini 在linux里,怎么配置成横屏?

Labels (2)
0 Kudos
Reply
3 Replies

1,361 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Which version of Linux BSP are you using? Do you mean rotate the screen 90 degree?

0 Kudos
Reply

1,361 Views
tanyid
Contributor I

hi Rita :

    我使用的是 imx-yocto-L4.14.98_2.0.0_ga

root@imx8mmevk:~# cat /proc/version
Linux version 4.14.98 (root@sunday) (gcc version 7.3.0 (GCC)) #60 SMP PREEMPT Thu Jun 11 14:15:30 CST 2020

I want to rotate screen  by soft set

here some infometion:

https://community.nxp.com/thread/521316
title is :How To Rotate 90 Degree Video For Display In I.MX8X

Hi Bright
   rotation patch was sent via mail.

   Best regards
igor

can you give me the patch ???

0 Kudos
Reply

1,361 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Sorry that I do not have that patch, you can ask in that thread or creat NXP Support Tickets to him for it.

0 Kudos
Reply