IMX8dx rootfs mount issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8dx rootfs mount issue

Jump to solution
2,661 Views
afridi20
Contributor III

Hi sir/mam,

Not able to mount rootfs for imx8dx custom board after kernel and system is getting restarted. I have attached the issue info in below log. Kindly help on this issue. Thank you in advance.

Source Version:

Android Q10.0.0_2.6.0 (Linux 5.4.70 kernel)

Error Log:

U-Boot 2020.04-dirty (Sep 06 2021 - 17:38:50 +0530)

CPU: NXP i.MX8QXP RevC A35 at 1200 MHz at 30C

Model: NXP i.MX8DX MEK
Board: iMX8DX MEK
Boot: SD1
DRAM: 1022 MiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... Run CMD11 1.8V switch
*** Warning - bad CRC, using default environment

In: serial@5a060000
Out: serial@5a060000
Err: serial@5a060000

BuildInfo:
- SCFW 0d54291f, SECO-FW d63fdb21, IMX-MKIMAGE 8947fea3, ATF cb435ee
- U-Boot 2020.04-dirty

flash target is MMC:1
Run CMD11 1.8V switch
Net: Could not get PHY for FEC0: addr 0
Could not get PHY for FEC0: addr 0
Could not get PHY for FEC1: addr 0
Could not get PHY for FEC1: addr 0
No ethernet found.

Fastboot: Normal
Normal Boot
Hit any key to stop autoboot: 0
=> mmc info
Card did not respond to voltage select!
=> mmc dev 1
Run CMD11 1.8V switch
switch to partitions #0, OK
mmc1 is current device
=> mmc info
Device: FSL_SDHC
Manufacturer ID: 3
OEM: 5344
Name: SD32G
Bus Speed: 200000000
Mode: UHS SDR104 (208MHz)
Rd Block Len: 512
SD version 3.0
High Capacity: Yes
Capacity: 29.7 GiB
Bus Width: 4-bit
Erase Group Size: 512 Bytes
=> boota mmc1
Writing A/B metadata to disk.
verify OK, boot 'boot_b'
Can't find partition: system_b
idx 0, ptn 0 name='gpt' start=0 len=2048
idx 1, ptn 0 name='' start=0 len=0
idx 2, ptn 0 name='all' start=0 len=62333952
idx 3, ptn 0 name='bootloader0' start=64 len=8192
idx 4, ptn 1 name='dtbo_a' start=16384 len=8192
idx 5, ptn 2 name='dtbo_b' start=24576 len=8192
idx 6, ptn 3 name='boot_a' start=32768 len=131072
idx 7, ptn 4 name='boot_b' start=163840 len=131072
idx 8, ptn 5 name='misc' start=294912 len=8192
idx 9, ptn 6 name='metadata' start=303104 len=4096
idx 10, ptn 7 name='presistdata' start=307200 len=2048
idx 11, ptn 8 name='super' start=311296 len=14680064
idx 12, ptn 9 name='userdata' start=14991360 len=43712512
idx 13, ptn 10 name='fbmisc' start=58703872 len=2048
idx 14, ptn 11 name='vbmeta_a' start=58707968 len=2048
idx 15, ptn 12 name='vbmeta_b' start=58712064 len=2048
kernel @ 80280000 (36860416)
ramdisk @ 86400000 (7266772)
fdt @ 83e80000 (101116)
## Flattened Device Tree blob at 83e80000
Booting using the fdt blob at 0x83e80000
Using Device Tree in place at 0000000083e80000, end 0000000083e9bafb
Disable clock-controller@37620000 rsrc 287 not owned
Disable clock-controller@5a4d0000 rsrc 62 not owned
Disable clock-controller@5ac90000 rsrc 102 not owned
Disable clock-controller@5b260000 rsrc 253 not owned

Starting kernel ...

[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd042]
[ 0.000000] Linux version 5.4.70-dirty (abc@abc) (Android (5271481 based on r349610) clang version 8.0.8 (https://android.googlesource.com/toolchain/clang 4dba9ad555eabb40b39dc53
c12d09423e9faea7b) (https://android.googlesource.com/toolchain/llvm ab552995647d484a712bf15f77e6c6f4e8ac532b) (based on LLVM 8.0.8svn), GNU ld (binutils-2.27-44492f8e) 2.27.0.20170315
) #33 SMP PREEMPT Mon Sep 6 17:48:18 IST 2021
[ 0.000000] Machine model: Freescale i.MX8QXP MEK
[ 0.000000] efi: Getting EFI parameters from FDT:
[ 0.000000] efi: UEFI not found.
[ 0.000000] Reserved memory: created DMA memory pool at 0x0000000090000000, size 0 MiB
[ 0.000000] OF: reserved mem: initialized node vdev0vring0@90000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x0000000090008000, size 0 MiB
[ 0.000000] OF: reserved mem: initialized node vdev0vring1@90008000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x0000000090010000, size 0 MiB
[ 0.000000] OF: reserved mem: initialized node vdev1vring0@90010000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x0000000090018000, size 0 MiB
[ 0.000000] OF: reserved mem: initialized node vdev1vring1@90018000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x0000000090400000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vdevbuffer, compatible id shared-dma-pool
[ 0.000000] cma: Region at 0x0000000096000000 defined on low/high memory boundary (0x00000000c0000000)
[ 0.000000] cma: Failed to reserve 1184 MiB
[ 0.000000] earlycon: lpuart32 at MMIO 0x000000005a060000 (options '')
[ 0.000000] printk: bootconsole [lpuart32] enabled
[ 0.000000] NUMA: No NUMA configuration found
[ 0.000000] NUMA: Faking a node at [mem 0x0000000080200000-0x00000000bfffffff]
[ 0.000000] NUMA: NODE_DATA [mem 0xbfdef500-0xbfdf0fff]
[ 0.000000] Zone ranges:
[ 0.000000] DMA32 [mem 0x0000000080200000-0x00000000bfffffff]
[ 0.000000] Normal empty
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000080200000-0x0000000083ffffff]
[ 0.000000] node 0: [mem 0x0000000086200000-0x0000000087ffffff]
[ 0.000000] node 0: [mem 0x0000000090020000-0x00000000900fefff]
[ 0.000000] node 0: [mem 0x0000000090100000-0x00000000901fffff]
[ 0.000000] node 0: [mem 0x0000000090500000-0x0000000091ffffff]
[ 0.000000] node 0: [mem 0x0000000094c10000-0x00000000bfffffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000080200000-0x00000000bfffffff]
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: MIGRATE_INFO_TYPE not supported.
[ 0.000000] psci: SMC Calling Convention v1.1
[ 0.000000] percpu: Embedded 32 pages/cpu s93400 r8192 d29480 u131072
[ 0.000000] Detected VIPT I-cache on CPU0
[ 0.000000] CPU features: detected: GIC system register CPU interface
[ 0.000000] Speculative Store Bypass Disable mitigation not required
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 204827
[ 0.000000] Policy zone: DMA32
[ 0.000000] Kernel command line: console=ttyLP0,115200 earlycon init=/init androidboot.hardware=freescale firmware_class.path=/vendor/firmware loop.max_part=7 androidboot.fbTileSup
port=enable cma=1184M@0x960M-0xe00M transparent_hugepage=never androidboot.lcd_density=240 androidboot.primary_display=imx-drm androidboot.wificountrycode=CN androidboot.console=ttyLP
0 buildvariant=userdebug androidboot.serialno=0c0f080e828e5263 androidboot.btmacaddr=0c:0f:08:0e:82:8e androidboot.soc_type=imx8qxp androidboot.boot_device_root=mmcblk1 androidboot.bo
ottime=1BLL:0,1BLE:125291,KL:0,KD:0,AVB:2529,ODT:0,SW:0 androidboot.bootreason=reboot androidboot.verifiedbootstate=green androidboot.flash.locked=1 androidboot.slot_suffix=_b android
boot.vbmeta.device=PARTUUID=a4545c7d-a733-42d5-bb9f-8ec63f2e4350 androidboot.vbmeta.avb_version=1.1 androidboot.vbmeta.device_state=locked androidboot.vbmeta.hash_alg=sha256 androidbo
ot.vbmeta.size=3456 androidboot.vbmeta.digest=6ea552819edddaf3991bcdeaa3aa893dc0ec0418c10
[ 0.000000] Dentry cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 7, 524288 bytes, linear)
[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[ 0.000000] Memory: 774024K/832316K available (19324K kernel code, 1884K rwdata, 10268K rodata, 4416K init, 589K bss, 58292K reserved, 0K cma-reserved)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=4.
[ 0.000000] Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000] GICv3: 512 SPIs implemented
[ 0.000000] GICv3: 0 Extended SPIs implemented
[ 0.000000] GICv3: Distributor has no Range Selector support
[ 0.000000] GICv3: 16 PPIs implemented
[ 0.000000] GICv3: no VLPI support, no direct LPI support
[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000051b00000
[ 0.000000] random: get_random_bytes called from start_kernel+0x1e0/0x3a4 with crng_init=0
[ 0.000000] arch_timer: cp15 timer(s) running at 8.00MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x1d854df40, max_idle_ns: 440795202120 ns
[ 0.000005] sched_clock: 56 bits at 8MHz, resolution 125ns, wraps every 2199023255500ns
[ 0.008837] Console: colour dummy device 80x25
[ 0.013028] Calibrating delay loop (skipped), value calculated using timer frequency.. 16.00 BogoMIPS (lpj=32000)
[ 0.023197] pid_max: default: 32768 minimum: 301
[ 0.027893] LSM: Security Framework initializing
[ 0.032440] SELinux: Initializing.
[ 0.035960] Mount-cache hash table entries: 2048 (order: 2, 16384 bytes, linear)
[ 0.043270] Mountpoint-cache hash table entries: 2048 (order: 2, 16384 bytes, linear)
[ 0.052729] ASID allocator initialised with 32768 entries
[ 0.057933] rcu: Hierarchical SRCU implementation.
[ 0.065096] EFI services will not be available.
[ 0.069629] smp: Bringing up secondary CPUs ...
[ 0.074621] Detected VIPT I-cache on CPU1
[ 0.074653] GICv3: CPU1: found redistributor 1 region 0:0x0000000051b20000
[ 0.074690] CPU1: Booted secondary processor 0x0000000001 [0x410fd042]
[ 0.075291] psci: failed to boot CPU2 (-22)
[ 0.096529] CPU2: failed to boot: -22
[ 0.100709] psci: failed to boot CPU3 (-22)
[ 0.104576] CPU3: failed to boot: -22
[ 0.108260] smp: Brought up 1 node, 2 CPUs
[ 0.112289] SMP: Total of 2 processors activated.
[ 0.116999] CPU features: detected: 32-bit EL0 Support
[ 0.122108] CPU features: detected: CRC32 instructions
[ 0.127284] CPU features: emulated: Privileged Access Never (PAN) using TTBR0_EL1 switching
[ 0.135570] CPU: All CPU(s) started at EL2
[ 0.139675] alternatives: patching kernel code
[ 0.145363] CPU1: update max cpu_capacity 1024
[ 0.146022] devtmpfs: initialized
[ 0.157201] CPU1: update max cpu_capacity 1024
[ 0.172474] Initilizing CustomIPI irq domain
[ 0.176458] Registered cp15_barrier emulation handler
[ 0.181468] Registered setend emulation handler
[ 0.186394] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.195817] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)
[ 0.203024] pinctrl core: initialized pinctrl subsystem
[ 0.208985] DMI not present or invalid.
[ 0.212975] NET: Registered protocol family 16
[ 0.217825] schedtune: configured to support 5 boost groups
[ 0.223217] DMA: preallocated 256 KiB pool for atomic allocations
[ 0.229144] audit: initializing netlink subsys (disabled)
[ 0.234719] audit: type=2000 audit(0.180:1): state=initialized audit_enabled=0 res=1
[ 0.242398] cpuidle: using governor menu
[ 0.246947] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.255324] Serial: AMBA PL011 UART driver
[ 0.259181] imx mu driver is registered.
[ 0.263009] imx rpmsg driver is registered.
[ 0.268343] printk: console [pstore-1] enabled
[ 0.272679] pstore: Registered ramoops as persistent store backend
[ 0.278625] ramoops: using 0x100000@0x91f00000, ecc: 0
[ 0.379597] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages
[ 0.386046] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages
[ 0.392661] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.399351] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages
[ 0.407442] cryptd: max_cpu_qlen set to 1000
[ 0.416593] ACPI: Interpreter disabled.
[ 0.422432] iommu: Default domain type: Translated
[ 0.427193] vgaarb: loaded
[ 0.430039] SCSI subsystem initialized
[ 0.433981] usbcore: registered new interface driver usbfs
[ 0.439180] usbcore: registered new interface driver hub
[ 0.444520] usbcore: registered new device driver usb
[ 0.452073] mc: Linux media interface: v0.10
[ 0.456072] videodev: Linux video capture interface: v2.00
[ 0.461559] pps_core: LinuxPPS API ver. 1 registered
[ 0.466435] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <[email protected]>
[ 0.475569] PTP clock support registered
[ 0.480229] trusty trusty: failed to get version: -1
[ 0.484873] trusty trusty: selected api version: 0 (requested 3)
[ 0.539097] EDAC MC: Ver: 3.0.0
[ 0.544142] FPGA manager framework
[ 0.547332] Advanced Linux Sound Architecture Driver Initialized.
[ 0.553816] Bluetooth: Core ver 2.22
[ 0.557060] NET: Registered protocol family 31
[ 0.561486] Bluetooth: HCI device and connection manager initialized
[ 0.567830] Bluetooth: HCI socket layer initialized
[ 0.572695] Bluetooth: L2CAP socket layer initialized
[ 0.577734] Bluetooth: SCO socket layer initialized
[ 0.584189] imx-scu scu: NXP i.MX SCU Initialized
[ 0.623285] random: fast init done
[ 0.689894] imx8qxp-pinctrl scu:pinctrl: Invalid fsl,pins or pins property in node /scu/pinctrl/wifi_initgrp
[ 0.699609] imx8qxp-pinctrl scu:pinctrl: initialized IMX pinctrl driver
[ 0.727299] clocksource: Switched to clocksource arch_sys_counter
[ 0.823556] VFS: Disk quotas dquot_6.6.0
[ 0.827211] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 0.834253] pnp: PnP ACPI: disabled
[ 0.872180] thermal_sys: Registered thermal governor 'step_wise'
[ 0.872186] thermal_sys: Registered thermal governor 'power_allocator'
[ 0.878438] NET: Registered protocol family 2
[ 0.889559] tcp_listen_portaddr_hash hash table entries: 512 (order: 1, 8192 bytes, linear)
[ 0.897619] TCP established hash table entries: 8192 (order: 4, 65536 bytes, linear)
[ 0.905386] TCP bind hash table entries: 8192 (order: 5, 131072 bytes, linear)
[ 0.912643] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.918971] UDP hash table entries: 512 (order: 2, 16384 bytes, linear)
[ 0.925494] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes, linear)
[ 0.932644] NET: Registered protocol family 1
[ 0.937336] PCI: CLS 0 bytes, default 64
[ 0.942158] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available
[ 0.950844] kvm [1]: IPA Size Limit: 40bits
[ 0.955841] kvm [1]: GICv3: no GICV resource entry
[ 0.960305] kvm [1]: disabling GICv2 emulation
[ 0.964732] kvm [1]: GIC system register CPU interface enabled
[ 0.970615] kvm [1]: vgic interrupt IRQ1
[ 0.974574] kvm [1]: Hyp mode initialized successfully
[ 0.984239] Initialise system trusted keyrings
[ 0.988503] workingset: timestamp_bits=44 max_order=18 bucket_order=0
[ 1.002694] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 1.008361] Registering sdcardfs 0.1
[ 1.012002] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
[ 1.018343] fuse: init (API version 7.31)
[ 1.022412] 9p: Installing v9fs 9p2000 file system support
[ 1.046515] Key type asymmetric registered
[ 1.050284] Asymmetric key parser 'x509' registered
[ 1.055182] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 242)
[ 1.062529] io scheduler mq-deadline registered
[ 1.067045] io scheduler kyber registered
[ 1.093813] pwm-backlight lvds_backlight@0: lvds_backlight@0 supply power not found, using dummy regulator
[ 1.103433] pwm-backlight lvds_backlight@1: lvds_backlight@1 supply power not found, using dummy regulator
[ 1.199691] mxs-dma 5b810000.dma-apbh: initialized
[ 1.207973] Bus freq driver module loaded
[ 1.218807] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 1.230756] 5a060000.serial: ttyLP0 at MMIO 0x5a060010 (irq = 51, base_baud = 5000000) is a FSL_LPUAR[ 1.239936] printk: console [ttyLP0] enabled
[ 1.239936] printk: console [ttyLP0] enabled
[ 1.248362] printk: bootconsole [lpuart32] disabled
[ 1.248362] printk: bootconsole [lpuart32] disabled
[ 1.258483] fsl-lpuart 5a060000.serial: DMA tx channel request failed, operating without tx DMA
[ 1.267254] fsl-lpuart 5a060000.serial: DMA rx channel request failed, operating without rx DMA
[ 1.276589] 5a070000.serial: ttyLP1 at MMIO 0x5a070010 (irq = 52, base_baud = 5000000) is a FSL_LPUART
[ 1.286991] 5a080000.serial: ttyLP2 at MMIO 0x5a080010 (irq = 53, base_baud = 5000000) is a FSL_LPUART
[ 1.339080] dpu-core 56180000.dpu: driver probed
[ 1.370071] brd: module loaded
[ 1.382516] loop: module loaded
[ 1.386229] zram: Added device: zram0
[ 1.395966] imx ahci driver is registered.
[ 1.411733] libphy: Fixed MDIO Bus: probed
[ 1.416930] tun: Universal TUN/TAP device driver, 1.6
[ 1.424823] thunder_xcv, ver 1.0
[ 1.428117] thunder_bgx, ver 1.0
[ 1.431412] nicpf, ver 1.0
[ 1.438589] hclge is initializing
[ 1.441944] hns3: Hisilicon Ethernet Network Driver for Hip08 Family - version
[ 1.449189] hns3: Copyright (c) 2017 Huawei Corporation.
[ 1.454567] e1000: Intel(R) PRO/1000 Network Driver - version 7.3.21-k8-NAPI
[ 1.461627] e1000: Copyright (c) 1999-2006 Intel Corporation.
[ 1.467439] e1000e: Intel(R) PRO/1000 Network Driver - 3.2.6-k
[ 1.473287] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[ 1.479266] igb: Intel(R) Gigabit Ethernet Network Driver - version 5.6.0-k
[ 1.486237] igb: Copyright (c) 2007-2014 Intel Corporation.
[ 1.491863] igbvf: Intel(R) Gigabit Virtual Function Network Driver - version 2.4.0-k
[ 1.499714] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[ 1.506225] sky2: driver version 1.30
[ 1.512422] PPP generic driver version 2.4.2
[ 1.516949] PPP BSD Compression module registered
[ 1.521676] PPP Deflate Compression module registered
[ 1.526763] PPP MPPE Compression module registered
[ 1.531571] NET: Registered protocol family 24
[ 1.536024] PPTP driver version 0.8.5
[ 1.540002] usbcore: registered new interface driver r8152
[ 1.545550] usbcore: registered new interface driver asix
[ 1.551039] usbcore: registered new interface driver ax88179_178a
[ 1.557185] usbcore: registered new interface driver cdc_ether
[ 1.563075] usbcore: registered new interface driver net1080
[ 1.568785] usbcore: registered new interface driver cdc_subset
[ 1.574761] usbcore: registered new interface driver zaurus
[ 1.580400] usbcore: registered new interface driver cdc_ncm
[ 1.586345] VFIO - User Level meta-driver version: 0.3
[ 1.597684] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 1.604256] ehci-pci: EHCI PCI platform driver
[ 1.608801] ehci-platform: EHCI generic platform driver
[ 1.614718] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
[ 1.620915] ohci-pci: OHCI PCI platform driver
[ 1.625441] ohci-platform: OHCI generic platform driver
[ 1.632985] usbcore: registered new interface driver uas
[ 1.638408] usbcore: registered new interface driver usb-storage
[ 1.644534] usbcore: registered new interface driver usbserial_generic
[ 1.651100] usbserial: USB Serial support registered for generic
[ 1.657153] usbcore: registered new interface driver ftdi_sio
[ 1.662938] usbserial: USB Serial support registered for FTDI USB Serial Device
[ 1.670304] usbcore: registered new interface driver usb_serial_simple
[ 1.676873] usbserial: USB Serial support registered for carelink
[ 1.683005] usbserial: USB Serial support registered for zio
[ 1.688704] usbserial: USB Serial support registered for funsoft
[ 1.694749] usbserial: USB Serial support registered for flashloader
[ 1.701136] usbserial: USB Serial support registered for google
[ 1.707100] usbserial: USB Serial support registered for libtransistor
[ 1.713661] usbserial: USB Serial support registered for vivopay
[ 1.719705] usbserial: USB Serial support registered for moto_modem
[ 1.726009] usbserial: USB Serial support registered for motorola_tetra
[ 1.732663] usbserial: USB Serial support registered for novatel_gps
[ 1.739057] usbserial: USB Serial support registered for hp4x
[ 1.744833] usbserial: USB Serial support registered for suunto
[ 1.750794] usbserial: USB Serial support registered for siemens_mpi
[ 1.757279] usbcore: registered new interface driver usb_ehset_test
[ 1.773815] input: sc-powerkey as /devices/platform/sc-powerkey/input/input0
[ 1.782684] usbcore: registered new interface driver xpad
[ 1.788768] usbcore: registered new interface driver usb_acecad
[ 1.794905] usbcore: registered new interface driver aiptek
[ 1.801051] usbcore: registered new interface driver gtco
[ 1.806688] usbcore: registered new interface driver hanwang
[ 1.812710] usbcore: registered new interface driver kbtab
[ 1.821837] imx-sc-rtc scu:rtc: registered as rtc0
[ 1.826754] imx-sc-rtc scu:rtc: setting system clock to 1970-01-01T00:02:16 UTC (136)
[ 1.835979] i2c /dev entries driver
[ 1.843546] mxc-jpeg 58400000.jpegdec: decoder device registered as /dev/video0 (81,0)
[ 1.853136] mxc-jpeg 58450000.jpegenc: encoder device registered as /dev/video1 (81,1)
[ 1.862945] uvcvideo: Unable to create debugfs directory
[ 1.868366] usbcore: registered new interface driver uvcvideo
[ 1.874128] USB Video Class driver (1.1.1)
[ 1.880540] __power_supply_register: Expected proper parent device for 'battery'
[ 1.888471] __power_supply_register: Expected proper parent device for 'usb'
[ 1.899872] trusty-log not supported on secure side.
[ 1.905433] trusty-virtio trusty:trusty-virtio: initializing
[ 1.911176] trusty-virtio trusty:trusty-virtio: trusty_load_device_descr: virtio get descr returned (-1)
[ 1.920687] trusty-virtio trusty:trusty-virtio: failed (-19) to load device descr
[ 1.928195] trusty-virtio trusty:trusty-virtio: Failed to add virtio devices
[ 1.937827] device-mapper: uevent: version 1.0.3
[ 1.942823] device-mapper: ioctl: 4.41.0-ioctl (2019-09-16) initialised: [email protected]
[ 1.951680] Bluetooth: HCI UART driver ver 2.3
[ 1.956155] Bluetooth: HCI UART protocol H4 registered
[ 1.961317] Bluetooth: HCI UART protocol BCSP registered
[ 1.966674] Bluetooth: HCI UART protocol LL registered
[ 1.971828] Bluetooth: HCI UART protocol ATH3K registered
[ 1.977268] Bluetooth: HCI UART protocol Three-wire (H5) registered
[ 1.984084] Bluetooth: HCI UART protocol Broadcom registered
[ 1.989783] Bluetooth: HCI UART protocol QCA registered
[ 2.002083] sdhci: Secure Digital Host Controller Interface driver
[ 2.008346] sdhci: Copyright(c) Pierre Ossman
[ 2.013527] Synopsys Designware Multimedia Card Interface Driver
[ 2.021802] sdhci-pltfm: SDHCI platform and OF driver helper
[ 2.030198] mmc0: CQHCI version 5.10
[ 2.065328] mmc0: SDHCI controller on 5b010000.mmc [5b010000.mmc] using ADMA
[ 2.078797] ledtrig-cpu: registered to indicate activity on CPUs
[ 2.086488] hidraw: raw HID events driver (C) Jiri Kosina
[ 2.094945] usbcore: registered new interface driver usbhid
[ 2.100568] usbhid: USB HID core driver
[ 2.113906] mxc-isi 58100000.isi: mxc_isi.0 registered successfully
[ 2.124844] mxc-isi 58140000.isi: mxc_isi.4 registered successfully
[ 2.151337] mxc-mipi-csi2 58227000.csi: lanes: 2, name: mxc-mipi-csi2.0
[ 2.160618] mxc-parallel-csi 58261000.pcsi: mxc_parallel_csi_probe probe successfully
[ 2.169691] ashmem: initialized
[ 2.188850] Galcore version 6.4.3.p1.305572
[ 2.215279] [drm] Initialized vivante 1.0.0 20170808 for 80000000.imx8_gpu0_ss on minor 0
[ 2.229860] usbcore: registered new interface driver snd-usb-audio
[ 2.283961] fsl-audmix 59840000.amix: DAI FE name:HiFi-AUDMIX-FE-ai@59820000
[ 2.291100] fsl-audmix 59840000.amix: DAI FE name:HiFi-AUDMIX-FE-ai@59830000
[ 2.298543] imx-audmix imx-audmix.0: snd-soc-dummy-dai <-> 59820000.sai mapping ok
[ 2.306192] imx-audmix imx-audmix.0: snd-soc-dummy-dai <-> 59830000.sai mapping ok
[ 2.313879] imx-audmix imx-audmix.0: snd-soc-dummy-dai <-> audmix-0 mapping ok
[ 2.321205] imx-audmix imx-audmix.0: snd-soc-dummy-dai <-> audmix-1 mapping ok
[ 2.328519] imx-audmix imx-audmix.0: ASoC: no DMI vendor name!
[ 2.340418] pktgen: Packet Generator for packet performance testing. Version: 2.75
[ 2.348389] drop_monitor: Initializing network drop monitor service
[ 2.354818] NET: Registered protocol family 26
[ 2.359305] netem: version 1.3
[ 2.362369] u32 classifier
[ 2.365112] input device check on
[ 2.368798] Actions configured
[ 2.373042] xt_time: kernel timezone is -0000
[ 2.377588] gre: GRE over IPv4 demultiplexor driver
[ 2.382491] IPv4 over IPsec tunneling driver
[ 2.387498] Initializing XFRM netlink socket
[ 2.391831] IPsec XFRM device driver
[ 2.396000] NET: Registered protocol family 10
[ 2.401573] Segment Routing with IPv6
[ 2.405361] mip6: Mobile IPv6
[ 2.409496] NET: Registered protocol family 17
[ 2.414030] NET: Registered protocol family 15
[ 2.418645] Bluetooth: RFCOMM TTY layer initialized
[ 2.423561] Bluetooth: RFCOMM socket layer initialized
[ 2.428761] Bluetooth: RFCOMM ver 1.11
[ 2.432529] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[ 2.437863] Bluetooth: BNEP filters: protocol multicast
[ 2.443103] Bluetooth: BNEP socket layer initialized
[ 2.448087] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[ 2.454058] Bluetooth: HIDP socket layer initialized
[ 2.459077] l2tp_core: L2TP core driver, V2.0
[ 2.463468] l2tp_ppp: PPPoL2TP kernel driver, V2.0
[ 2.468297] 8021q: 802.1Q VLAN Support v1.8
[ 2.472522] lib80211: common routines for IEEE802.11 drivers
[ 2.478989] 9pnet: Installing 9P2000 support
[ 2.483322] tsn generic netlink module v1 init...
[ 2.488973] registered taskstats version 1
[ 2.493127] Loading compiled-in X.509 certificates
[ 2.498104] Key type ._fscrypt registered
[ 2.502134] Key type .fscrypt registered
[ 2.506076] Key type fscrypt-provisioning registered
[ 2.512304] pstore: Using crash dump compression: deflate
[ 2.520905] mxs_phy 5b100000.usbphy: 5b100000.usbphy supply phy-3p0 not found, using dummy regulator
[ 2.545408] usb_phy_generic bus@5b000000:usb3-phy: bus@5b000000:usb3-phy supply vcc not found, using dummy regulator
[ 2.561929] ov5640 16-003c: 16-003c supply DOVDD not found, using dummy regulator
[ 2.569570] ov5640 16-003c: 16-003c supply AVDD not found, using dummy regulator
[ 2.577002] ov5640 16-003c: 16-003c supply DVDD not found, using dummy regulator
[ 2.632139] ov5640 16-003c: ov5640_read_reg: error: reg=300a
[ 2.637831] ov5640 16-003c: ov5640_check_chip_id: failed to read chip identifier
[ 2.645391] ov5640: probe of 16-003c failed with error -5
[ 2.650923] i2c i2c-16: LPI2C adapter registered
[ 2.714436] mmc1: CQHCI version 5.10
[ 2.718142] sdhci-esdhc-imx 5b020000.mmc: Got CD GPIO
[ 2.755353] mmc1: SDHCI controller on 5b020000.mmc [5b020000.mmc] using ADMA
[ 2.766072] pps pps0: new PPS source ptp0
[ 2.770565] fec 5b040000.ethernet: Invalid MAC address: 00:00:00:00:00:00
[ 2.777461] fec 5b040000.ethernet: Using random MAC address: 32:2a:c5:1a:94:23
[ 2.789561] libphy: fec_enet_mii_bus: probed
[ 2.794056] mdio_bus 5b040000.ethernet-1: MDIO device at address 0 is missing.
[ 2.802293] fec 5b040000.ethernet eth0: registered PHC device 0
[ 2.813432] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 2.820168] [drm] No driver support for vblank timestamp query.
[ 2.826385] imx-drm display-subsystem: bound imx-drm-dpu-bliteng.2 (ops dpu_bliteng_ops)
[ 2.835253] imx-drm display-subsystem: bound imx-dpu-crtc.0 (ops dpu_crtc_ops)
[ 2.843085] imx-drm display-subsystem: bound imx-dpu-crtc.1 (ops dpu_crtc_ops)
[ 2.853211] pwm-backlight lvds_backlight@0: lvds_backlight@0 supply power not found, using dummy regulator
[ 2.864870] pwm-backlight lvds_backlight@1: lvds_backlight@1 supply power not found, using dummy regulator
[ 2.883526] imx-rproc imx8x_cm4@0: failed to find syscon
[ 2.889106] imx-rproc imx8x_cm4@0: mbox_request_channel_byname() could not locate channel named "txdb"
[ 2.898483] imx-rproc imx8x_cm4@0: No txdb, ret 0
[ 2.903773] remoteproc remoteproc0: imx-rproc is available
[ 2.910472] asoc-simple-card sound-bt-sco: bt-sco-pcm-wb <-> 59040000.sai mapping ok
[ 2.918314] asoc-simple-card sound-bt-sco: ASoC: no DMI vendor name!
[ 2.936298] adv7511 17-003d: 17-003d supply avdd not found, using dummy regulator
[ 2.943905] adv7511 17-003d: 17-003d supply dvdd not found, using dummy regulator
[ 2.951447] adv7511 17-003d: 17-003d supply pvdd not found, using dummy regulator
[ 2.958997] adv7511 17-003d: 17-003d supply a2vdd not found, using dummy regulator
[ 2.966630] adv7511 17-003d: 17-003d supply v3p3 not found, using dummy regulator
[ 2.974153] adv7511 17-003d: 17-003d supply v1p2 not found, using dummy regulator
[ 2.982149] adv7511 17-003d: Probe failed. Remote port 'dsi_host@56228000' disabled
[ 2.989927] i2c i2c-17: LPI2C adapter registered
[ 3.002812] adv7511 18-003d: 18-003d supply avdd not found, using dummy regulator
[ 3.010538] adv7511 18-003d: 18-003d supply dvdd not found, using dummy regulator
[ 3.018098] adv7511 18-003d: 18-003d supply pvdd not found, using dummy regulator
[ 3.025664] adv7511 18-003d: 18-003d supply a2vdd not found, using dummy regulator
[ 3.033297] adv7511 18-003d: 18-003d supply v3p3 not found, using dummy regulator
[ 3.040854] adv7511 18-003d: 18-003d supply v1p2 not found, using dummy regulator
[ 3.048807] adv7511 18-003d: Probe failed. Remote port 'dsi_host@56248000' disabled
[ 3.056622] i2c i2c-18: LPI2C adapter registered
[ 3.066531] mmc1: host does not support reading read-only switch, assuming write-enable
[ 3.077135] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 3.083877] [drm] No driver support for vblank timestamp query.
[ 3.090021] imx-drm display-subsystem: bound imx-drm-dpu-bliteng.2 (ops dpu_bliteng_ops)
[ 3.098581] imx-drm display-subsystem: bound imx-dpu-crtc.0 (ops dpu_crtc_ops)
[ 3.106481] imx-drm display-subsystem: bound imx-dpu-crtc.1 (ops dpu_crtc_ops)
[ 3.122367] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 3.129046] [drm] No driver support for vblank timestamp query.
[ 3.135069] imx-drm display-subsystem: bound imx-drm-dpu-bliteng.2 (ops dpu_bliteng_ops)
[ 3.143572] imx-drm display-subsystem: bound imx-dpu-crtc.0 (ops dpu_crtc_ops)
[ 3.151098] imx-drm display-subsystem: bound imx-dpu-crtc.1 (ops dpu_crtc_ops)
[ 3.168873] isi-m2m 58100000.isi:m2m_device: Register m2m success for ISI.0
[ 3.176886] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 3.179463] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[ 3.183543] [drm] No driver support for vblank timestamp query.
[ 3.193075] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[ 3.197360] imx-drm display-subsystem: bound imx-drm-dpu-bliteng.2 (ops dpu_bliteng_ops)
[ 3.204034] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2
[ 3.212375] imx-drm display-subsystem: bound imx-dpu-crtc.0 (ops dpu_crtc_ops)
[ 3.220640] platform regulatory.0: Falling back to sysfs fallback for: regulatory.db
[ 3.235688] imx-drm display-subsystem: bound imx-dpu-crtc.1 (ops dpu_crtc_ops)
[ 3.253487] mx8-img-md: Registered mxc_isi.0.capture as /dev/video3
[ 3.260380] mx8-img-md: Registered mxc_isi.4.capture as /dev/video4
[ 3.262721] mmc1: new ultra high speed SDR104 SDHC card at address aaaa
[ 3.266919] mx8-img-md: Can't find i2c client device for ov5640@3c
[ 3.275764] mmcblk1: mmc1:aaaa SD32G 29.7 GiB
[ 3.279868] mx8-img-md: Unregistered all entities
[ 3.289428] mmcblk1: p1 p2 p3 p4 p5 p6 p7 p8 p9 p10 p11 p12
[ 3.290927] ALSA device list:
[ 3.298227] #0: imx-audmix
[ 3.298243] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 3.301163] #1: bt-sco-audio
[ 3.307820] [drm] No driver support for vblank timestamp query.
[ 3.307922] imx-drm display-subsystem: bound imx-drm-dpu-bliteng.2 (ops dpu_bliteng_ops)
[ 3.311409] imx-drm display-subsystem: bound imx-dpu-crtc.0 (ops dpu_crtc_ops)
[ 3.332946] imx-drm display-subsystem: bound imx-dpu-crtc.1 (ops dpu_crtc_ops)
[ 3.349620] mx8-img-md: Registered mxc_isi.0.capture as /dev/video3
[ 3.356324] mx8-img-md: Registered mxc_isi.4.capture as /dev/video4
[ 3.362841] mx8-img-md: Can't find i2c client device for ov5640@3c
[ 3.369422] mx8-img-md: Unregistered all entities
[ 3.376656] VFS: Cannot open root device "(null)" or unknown-block(0,0): error -6
[ 3.384258] Please append a correct "root=" boot option; here are the available partitions:
[ 3.392673] 0100 8192 ram0
[ 3.392676] (driver?)
[ 3.398807] 0101 8192 ram1
[ 3.398808] (driver?)
[ 3.404951] 0102 8192 ram2
[ 3.404953] (driver?)
[ 3.411081] 0103 8192 ram3
[ 3.411083] (driver?)
[ 3.417227] 0104 8192 ram4
[ 3.417228] (driver?)
[ 3.423369] 0105 8192 ram5
[ 3.423370] (driver?)
[ 3.429515] 0106 8192 ram6
[ 3.429516] (driver?)
[ 3.435660] 0107 8192 ram7
[ 3.435661] (driver?)
[ 3.441792] 0108 8192 ram8
[ 3.441794] (driver?)
[ 3.447954] 0109 8192 ram9
[ 3.447957] (driver?)
[ 3.454094] 010a 8192 ram10
[ 3.454095] (driver?)
[ 3.460350] 010b 8192 ram11
[ 3.460352] (driver?)
[ 3.466569] 010c 8192 ram12
[ 3.466570] (driver?)
[ 3.472810] 010d 8192 ram13
[ 3.472812] (driver?)
[ 3.479027] 010e 8192 ram14
[ 3.479028] (driver?)
[ 3.485283] 010f 8192 ram15
[ 3.485285] (driver?)
[ 3.491532] b300 31166976 mmcblk1
[ 3.491535] driver: mmcblk
[ 3.498386] b301 4096 mmcblk1p1 779d152a-7f98-4398-8992-d755e6a16a3a
[ 3.498388]
[ 3.507423] b302 4096 mmcblk1p2 95d49157-7b52-4ed7-a859-4a98ee521392
[ 3.507425]
[ 3.516471] b303 65536 mmcblk1p3 777ba0a1-7688-49ce-b3c1-a528fe5ad0ac
[ 3.516473]
[ 3.525470] b304 65536 mmcblk1p4 89dc66d7-5960-4aee-8380-f794c8a43b7c
[ 3.525471]
[ 3.534477] b305 4096 mmcblk1p5 5f2818a4-f613-46a2-93e7-4304
[ 3.534479]
[ 3.543503] b306 2048 mmcblk1p6 1234ac41-a6b0-47ba-b583-d018
[ 3.543505]
[ 3.552511] b307 1024 mmcblk1p7 665c8871-de2c-4307-ac71-c7f7
[ 3.552512]
[ 3.561521] b308 7340032 mmcblk1p8 b378f871-947f-4b66-9bb6-d81d8e5a7b42
[ 3.561523]
[ 3.570516] b309 21856256 mmcblk1p9 a172d61c-43af-4306-95b9-fde159a5a831
[ 3.570518]
[ 3.579552] b30a 1024 mmcblk1p10 7e7d0b6b-8334-4f68-b6bd-ab98cc228820
[ 3.579554]
[ 3.588667] b30b 1024 mmcblk1p11 cea107d7-2256-4b82-b73c-eb361efdc859
[ 3.588669]
[ 3.597752] b30c 1024 mmcblk1p12 a4545c7d-a733-42d5-bb9f-8ec63f2e4350
[ 3.597753]
[ 3.606843] Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0)
[ 3.615117] CPU: 0 PID: 1 Comm: swapper/0 Not tainted 5.4.70-dirty #33
[ 3.621644] Hardware name: Freescale i.MX8QXP MEK (DT)
[ 3.626787] Call trace:
[ 3.629246] dump_backtrace+0x0/0x134
[ 3.632915] show_stack+0x14/0x1c
[ 3.636234] dump_stack+0xa0/0xd8
[ 3.639552] panic+0x148/0x350
[ 3.642612] mount_block_root+0x130/0x1e4
[ 3.646623] mount_root+0x70/0x90
[ 3.649941] prepare_namespace+0xf0/0x1cc
[ 3.653955] kernel_init_freeable+0x118/0x13c
[ 3.658318] kernel_init+0x14/0x294
[ 3.661809] ret_from_fork+0x10/0x18
[ 3.665392] SMP: stopping secondary CPUs
[ 3.669318] Kernel Offset: disabled
[ 3.672807] CPU features: 0x00010002,20002008
[ 3.677165] Memory Limit: none
[ 3.682430] Rebooting in 5 seconds..

0 Kudos
Reply
1 Solution
2,418 Views
afridi20
Contributor III
Enabled DYNAMIC_PARTIONS in uboot defconfig which resolves the issue.

View solution in original post

0 Kudos
Reply
1 Reply
2,419 Views
afridi20
Contributor III
Enabled DYNAMIC_PARTIONS in uboot defconfig which resolves the issue.
0 Kudos
Reply